This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
从28335的datasheet上看到,芯片的GPIO的驱动电流能达到4mA,部分管脚(Group 2)的驱动电流能达到8mA。
我将GPIO31配置为GPIO管脚,配置成output,输出高电平,外接一个1K的电阻。
程序运行起来后,高电平被拉低到了1.2V,去掉1K电阻,则正常输出3.3V,
请问有人知道是怎么回事吗?为什么驱动电流达不到手册上写的4mA
你好,请问你的电阻是怎么接的?串联在引脚上吗?
这里你是如何测试的?user3691519 说:高电平被拉低到了1.2V
user3691519 说:电阻一端接GPIO,一端接地,然后是用示波器测的
如果你的示波器一端连接的是电阻靠近GPIO侧,一端接地,那测量的应该是GPIO输出电压在电阻上的分压?