您好!
TMS320F28377D的CPU1,CPU2同时使用DCSM文件进行加密。
CPU1进行“UNLOCK”操作后可以再次导入代码
CPU2进行“UNLOCK”操作后代码烧写失败(多次尝试,可以Erase,但是烧写到最后始终显示,Load Failed)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
TMS320F28377D的CPU1,CPU2同时使用DCSM文件进行加密。
CPU1进行“UNLOCK”操作后可以再次导入代码
CPU2进行“UNLOCK”操作后代码烧写失败(多次尝试,可以Erase,但是烧写到最后始终显示,Load Failed)
user4862132 说:CPU1,CPU2同时使用DCSM文件进行加密。
能否给出您的详细设置?另外您使用的自己的程序还是TI的某个例程?
user4862132 说:CPU2进行“UNLOCK”操作后代码烧写失败(多次尝试,可以Erase,但是烧写到最后始终显示,Load Failed)
能否给出详细的错误信息?是否有使用uniflash来unlock?
我是用的uniflash来加密解密的,如下图可以正常加密解密,并且解密后可以正常烧录out文件
另外请您参考一下
若还是不行的话,请您分享一下debug log,如下操作:
CCS Help-> CCS Support -> Select Debug Server Log -> Properties -> Select Enable Debug Server Logging + 选择 log file location -> Ok
或者您可以私信一下您的工程,我们拿开发板测试一下,谢谢