This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DSP28075CLA配置中断源后不执行

28075的CLA中断源选择EPWM1INT,中断频率16K,但CLA不会执行里面程序,CLA跟什么配置会产生冲突

  • 能否请您详细说一下,给出相关截图?或者给出相关代码/工程?
  • 起初我将CLA配置成中断源是EPWM1INT(DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = 36)频率为16K,此时CLA正常执行程序,但是后来为了增加一个中断,配置了EPWM2作为内部中断的中断源,频率为10K,之后CLA就不能正常执行了,

    CLA配置:
    EALLOW;

    // Initialize and wait for CLA1ToCPUMsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CLA1TOCPU = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CLA1TOCPU != 1){};

    //
    // Initialize and wait for CPUToCLA1MsgRAM
    //
    MemCfgRegs.MSGxINIT.bit.INIT_CPUTOCLA1 = 1;
    while(MemCfgRegs.MSGxINITDONE.bit.INITDONE_CPUTOCLA1 != 1){};

    //
    // Select LS5RAM to be the programming space for the CLA
    // First configure the CLA to be the master for LS5 and then
    // set the space to be a program block
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS3 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS3 = 1;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS2 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS2 = 1;

    //
    // Next configure LS0RAM and LS1RAM as data spaces for the CLA
    // First configure the CLA to be the master for LS0(1) and then
    // set the spaces to be code blocks
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS0 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS0 = 0;

    MemCfgRegs.LSxMSEL.bit.MSEL_LS1 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS1 = 0;

    EDIS;

    //
    // Compute all CLA task vectors
    // On Type-1 CLAs the MVECT registers accept full 16-bit task addresses as
    // opposed to offsets used on older Type-0 CLAs
    //
    EALLOW;
    #pragma diag_suppress 770
    Cla1Regs.MVECT1 = (Uint16)(&Cla1Task1);
    Cla1Regs.MVECT2 = (Uint16)(&Cla1Task2);
    Cla1Regs.MVECT3 = (Uint16)(&Cla1Task3);
    Cla1Regs.MVECT4 = (Uint16)(&Cla1Task4);
    Cla1Regs.MVECT5 = (Uint16)(&Cla1Task5);
    Cla1Regs.MVECT6 = (Uint16)(&Cla1Task6);
    Cla1Regs.MVECT7 = (Uint16)(&Cla1Task7);
    Cla1Regs.MVECT8 = (Uint16)(&Cla1Task8);
    #pragma diag_default 770
    // //
    // // Enable the IACK instruction to start a task on CLA in software
    // // for all 8 CLA tasks. Also, globally enable all 8 tasks (or a
    // // subset of tasks) by writing to their respective bits in the
    // // MIER register
    // //
    // Cla1Regs.MCTL.bit.IACKE = 1;
    // Cla1Regs.MIER.all = 0x00FF;
    DmaClaSrcSelRegs.CLA1TASKSRCSEL1.bit.TASK1 = 36; //EPWM12 INT trigger CLA task1
    Cla1Regs.MIER.all = M_INT1; //使能任务1

    EDIS;

    //
    // Configure the vectors for the end-of-task interrupt for all
    // 8 tasks
    //
    PieVectTable.CLA1_1_INT = &cla1Isr1;
    PieVectTable.CLA1_2_INT = &cla1Isr2;
    PieVectTable.CLA1_3_INT = &cla1Isr3;
    PieVectTable.CLA1_4_INT = &cla1Isr4;
    PieVectTable.CLA1_5_INT = &cla1Isr5;
    PieVectTable.CLA1_6_INT = &cla1Isr6;
    PieVectTable.CLA1_7_INT = &cla1Isr7;
    PieVectTable.CLA1_8_INT = &cla1Isr8;

    //
    // Enable CLA interrupts at the group and subgroup levels
    //
    //PieCtrlRegs.PIEIER11.all = 0xFFFF;
    //IER |= (M_INT11 );

    // Disable CLA interrupts at the group and subgroup levels
    //
    PieCtrlRegs.PIEIER11.all = 0x0000;
    IER = 0x0000;

    EPWM中断源配置
    //EPWM1A --> INT & ADC Trigger //
    EALLOW;
    EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_HI; // Forced Hi (EPWM1A = High state)
    EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_HI; // Forced Hi (EPWM1B = High state)
    EPwm1Regs.TZFRC.bit.OST = 1; // Forces a fault on the OST latch and sets the OSTFLG bit.
    EDIS;
    EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE; // This will clear CMPA Register
    EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE; // This will clear CMPB Register

    EPwm1Regs.TBPRD = EPWM1_TIMER_TBPRD; // Set timer period
    EPwm1Regs.CMPA.bit.CMPA = 600 + EPWM1_CMPA_INT_CNT; // CMPRA=1us
    EPwm1Regs.CMPB.bit.CMPB = 600;
    EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up and down
    EPwm1Regs.TBCTL.bit.PHSDIR = TB_UP; // Count up when synchronization
    EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
    EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm1Regs.TBCTL.bit.SYNCOSEL=TB_CTR_ZERO;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm1Regs.AQCTLA.bit.CAU = AQ_NO_ACTION; // CNT = CMP up ->1
    EPwm1Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // CNT = CMP down ->no action
    EPwm1Regs.AQCTLA.bit.ZRO = AQ_CLEAR; // CNT = 0, -->0, Start the Logic ADC when counter reach zero

    EPwm1Regs.TBCTR = EPWM1_CMPA_INT_CNT+10; // Clear counter

    EPwm1Regs.ETPS.bit.SOCAPRD = ET_1ST; // One event will generate a SCOA pulse
    // EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTR_ZERO; // SOCA PULSE GENERAT A TB=0
    EPwm1Regs.ETSEL.bit.SOCASEL = ET_CTRU_CMPB;
    // EPwm1Regs.ETSEL.bit.SOCASELCMP = 0; // SOCA Plues Generate By CompareA
    EPwm1Regs.ETSEL.bit.SOCAEN = 1; // ENABLE SOCA PULSE
    // EPwm1Regs.ETCNTINITCTL.bit.SOCAINITEN = 0;

    EPwm1Regs.ETSEL.bit.INTSEL = ET_CTRU_CMPA; // INT when TB count up and TB=cmpra
    EPwm1Regs.ETSEL.bit.INTEN = 0; // Disable INT
    EPwm1Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1rd event

    EPwm1Regs.AQCTL.bit.SHDWAQAMODE = 1;
    EPwm1Regs.AQCTL.bit.LDAQAMODE = 1;
    EPwm1Regs.AQSFRC.bit.RLDCSF = 0; // the active register load on event counter equal to zero
    EPwm1Regs.AQCSFRC.bit.CSFA = FORCE_HIGH; // Software forcing disabled, i.e., has no effect
    EPwm1Regs.AQCSFRC.bit.CSFB = AQC_NO_ACTION;


    //EPWM2A --> INT2 Trigger //
    EALLOW;
    EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_HI; // Forced Hi (EPWM1A = High state)
    EPwm2Regs.TZFRC.bit.OST = 1; // Forces a fault on the OST latch and sets the OSTFLG bit.
    EDIS;
    EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE; // This will clear CMPA Register

    EPwm2Regs.TBPRD = EPWM2_TIMER_TBPRD; // Set timer period
    EPwm2Regs.CMPA.bit.CMPA = 600 + EPWM1_CMPA_INT_CNT; // CMPRA=1us
    EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up and down
    EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // Count up when synchronization
    EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
    EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW;
    EPwm2Regs.TBCTL.bit.SYNCOSEL=TB_CTR_ZERO;
    EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
    EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;

    EPwm2Regs.AQCTLA.bit.CAU = AQ_NO_ACTION; // CNT = CMP up ->1
    EPwm2Regs.AQCTLA.bit.CAD = AQ_NO_ACTION; // CNT = CMP down ->no action
    EPwm2Regs.AQCTLA.bit.ZRO = AQ_CLEAR; // CNT = 0, -->0, Start the Logic ADC when counter reach zero

    EPwm2Regs.TBCTR = EPWM2_TIMER_TBPRD+10; // Clear counter

    EPwm2Regs.ETSEL.bit.INTSEL = ET_CTRU_CMPA; // INT when TB count up and TB=cmpra
    EPwm2Regs.ETSEL.bit.INTEN = 0; // Disable INT
    EPwm2Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1rd event

    EPwm2Regs.AQCTL.bit.SHDWAQAMODE = 1;
    EPwm2Regs.AQCTL.bit.LDAQAMODE = 1;
    EPwm2Regs.AQSFRC.bit.RLDCSF = 0; // the active register load on event counter equal to zero
    EPwm2Regs.AQCSFRC.bit.CSFA = FORCE_HIGH;
  • 是否有可能是您的中断服务程序处理时间太长/中断频率太大,导致中断无法正常响应?您可以尝试减少EPWM2的中断频率试试
  • 所以多开中断与CLA是不会冲突的是吗?
  • 是的,两者是不会冲突的