This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

280049编译的 提示.text空间不够

Hi,

我在编译的时候出错,提示.text的section空间不够,提示空间需要0x453a,差不多17k空间,我看了280049的规格书中LS RAM总共才16k空间,不知道在我这种情况下,我应该怎么去分配text这个空间?

报错具体如下:

<a href="file:/D:/TI/ccs1011/ccs/tools/compiler/dmed/HTML/10099.html">#10099-D</a>  program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. placement with alignment/blocking fails for section ".text" size 0x453a page 0.  

规格书的存储空间如下:

  • 您可以在.text分配上合并LSRAM和 GSRAM
  • Hi Susan,

    GSRAM我大部分分配给了.ebss。

    我现在做了一个测试就是把flash_bank0分配给了.text,在运行程序发现无法正常控制EPWM模块。。不知道怎么回事。

    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN           	: origin = 0x000000, length = 0x000002
       RAMM0           	: origin = 0x0000F4, length = 0x00030C
    
       RAMLS0          	: origin = 0x008000, length = 0x000800
       RAMLS1          	: origin = 0x008800, length = 0x000800
       RAMLS2      		: origin = 0x009000, length = 0x000800
       RAMLS3      		: origin = 0x009800, length = 0x000800
       RAMLS4      		: origin = 0x00A000, length = 0x000800
       RESET           	: origin = 0x3FFFC0, length = 0x000002
    
     /* Flash sectors: you can use FLASH for program memory when the RAM is filled up*/
       /* BANK 0 */
       FLASH_BANK0_SEC0  : origin = 0x080000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000	/* on-chip Flash */
    
      /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000	/* on-chip Flash */
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
       RAMLS6      : origin = 0x00B000, length = 0x000800
       RAMLS7      : origin = 0x00B800, length = 0x000800
       
       RAMGS0      : origin = 0x00C000, length = 0x002000
       RAMGS1      : origin = 0x00E000, length = 0x002000
       RAMGS2      : origin = 0x010000, length = 0x002000
       RAMGS3      : origin = 0x012000, length = 0x001FF8
    //   RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    }
    
    /*You can arrange the .text, .cinit, .const, .pinit, .switch and .econst to FLASH when RAM is filled up.*/
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
       .TI.ramfunc      : > RAMM0,      PAGE = 0
    //   .text            : >> RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,   PAGE = 0
       .text            : >> FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4,   PAGE = 0
       .cinit           : > RAMM0,     PAGE = 0
       .switch          : > RAMM0,     PAGE = 0
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       .stack           : > RAMM1,     PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS5,     PAGE = 1
       .bss:output      : > RAMLS5,     PAGE = 1
       .init_array      : > RAMM0,      PAGE = 0
       .const           : > RAMLS5,     PAGE = 1
       .data            : > RAMLS5,     PAGE = 1
       .sysmem          : > RAMLS5,     PAGE = 1
       .bss:cio         : > RAMLS0,     PAGE = 0
    #else
       .pinit           : > RAMM0,      PAGE = 0
       .ebss            : > RAMLS5|RAMLS6|RAMLS7|RAMGS0|RAMGS1|RAMGS2,     PAGE = 1
       .econst          : > RAMGS3,     PAGE = 1
       .esysmem         : > RAMGS3,     PAGE = 1
       .cio             : > RAMGS3,     PAGE = 1
    #endif
    
       ramgs0           : > RAMGS0,    PAGE = 1
       ramgs1           : > RAMGS1,    PAGE = 1  
    }

  • Hi Susan,

    还有一个问题就是,我尝试给.ebss分配了RAMLS的空间,在编译的时候提示空间需要0X1148,差不多4k,但是实际上我给他分配了16k,为啥还是会提示空间不够呢?

    配置代码为:

    .ebss : > RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4 | RAMLS5 | RAMLS6 | RAMLS7, PAGE = 0

    报错描述为:

    <a href="file:/D:/TI/ccs1011/ccs/tools/compiler/dmed/HTML/10099.html">#10099-D</a> program will not fit into available memory, or the section contains a call site that requires a trampoline that can't be generated for this section. run placement with alignment/blocking fails for section ".ebss" size 0x1148page 0. 

    这个是哪里出了问题了?

  • 若是可以的话,请您私信一下工程吧,我们具体看一下,谢谢
  • 你好,我已经私信你了,请查收!
  • Hi Susan,我把.text的段分配到flash,然后再debug的时候,无法正常运行,提示错误为:
    Break at address "0x3fbd92" with no debug information available, or outside of program code.

    段配置如下:
    .text : >> FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC5, PAGE = 0, ALIGN(4)

    你也一起帮我看了,
    thanks!
  • 查看您的工程可以看到,您之前cmd的分配并没有成功

    而后我修改了一些,您可以看一下。编译后,就没有警告了

    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN           	: origin = 0x000000, length = 0x000002
       RAMM0           	: origin = 0x0000F4, length = 0x00030C
    
       RAMLS0          	: origin = 0x008000, length = 0x002000
     //  RAMLS1          	: origin = 0x008800, length = 0x000800
      // RAMLS2      		: origin = 0x009000, length = 0x000800
      // RAMLS3      		: origin = 0x009800, length = 0x000800
      // RAMLS4      		: origin = 0x00A000, length = 0x000800
       RESET           	: origin = 0x3FFFC0, length = 0x000002
    
     /* Flash sectors: you can use FLASH for program memory when the RAM is filled up*/
       /* BANK 0 */
       FLASH_BANK0_SEC0  : origin = 0x080000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC1  : origin = 0x081000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC2  : origin = 0x082000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC3  : origin = 0x083000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC4  : origin = 0x084000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC5  : origin = 0x085000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC6  : origin = 0x086000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC7  : origin = 0x087000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC8  : origin = 0x088000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC9  : origin = 0x089000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000	/* on-chip Flash */
    
      /* BANK 1 */
       FLASH_BANK1_SEC0  : origin = 0x090000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC1  : origin = 0x091000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC2  : origin = 0x092000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC3  : origin = 0x093000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC4  : origin = 0x094000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC5  : origin = 0x095000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC6  : origin = 0x096000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC7  : origin = 0x097000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC8  : origin = 0x098000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC9  : origin = 0x099000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000	/* on-chip Flash */
       FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000	/* on-chip Flash */
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x0000F1     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMLS5      : origin = 0x00A800, length = 0x000800
       RAMLS6      : origin = 0x00B000, length = 0x000800
       RAMLS7      : origin = 0x00B800, length = 0x000800
       
       RAMGS0      : origin = 0x00C000, length = 0x002000
       RAMGS1      : origin = 0x00E000, length = 0x002000
       RAMGS2      : origin = 0x010000, length = 0x002000
       RAMGS3      : origin = 0x012000, length = 0x001FF8
    //   RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    }
    
    /*You can arrange the .text, .cinit, .const, .pinit, .switch and .econst to FLASH when RAM is filled up.*/
    SECTIONS
    {
       codestart        : > BEGIN,     PAGE = 0
       .TI.ramfunc      : > RAMM0,      PAGE = 0
    //   .text            : >> RAMLS0 | RAMLS1 | RAMLS2 | RAMLS3 | RAMLS4,   PAGE = 0
    //   .text            : >> FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2 | FLASH_BANK0_SEC3 | FLASH_BANK0_SEC4,   PAGE = 0
       .text            : >> RAMLS5|RAMLS6|RAMLS7|RAMGS0|RAMGS1|RAMGS2,   PAGE = 1
       .cinit           : > RAMM0,     PAGE = 0
       .switch          : > RAMM0,     PAGE = 0
       .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */
    
       .stack           : > RAMM1,     PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS5,     PAGE = 1
       .bss:output      : > RAMLS5,     PAGE = 1
       .init_array      : > RAMM0,      PAGE = 0
       .const           : > RAMLS5,     PAGE = 1
       .data            : > RAMLS5,     PAGE = 1
       .sysmem          : > RAMLS5,     PAGE = 1
       .bss:cio         : > RAMLS0,     PAGE = 0
    #else
       .pinit           : > RAMM0,      PAGE = 0
    //   .ebss            : > RAMLS5|RAMLS6|RAMLS7|RAMGS0|RAMGS1|RAMGS2,     PAGE = 1
       .ebss            : > RAMLS0,     PAGE = 0
       .econst          : > RAMGS3,     PAGE = 1
       .esysmem         : > RAMGS3,     PAGE = 1
       .cio             : > RAMGS3,     PAGE = 1
    #endif
    
       ramgs0           : > RAMGS0,    PAGE = 1
       ramgs1           : > RAMGS1,    PAGE = 1  
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */
    

  • Hi Susan,
    我看你就是把LS0 1 2 3 4 合并在一起了。我按照你的写法改,空间确实分配开了,也可以debug,但是为什么合并就可以,分开就不行呢?
  • 此贴已结,我们将在下面的链接继续讨论后续问题

    e2echina.ti.com/.../198968