This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28377D CLA无法运行

专家好:
我用28377D做的自己程序,CPU2的CLA程序没有运行,没有查到原因,用例程和自己的程序在RAM仿真下是没有问题的,我的程序涉及到CLA的部分有以下内容:
在CPU1中
在CPU2中初始化CLA的部分见附件CLA_RUN.C  CPU2的CMD文件见附件
在CPU2的主程序中使用 Cla1ForceTask1andWait(); 会一直wait,感觉CLA没有运行起来
CCS设置了CPU2  —FLASH
麻烦专家给看看哪块设置有问题,谢谢
// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x100;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C

MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
          /* BEGIN is used for the "boot to Flash" bootloader mode   */

   BEGIN           	: origin = 0x080000, length = 0x000002
   RAMM0           	: origin = 0x000080, length = 0x000380
   RAMD0           	: origin = 0x00B000, length = 0x000800
   //RAMLS0          	: origin = 0x008000, length = 0x000800
   //RAMLS1          	: origin = 0x008800, length = 0x000800
   RAMLS2      		: origin = 0x009000, length = 0x000800
   RAMLS3      		: origin = 0x009800, length = 0x000800
   //RAMLS4      		: origin = 0x00A000, length = 0x000800
   RAMLS4_5         : origin = 0x00A000,   length = 0x001000

   RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15          : origin = 0x01B000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RESET       		: origin = 0x3FFFC0, length = 0x000002

   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */

PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

   BOOT_RSVD       : origin = 0x000002, length = 0x00007E     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   //RAMM0           : origin = 0x000080, length = 0x000380
   //RAMD0           : origin = 0x00B000, length = 0x000800
   RAMD1           : origin = 0x00B800, length = 0x000800
   RAMLS0          : origin = 0x008000, length = 0x000800
   RAMLS1          : origin = 0x008800, length = 0x000800

   //RAMLS5      : origin = 0x00A800, length = 0x000800

   RAMGS0          : origin = 0x00C000, length = 0x001000
   RAMGS1          : origin = 0x00D000, length = 0x001000

   RAMGS9      : origin = 0x015000, length = 0x001000
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11         : origin = 0x017000, length = 0x001000
   RAMGS12         : origin = 0x018000, length = 0x001000
   RAMGS13         : origin = 0x019000, length = 0x001000

   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400

   CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
   CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
}

SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHB      PAGE = 0, ALIGN(4)
   .pinit              : > FLASHB,     PAGE = 0, ALIGN(4)
   .text               : >> FLASHB | FLASHC | FLASHD | FLASHE     PAGE = 0, ALIGN(4)
   codestart           : > BEGIN       PAGE = 0, ALIGN(4)
   ramfuncs            : LOAD = FLASHD,
                         RUN =  RAMLS2 | RAMLS3,//RUN = RAMLS0 | RAMLS1 | RAMLS2,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)
						 
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1        PAGE = 1
   .ebss               : > RAMGS11       PAGE = 1
   .esysmem            : > RAMM1       PAGE = 1

   /* Initalized sections go in Flash */
   .econst             : > FLASHB      PAGE = 0, ALIGN(4)
   .switch             : > FLASHB      PAGE = 0, ALIGN(4)
   .reset           : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   twiddleFactors   : > RAMGS12,    PAGE = 1

   buffer1          : > RAMGS12, ALIGN = 256, PAGE = 1
   buffer2          : > RAMGS13, ALIGN = 256, PAGE = 1

   SHARERAMGS0		: > RAMGS0,		PAGE = 1
   SHARERAMGS1		: > RAMGS1,		PAGE = 1

   Cla1Prog    : LOAD = FLASHD,
                 RUN = RAMLS4_5,
                      LOAD_START(_Cla1funcsLoadStart),
                      LOAD_END(_Cla1funcsLoadEnd),
                      RUN_START(_Cla1funcsRunStart),
                      LOAD_SIZE(_Cla1funcsLoadSize),
                      PAGE = 0, ALIGN(4)

   CLADataLS0		: > RAMLS0, PAGE=1
   CLADataLS1		: > RAMLS1, PAGE=1

   Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW,   PAGE = 1
   CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH,  PAGE = 1

#ifdef __TI_COMPILER_VERSION
   #if __TI_COMPILER_VERSION >= 15009000
    .TI.ramfunc : {} LOAD = FLASHD,
                         RUN = RAMLS2 |RAMLS3,//RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)
   #else
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMLS2 |RAMLS3,//RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)
   #endif
#endif

   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        PUTBUFFER 
        PUTWRITEIDX 
        GETREADIDX 
    }

    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }

#ifdef CLA_C
   /* CLA C compiler sections */
   //
   // Must be allocated to memory the CLA has write access to
   //
   CLAscratch       :
                     { *.obj(CLAscratch)
                     . += CLA_SCRATCHPAD_SIZE;
                     *.obj(CLAscratch_end) } >  RAMLS1,  PAGE = 1

   .scratchpad      : > RAMLS1,       PAGE = 1
   .bss_cla		    : > RAMLS1,       PAGE = 1
   .const_cla	    :  LOAD = FLASHB,
                       RUN = RAMLS1,
                       RUN_START(_Cla1ConstRunStart),
                       LOAD_START(_Cla1ConstLoadStart),
                       LOAD_SIZE(_Cla1ConstLoadSize),
                       PAGE = 1
#endif //CLA_C
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/
CLA_RUN.C