This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C2000芯片SYS/BIOS 工程

哪位专家收有C2000系列芯片的SYS/BIOS工程,最好是F28377D芯片的。

谢谢

  • 我在之前的帖子已经给出了相关的回复

    e2echina.ti.com/.../198713

    另外请参考E2E上的相关帖子

    e2e.ti.com/.../880154

    e2e.ti.com/.../953170

    请问您现在是遇到什么问题了吗?
  • 你好,TI专家:

           谢谢你的指导,你给的BIOS的例程我找到了。

           我有不明白的地方是:在例程中怎么样在初始化中,添加对C2000系列芯片资源的调用与设置,如芯片时钟,EPWM外设等。我自己建立了一个工程,是在建立的简单的BIOS工程中添加了普通工程中能够正常运行的小程序。程序的设置为先初始化EPWM1,在EPWM1_INT(及计数值达到周期值时进入中断),验证中断计数器数值的正确性。正确的结果为second01值每约1秒。程序安排为先在main()中,InitSysCtrl()->InitGpio();->ConfigureEPWM();->BIOS_INIT->BIOS_start()->return(0)。硬件中断程序中epwm1_isr()。运行环境为CCS9.3,bios_6_83_00_18。

    运行结果为计数器second01无法正常增加,观察EPwm1Regs,出现了不希望的变换,如EPwm1Regs.TBPRD变化。

    麻烦你看看,问题出在哪儿。现将源代码发给你,可重点看main()文件。

    谢谢

    2541.LNPCSStandard.rar