This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于flash扇区问题,一个Sector范围是多少?

Other Parts Discussed in Thread: MOTORWARE

我看到F28027F的Flash:

Sector A(0x3F6000-0x3F7FFF)

Sector B(0x3F4000-0x3F5FFF)

Sector C(0x3F3000-0x3F3FFF)

Sector D(0x3F0000-0x3F1FFF)

1、那么我擦除Sector B,擦除范围是 0x3F4000-0x3F5FFF 吗?这样不是和其他几个Sector重复了吗?

2、我理解的Flash 扇区,是每个扇区互不相干的,地址不重复,但上面显示的每个Sector,都是地址重复的,我应该怎么理解?

3、另外,我只是想在片内的Flash,储存几个需要掉电记忆的参数,仅用到几个uint16的空间,我应该怎样使用Flash api?要全部擦除整个扇区再写入吗?

希望得到答复,万分感谢。

Best Regards!

  • 你好,这几个扇区都是独立的,没有重复啊,你是说哪里重复了?
    擦除扇区都是按一个扇区来擦除的,最小单位就是一个扇区,不能按bit擦除。
  • 明白了,之前看错,以为地址重复了。

    另外我用flash api编程,按例程配置PLL,测试flash PLL时,发现引脚输出的频率是30KHz,并不是10KHz。检查了PLL的配置,没有发现问题。可以帮我看看我哪里出错了吗?

    以下是程序:

    void HAL_setupClks(HAL_Handle handle)
    {
      HAL_Obj *obj = (HAL_Obj *)handle;
    
    
      // enable internal oscillator 1
      CLK_enableOsc1(obj->clkHandle);
    
      // set the oscillator source
      CLK_setOscSrc(obj->clkHandle,CLK_OscSrc_Internal);
    
      // disable the external clock in
      CLK_disableClkIn(obj->clkHandle);
    
      // disable the crystal oscillator
      CLK_disableCrystalOsc(obj->clkHandle);
    
      // disable oscillator 2
      CLK_disableOsc2(obj->clkHandle);
    
      // set the low speed clock prescaler
      CLK_setLowSpdPreScaler(obj->clkHandle,CLK_LowSpdPreScaler_SysClkOut_by_4);
    
      // set the clock out prescaler
      CLK_setClkOutPreScaler(obj->clkHandle,CLK_ClkOutPreScaler_SysClkOut_by_1);
    
      return;
    } // end of HAL_setupClks() function
    
    
    void HAL_setupPll(HAL_Handle handle,const PLL_ClkFreq_e clkFreq)
    {
      HAL_Obj *obj = (HAL_Obj *)handle;
    
    
      // make sure PLL is not running in limp mode
      if(PLL_getClkStatus(obj->pllHandle) != PLL_ClkStatus_Normal)
        {
          // reset the clock detect
          PLL_resetClkDetect(obj->pllHandle);
    
          // ???????
          asm("        ESTOP0");
        }
    
    
      // Divide Select must be ClkIn/4 before the clock rate can be changed
      if(PLL_getDivideSelect(obj->pllHandle) != PLL_DivideSelect_ClkIn_by_4)
        {
          PLL_setDivideSelect(obj->pllHandle,PLL_DivideSelect_ClkIn_by_4);
        }
    
    
      if(PLL_getClkFreq(obj->pllHandle) != clkFreq)
        {
          // disable the clock detect
          PLL_disableClkDetect(obj->pllHandle);
    
          // set the clock rate
          PLL_setClkFreq(obj->pllHandle,clkFreq);
        }
    
    
      // wait until locked
      while(PLL_getLockStatus(obj->pllHandle) != PLL_LockStatus_Done) {}
    
    
      // enable the clock detect
      PLL_enableClkDetect(obj->pllHandle);
    
    
      // set divide select to ClkIn/2 to get desired clock rate
      // NOTE: clock must be locked before setting this register
      PLL_setDivideSelect(obj->pllHandle,PLL_DivideSelect_ClkIn_by_2);
      //PLL_setDivideSelect(obj->pllHandle,PLL_DivideSelect_ClkIn_by_4);
    
      return;
    } // end of HAL_setupPll() function
    
    void HAL_setupPeripheralClks(HAL_Handle handle)
    {
      HAL_Obj *obj = (HAL_Obj *)handle;
    
    
      CLK_enableAdcClock(obj->clkHandle);
    
      CLK_enableCompClock(obj->clkHandle,CLK_CompNumber_1);
      CLK_enableCompClock(obj->clkHandle,CLK_CompNumber_2);
      CLK_enableCompClock(obj->clkHandle,CLK_CompNumber_3);
    
      CLK_enableEcap1Clock(obj->clkHandle);
    
      CLK_enablePwmClock(obj->clkHandle,PWM_Number_1);
      CLK_enablePwmClock(obj->clkHandle,PWM_Number_2);
      CLK_enablePwmClock(obj->clkHandle,PWM_Number_3);
      CLK_enablePwmClock(obj->clkHandle,PWM_Number_4);
    
      CLK_disableHrPwmClock(obj->clkHandle);
    
      CLK_disableI2cClock(obj->clkHandle);
    
      CLK_enableSciaClock(obj->clkHandle);
    
      CLK_enableSpiaClock(obj->clkHandle);
      
      CLK_enableTbClockSync(obj->clkHandle);
    
      CLK_enablePwmClock(obj->clkHandle,PWM_Number_4);  //cywen add
    
      return;
    } // end of HAL_setupPeripheralClks() function
    
    
    #define GPBMUX1 (volatile Uint32*)0x00006F98 // GPIO B mux 1
    #define GPBTOGGLE (volatile Uint32*)0x00006FCE // GPIO B toggle
    #define GPBDIR (volatile Uint32*)0x00006F9A // GPIO B dir
    #define GPIO32_MASK (Uint32)0x00000001 // GPIO32 mask
    
    
    void main(void)
    {
    
      // setup the clocks
      HAL_setupClks(handle);
    
    
      // Setup the PLL
      HAL_setupPll(handle,PLL_ClkFreq_60_MHz);
    
    
      // setup the PIE
      HAL_setupPie(handle);
    
    
      // run the device calibration
      HAL_cal(handle);
    
    
      // setup the peripheral clocks
      HAL_setupPeripheralClks(handle);
    
      Status = Example_CsmUnlock();
      if(Status != STATUS_SUCCESS)
      {
          //Example_Error(Status);
      }
    
      EALLOW;
      Flash_CPUScaleFactor = SCALE_FACTOR;
      EDIS;
    
      EALLOW;
      Flash_CallbackPtr = NULL;//&MyCallbackFunction;
      EDIS;
    
      //MyCallbackCounter = 0; // Increment this counter in the callback function
    
    // BEFORE calling the toggle test, configure the desired pin to be a GPIO
    // output pin. For this example, configure GPIO32 as a GPIO output
    
      EALLOW; // Macro for asm(“ EALLOW);
      *GPBMUX1 = 0x00000000; // All GPIO B pins are GPIO
      *GPBDIR = 0x00000001; // All GPIO B pins are outputs
      EDIS;
    
    // Call the Toggle Test function. This function will run forever
    // and will not exit.
      Flash_ToggleTest(GPBTOGGLE,GPIO32_MASK);
    
      // enable global interrupts
      HAL_enableGlobalInts(halHandle);
    
    
      // enable debug interrupts
      HAL_enableDebugInt(halHandle);
    }

  • 请问你这部分程序是参考了哪里的例程吗?我看不到里面具体的数值,不知道怎么配置的。
  • 是PLL配置是motorware里的lab05b例程,没做修改;其他flash配置参考了flash api例程;
    lab05b例程里,我看PLL配置看不错有什么问题,但运行Flash_ToggleTest(GPBTOGGLE,GPIO32_MASK);函数时,输出的PWM频率却是30kHz。
    希望可以得到解决,感谢。

    Best Regards
x 出现错误。请重试或与管理员联系。