This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

28035 HVPM_Enhanced_Sensorless - Settings.h 参数设置



在做无传感器控制时,修改电机参数,Base_Voltage 是说电机的额定电压峰值吗? 后面的Vdc/ 根号3是什么意思?
不太懂 这里的Base_Voltage 怎么取值

// Define the base quantites
#define BASE_VOLTAGE 236.14 // Base peak phase voltage (volt), Vdc/sqrt(3)
#define BASE_CURRENT 10 // Base peak phase current (amp), Max. measurable peak curr.
#define BASE_TORQUE // Base torque (N.m)
#define BASE_FLUX // Base flux linkage (volt.sec/rad)
#define BASE_FREQ 200 // Base electrical frequency (Hz)

  • 关于这几个量如何设置,请查看如下:

    // Define the base quantites
    #define BASE_VOLTAGE    236.140      // Base peak phase voltage (volt) //对应最大相电压,由电压采样电路决定,如VDCmax/3^0.5
    #define BASE_CURRENT    10              // 实际为最大电流,由板上电流采样电路硬件决定,对于TI高压电机套件,10A时对应到ADC输入管脚为3.3V或者0V,
    #define BASE_TORQUE                        // Base torque (N.m)
    #define BASE_FLUX                              // Base flux linkage (volt.sec/rad)
    #define BASE_FREQ       100                // Base electrical frequency (Hz),电机内电气频率,可以根据实际电机调整,如最大电机速度6000RPM,
    
                                                                   //可以这样设:BASE_FREQ=(6000/60)*Poles/2.

  • 你好,Base Voltage 对应最大相电压,这个并不是说电机的相电压最大值吗?(个人之前理解为电机额定电压(相电压)220V,则这个值设定为220×根号2)

    由电压采样电路决定,如VDCmax/3^0.5,这里的Vdc是什么可以阐述一下吗,以及/3 乘以0.5是为什么
  • Vdc的问题可以看一下这个帖子:e2echina.ti.com/.../129102
    至于/3^0.5,这里是指除以3的0.5次幂(根号打不出来),不是除以3再乘以0.5。