This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于DRV801供电范围与电机额定电压之间关系的问题

大家好,我设了一个DRV8301的三相桥电路

我的电机可能是额定电压24VDC或者48VDC的直流无刷机或者永磁同步机

DRV8301的供电我是直接从驱动桥母线取电的

我想请问大家,如果是额定电压48VDC的电机,用DRV8301驱动有可能会不太安全吗?因为DRV8301的供电范围是6V~60V

对于48VDC的系统,余量是不是小了一些。不过我的驱动管(MOSFET)选用的是VDS 100V的驱动管

对于48V的系统,是不是选用DRV8353更安全一些呢?

我目前设计的DRV8301+100V VDS MOSFET驱动48VDC额定电压的永磁同步机或者直流无刷机会有问题吗?

麻烦大家指点下 多谢

这个帖子也发到 “其他模拟产品” 的论坛了