This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AdcRegs.INTSEL1N2.bit.INT1SEL寄存器设置是7一切正常,设为8,ADC没有中断是为什么

AdcRegs.INTSEL1N2.bit.INT1SEL = 8; //setup EOC5 to trigger ADCINT1 to fire,SOC5转换完成产生中断

AdcRegs.ADCSAMPLEMODE.bit.SIMULEN0 = 0; //SOC0,SOC1 SEQUENTIAL Sampling Enable //顺序采样
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN2 = 0; //SOC2,SOC3 SEQUENTIAL Sampling Enable
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN4 = 0; //SOC4,SOC5 SEQUENTIAL Sampling Enable
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN6 = 0;
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN8 = 0;


AdcRegs.ADCSOC0CTL.bit.CHSEL = 7; //SOC0 ADCINA1 //ADCINA7

AdcRegs.ADCSOC1CTL.bit.CHSEL = 8; //SOC0 ADCINA1 //ADCINB0
AdcRegs.ADCSOC2CTL.bit.CHSEL = 9; //SOC0 ADCINA1 //ADCINB1
AdcRegs.ADCSOC3CTL.bit.CHSEL = 10; //SOC0 ADCINA1 //ADCINB2
AdcRegs.ADCSOC4CTL.bit.CHSEL = 11; //SOC0 ADCINA1 //ADCINB3
AdcRegs.ADCSOC5CTL.bit.CHSEL = 12; //SOC0 ADCINA1 //ADCINB4
AdcRegs.ADCSOC6CTL.bit.CHSEL = 14; //SOC0 ADCINA1 //ADCINB6
AdcRegs.ADCSOC7CTL.bit.CHSEL = 15; //SOC0 ADCINA1 //ADCINB7

AdcRegs.ADCSOC8CTL.bit.CHSEL = 6; //ADCINA6

AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC3CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC4CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC5CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC6CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC7CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only
AdcRegs.ADCSOC8CTL.bit.TRIGSEL = 0x00; //ADCTRIG0- Software only

//Sample window is 7 cycles long (6 + 1 clock cycles).
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC3CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC4CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC5CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC6CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC7CTL.bit.ACQPS = 6;
AdcRegs.ADCSOC8CTL.bit.ACQPS = 6;

  • 你好,还请说明一下使用的是哪款芯片?
  • TMS320F2803x 我想知道为什么会发生这种情况,还有如果设置SOC8,应该怎么修改,谢谢
  • 尝试一下把上述程序

    user6620123 说:

    AdcRegs.ADCSOC0CTL.bit.CHSEL = 7; //SOC0 ADCINA1 //ADCINA7

    AdcRegs.ADCSOC1CTL.bit.CHSEL = 8; //SOC0 ADCINA1 //ADCINB0
    AdcRegs.ADCSOC2CTL.bit.CHSEL = 9; //SOC0 ADCINA1 //ADCINB1
    AdcRegs.ADCSOC3CTL.bit.CHSEL = 10; //SOC0 ADCINA1 //ADCINB2
    AdcRegs.ADCSOC4CTL.bit.CHSEL = 11; //SOC0 ADCINA1 //ADCINB3
    AdcRegs.ADCSOC5CTL.bit.CHSEL = 12; //SOC0 ADCINA1 //ADCINB4
    AdcRegs.ADCSOC6CTL.bit.CHSEL = 14; //SOC0 ADCINA1 //ADCINB6
    AdcRegs.ADCSOC7CTL.bit.CHSEL = 15; //SOC0 ADCINA1 //ADCINB7

    AdcRegs.ADCSOC8CTL.bit.CHSEL = 6; //ADCINA6

    替换成

    AdcRegs.ADCSOC0CTL.bit.CHSEL = 7; 
    
    AdcRegs.ADCSOC1CTL.bit.CHSEL = 7; 
    AdcRegs.ADCSOC2CTL.bit.CHSEL = 8; 
    AdcRegs.ADCSOC3CTL.bit.CHSEL = 9; 
    AdcRegs.ADCSOC4CTL.bit.CHSEL = 10; 
    AdcRegs.ADCSOC5CTL.bit.CHSEL = 11; 
    AdcRegs.ADCSOC6CTL.bit.CHSEL = 12; 
    AdcRegs.ADCSOC7CTL.bit.CHSEL = 14; 
    
    AdcRegs.ADCSOC8CTL.bit.CHSEL = 15; 

    测试一下是否有效。其他问题暂时没看出来

  • 如果方便的话可以把工程转压缩文件后上传一下