This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

我是新手,刚学CLA模块,遇到一个问题:为什么28379D的CLA例程cla_fir32_cpu01中的任务cla1Task1只能触发一次,第二次就触发不了,而程序中是循环触发了133次?希望大佬们不吝赐教,跪谢!

还有就是,明明程序中给CLA申请LS5作为程序空间,为什么CLA程序运行时的起始地址是LS4?是例程错了吗?

  • 请问您是如何调试的?能否给出相关截图?

    请您先参考下:

    software-dl.ti.com/.../debugging.html

    software-dl.ti.com/.../getting_started.html

    在cmd文件中,

    RAMLS4_5 : origin = 0x00A000, length = 0x001000

    /* CLA specific sections */
    Cla1Prog : > RAMLS4_5, PAGE=0

    关于此,您可以看一下数据手册的 表 6-1. C28x Memory Map

    www.ti.com.cn/.../tms320f28379d.pdf
  • 多谢解惑,十分抱歉,我用的公司电脑,不能上传图片。。
    我采用单步调试,程序采用循环的方式重发触发任务1,第一次任务1运行完成,MIRUN[0]变为0后,第二次触发任务1,对应的MIFR和MIER相应的位都置1了,且CLA处于空闲状态,但是CLA就是不会再次运行任务1.
  • 请问在cmd文件中
    RAMLS4_5 : origin = 0x00A000, length = 0x001000

    /* CLA specific sections */
    Cla1Prog : > RAMLS4_5, PAGE=0
    对应的程序存放空间是不是LS4?但是例程中是将LS5分配位CLA的程序空间,我不清楚是例程出错了,还是我理解出错了
    例程中相关程序是这样的:
    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;
  • 我测试了一下程序是可以正常运行的,如下图:

    所以建议您还是按照之前链接的调试说明来调试一下

    user6574429 说:
    /* CLA specific sections */
    Cla1Prog : > RAMLS4_5, PAGE=0
    对应的程序存放空间是不是LS4?但是例程中是将LS5分配位CLA的程序空间,我不清楚是例程出错了,还是我理解出错了
    例程中相关程序是这样的:
    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;

    参考程序内说明

        //
        // Select LS4RAM and LS5RAM to be the programming space for the CLA
        // First configure the CLA to be the master for LS4 and LS5 and then
        // set the space to be a program block
        //
        MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
        MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;
        MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;
        MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;

    在cmd文件内将LS4 LS5合并了,但是在c文件内,LS4 LS5的设置是分开的,如上面的语句

    其实均表示使用的地址是 RAMLS4_5定义的地址范围

  • 你好,非常感谢你的回复,我想问一下你运行程序的时候CLA的任务1执行了多少次?我的只执行了一次就不执行了,而且例程里只有MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;
    LS5的内存分配。
  • clar任务执行了多次

    在cla_fir32_cpu01.c的void CLA_configClaMemory(void)内的341到344行

    //
    // Select LS4RAM and LS5RAM to be the programming space for the CLA
    // First configure the CLA to be the master for LS4 and LS5 and then
    // set the space to be a program block
    //
    MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;
    MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;
    MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;
  • 请问每次进入CLA程序都会停在__mdebugstop()吗?我的是第一次进入时停在这,然后单步调试至MSTOP后就再也没进入CLA的任务1了
    但是CLA中的寄存器是这样的
  • 您好,能分享一下CMD文件吗?我看一下是否是我的CMD文件有错?
  • “请问每次进入CLA程序都会停在__mdebugstop()吗?”

    是的

    // The user must define CLA_C in the project linker settings if using the
    // CLA C compiler
    // Project Properties -> C2000 Linker -> Advanced Options -> Command File
    // Preprocessing -> --define
    #ifdef CLA_C
    // Define a size for the CLA scratchpad area that will be used
    // by the CLA compiler for local symbols and temps
    // Also force references to the special symbols that mark the
    // scratchpad are.
    CLA_SCRATCHPAD_SIZE = 0x100;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start
    #endif //CLA_C
    
    MEMORY
    {
    PAGE 0 :
       /* BEGIN is used for the "boot to SARAM" bootloader mode   */
    
       BEGIN           	: origin = 0x000000,   length = 0x000002
       RAMM0           	: origin = 0x000123,   length = 0x0002DD
       RAMD0           	: origin = 0x00B000,   length = 0x000800
       RAMD1            : origin = 0x00B800,   length = 0x000800
       /* RAMLS4      	    : origin = 0x00A000, length = 0x000800 */
       /* RAMLS5           : origin = 0x00A800, length = 0x000800 */
       RAMLS4_5         : origin = 0x00A000,   length = 0x001000
       RESET           	: origin = 0x3FFFC0,   length = 0x000002
    
    PAGE 1 :
    
       BOOT_RSVD       : origin = 0x000002, length = 0x000121     /* Part of M0, BOOT rom will use this for stack */
       RAMM1           : origin = 0x000400, length = 0x0003F8     /* on-chip RAM block M1 */
    //   RAMM1_RSVD      : origin = 0x0007F8, length = 0x000008     /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
       RAMLS0          	: origin = 0x008000,   length = 0x000800
       RAMLS1          	: origin = 0x008800,   length = 0x000800
       RAMLS2      		: origin = 0x009000,   length = 0x000800
       RAMLS3      		: origin = 0x009800,   length = 0x000800
    
       RAMGS0           : origin = 0x00C000,   length = 0x001000
       RAMGS1           : origin = 0x00D000,   length = 0x001000
       RAMGS2           : origin = 0x00E000,   length = 0x001000
       RAMGS3           : origin = 0x00F000,   length = 0x001000
       RAMGS4           : origin = 0x010000,   length = 0x001000
       RAMGS5           : origin = 0x011000,   length = 0x001000
       RAMGS6           : origin = 0x012000,   length = 0x001000
       RAMGS7           : origin = 0x013000,   length = 0x001000
       RAMGS8           : origin = 0x014000,   length = 0x001000
       RAMGS9           : origin = 0x015000,   length = 0x001000
       RAMGS10          : origin = 0x016000,   length = 0x001000
    
    //   RAMGS11     : origin = 0x017000, length = 0x000FF8   /* Uncomment for F28374D, F28376D devices */
    
    //   RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
    
       RAMGS11          : origin = 0x017000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS12          : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS13          : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS14          : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
       RAMGS15          : origin = 0x01B000, length = 0x000FF8     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
    
    //   RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008    /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
                                                                /* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */
    
       EMIF1_CS0n       : origin = 0x80000000, length = 0x10000000
       EMIF1_CS2n       : origin = 0x00100000, length = 0x00200000
       EMIF1_CS3n       : origin = 0x00300000, length = 0x00080000
       EMIF1_CS4n       : origin = 0x00380000, length = 0x00060000
       EMIF2_CS0n       : origin = 0x90000000, length = 0x10000000
       EMIF2_CS2n       : origin = 0x00002000, length = 0x00001000
    
       CANA_MSG_RAM     : origin = 0x049000,   length = 0x000800
       CANB_MSG_RAM     : origin = 0x04B000,   length = 0x000800
    
       CLA1_MSGRAMLOW   : origin = 0x001480,   length = 0x000080
       CLA1_MSGRAMHIGH  : origin = 0x001500,   length = 0x000080
    }
    
    SECTIONS
    {
       codestart        : > BEGIN,      PAGE = 0
       .text            : >> RAMD0 | RAMD1 | RAMLS4_5,    PAGE = 0
       .cinit           : > RAMM0,      PAGE = 0
       .switch          : > RAMM0,      PAGE = 0
       .reset           : > RESET,      PAGE = 0, TYPE = DSECT /* not used, */
       .stack           : > RAMM1,      PAGE = 1
    
    #if defined(__TI_EABI__)
       .bss             : > RAMLS2,    PAGE = 1
       .bss:output      : > RAMLS2,    PAGE = 1
       .init_array      : > RAMM0,     PAGE = 0
       .const           : > RAMLS3,    PAGE = 1
       .data            : > RAMLS3,    PAGE = 1
       .sysmem          : > RAMLS3,    PAGE = 1
    #else
       .pinit           : > RAMM0,     PAGE = 0
       .ebss            : > RAMLS2,    PAGE = 1
       .econst          : > RAMLS3,    PAGE = 1
       .esysmem         : > RAMLS3,    PAGE = 1
    #endif
       Filter_RegsFile  : > RAMGS0,	    PAGE = 1
    
       .em1_cs0         : > EMIF1_CS0n, PAGE = 1
       .em1_cs2         : > EMIF1_CS2n, PAGE = 1
       .em1_cs3         : > EMIF1_CS3n, PAGE = 1
       .em1_cs4         : > EMIF1_CS4n, PAGE = 1
       .em2_cs0         : > EMIF2_CS0n, PAGE = 1
       .em2_cs2         : > EMIF2_CS2n, PAGE = 1
    
        /* CLA specific sections */
       Cla1Prog         : > RAMLS4_5, PAGE=0
    
       CLADataLS0		: > RAMLS0, PAGE=1
       CLADataLS1		: > RAMLS1, PAGE=1
    
       Cla1ToCpuMsgRAM  : > CLA1_MSGRAMLOW,   PAGE = 1
       CpuToCla1MsgRAM  : > CLA1_MSGRAMHIGH,  PAGE = 1
    
       /* The following section definition are for SDFM examples */
       Filter1_RegsFile : > RAMGS1,	PAGE = 1, fill=0x1111
       Filter2_RegsFile : > RAMGS2,	PAGE = 1, fill=0x2222
       Filter3_RegsFile : > RAMGS3,	PAGE = 1, fill=0x3333
       Filter4_RegsFile : > RAMGS4,	PAGE = 1, fill=0x4444
    
    #ifdef __TI_COMPILER_VERSION__
       #if __TI_COMPILER_VERSION__ >= 15009000
        .TI.ramfunc : {} > RAMM0,      PAGE = 0
       #else
        ramfuncs    : > RAMM0      PAGE = 0   
       #endif
    #endif
    
    #ifdef CLA_C
       /* CLA C compiler sections */
       //
       // Must be allocated to memory the CLA has write access to
       //
       CLAscratch       :
                         { *.obj(CLAscratch)
                         . += CLA_SCRATCHPAD_SIZE;
                         *.obj(CLAscratch_end) } >  RAMLS1,  PAGE = 1
    
       .scratchpad      : > RAMLS1,       PAGE = 1
       .bss_cla		    : > RAMLS1,       PAGE = 1
       .const_cla	    : > RAMLS1,       PAGE = 1
    #endif //CLA_C
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */