This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280021: 关于TMS320F280021问题请教

Part Number: TMS320F280021

     你好!

     我们目前打算使用TMS320F280021,LQFP48封装,在设计原理图中,有以下问题请教:

1、官网提供的MCU089A(001).PDF, (280025开发版原理图)中,调试引脚如下,是不是不需要接TDO,TDI这两个引脚,只需要TMS,TCK,GND这3个引脚,就可以使用ccs+XDS110调试了?  这种调试方法,和以前C2000系列mcu,比如28034必须要用TDO,TDI之类,有什么使用上的注意事项吗?(因为想将TDO,TDI引脚配置为CAN 通讯引脚)

2、启动方式选择从内部flash启动,是否必须要在上电的时候,硬件GPIO24,GPIO32为高电平,能否在程序内写某个寄存器固定从内部flash启动不需要管上电时GPIO24与32的电平。

3、INPUT X-BAR与GPIO1-x,是可以任意组合的吧? 比如程序里可以配置INPUT 1 X-BAR连接GPIO33?