Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE,
TMS320F28335debug时报错如下:
C28xx: Failed CPU Reset: (Error -1041 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00032)
C28xx: Trouble Reading Register PC: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.3.0.00032)
C28xx: Trouble Reading Register PC: (Error -1041 @ 0x0) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.3.0.00032)
C28xx: Error occurred during flash operation: CPU Reset error. Error code -1
C28xx: Can't Run Target CPU: (Error -1140 @ 0x3399AD) Lost debug connection to device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.3.0.00032)
C28xx: Flash Programmer: Error encountered when writing to flash memory
C28xx: File Loader: Memory write failed: Unknown error
已确认仿真器连接成功,在ccxml文件中,test connection选项测试是succeed
这是我点launch之后的情况