This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: EPwm submodule Trip-Zone

Part Number: TMS320F28035


想请问一下目前TripZone功能使用上碰到点问题

目前在TZ中断里面去清TZCLR[CBC],却不见效果(确实有进入中断)
只能等CTR=zero 去CLEAR
有叫出Expressions去看内部站存器没有发生变化

请问这有办法解决吗

 

  • 你好,我看你的程序应该是根据例程的基础修改的?例程中pwm1的配置是单次触发模式,不知道你的程序中有没有做相应的更改?或者,你的程序有做过其他修改吗?

  • 我是从这份例程去进行修改的Example_2803xEPwmDCEventTripComp
    想把OST改成CBC模式

    有对程式做出一些修改
    目前一定要等CTR=zero才能清除,没办法手动清除

    下面是目前TZ部分的程式码


    EALLOW;

    // Define an event (DCAEVT1) based on TZ1 and TZ2
    EPwm1Regs.DCTRIPSEL.bit.DCALCOMPSEL = DC_COMP1OUT; // DCAL = Comparator 1 output

    // EPwm1Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAL_LOW; // DCAEVT2 = DCAL low(will become active as Comparator output goes low)

    EPwm1Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // DCAEVT2 = DCAEVT2 (not filtered)
    EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // Take async path

    EPwm1Regs.TZSEL.bit.DCAEVT2 = 1;

    EPwm1Regs.TZCTL.bit.TZA= TZ_FORCE_LO; // EPWM1A will go high
    EPwm1Regs.TZCTL.bit.TZB = TZ_NO_CHANGE; // EPWM1B will go low

    EPwm1Regs.TZEINT.bit.CBC = 1;

    EPwm2Regs.DCTRIPSEL.bit.DCALCOMPSEL = DC_COMP1OUT; // DCAL = Comparator 1 output

    EPwm2Regs.TZDCSEL.bit.DCAEVT1 = TZ_DCAL_LOW; // DCAEVT2 = DCAH low(will become active as Comparator output goes low)

    EPwm2Regs.DCACTL.bit.EVT2SRCSEL = DC_EVT2; // DCAEVT1 = DCAEVT2 (not filtered)
    EPwm2Regs.DCACTL.bit.EVT2FRCSYNCSEL = DC_EVT_ASYNC; // Take async path

    EPwm2Regs.TZSEL.bit.DCAEVT2 = 1;

    EPwm2Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWM2A will NO CHANGE
    EPwm2Regs.TZCTL.bit.TZB = TZ_NO_CHANGE; // EPWM2B will NO CHANGE

    EPwm3Regs.DCTRIPSEL.bit.DCALCOMPSEL = DC_COMP1OUT; // DCAH = Comparator 1 output
    EPwm3Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_LOW; // DCAEVT2 = DCAH low(will become active as Comparator output goes low)
    EPwm3Regs.DCACTL.bit.EVT1SRCSEL = DC_EVT2; // DCAEVT2 = DCAEVT2 (not filtered)
    EPwm3Regs.DCACTL.bit.EVT1FRCSYNCSEL = DC_EVT_ASYNC; // Take async path

    EPwm3Regs.TZSEL.bit.DCAEVT2 = 1;

    EPwm3Regs.TZCTL.bit.TZA = TZ_FORCE_LO; // EPWM3A will NO CHANGE
    EPwm3Regs.TZCTL.bit.TZB = TZ_NO_CHANGE; // EPWM3B will NO CHANGE

    EDIS;

  • 我觉得这个现象是正常的,因为 CBC Latch只能在 CTR = ZERO时自动清除。而你通过TZCLR[CRC]清除的只是TZFLG,当CTR还没到ZERO时,CBC Latch是依然存在的,就算你通过TZCLR[CRC]清除了是一下TZFLG,马上又会置1,所以你看到操作不成功是正常的。

    记住:CBC Latch这个事件锁存只有在外部TZ条件已经消失,CTR=ZERO才会被自动解锁。