Part Number: TMS320F28335
例程中的相电流采样

最后计算出的clarke1.As的结果乘以电流基值BASE_CURRENT就是实际的相电流么
同样的直流母线电压也是乘以电压基值BASE_VOLTAGE就是实际的母线电压么??

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28335
例程中的相电流采样

最后计算出的clarke1.As的结果乘以电流基值BASE_CURRENT就是实际的相电流么
同样的直流母线电压也是乘以电压基值BASE_VOLTAGE就是实际的母线电压么??

不是的,你看一下这个帖子里面对几个基值的说明:e2echina.ti.com/.../28035-hvpm_enhanced_sensorless---settings-h
还有个问题

例程中的clarke1.As与clarke1.Bs分别是电机的A相与B相电流还是任意两相电流
可以看一下clarke.h中的定义:
typedef struct { _iq As; // Input: phase-a stator variable
_iq Bs; // Input: phase-b stator variable
_iq Cs; // Input: phase-c stator variable
_iq Alpha; // Output: stationary d-axis stator variable
_iq Beta; // Output: stationary q-axis stator variable
} CLARKE;
关于速度估算模块,这个speed3.BaseRpm乘以SpeedRef就是电机的实际转速么