This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: 咨询关于F2837x的CAN模块中关于过滤的问题

Part Number: TMS320F28377D


TI工程师你好!
请问一下:
1、CAN_IF1MSK寄存器中MXtd的含义是不是:当为扩展帧时,如果需要过滤ID[28:0],那么必须将该位置位,然后再和Msk[28:0]进行
过滤?当为标准帧时,如果需要过滤ID,MXtd为就设置为0,只需要将Msk[28:18]进行相应的配置,Msk[17:0]保持为0,这样就可以对
ID[28:18]进行过滤了?
2、CAN_IF1MSK寄存器中MDir的含义是什么呢?不知道怎么使用,如果我设置了MDir为1,有什么效果呢?