This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 库加载出现的问题

Part Number: TMS320F28335

<a href="file:/D:/TI/CCS/ccs/tools/compiler/dmed/HTML/16008.html">#16008-D</a>  file "D:/TI/CCS/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/lib/rts2800_ml.lib<memcpy.c.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
<a href="file:/D:/TI/CCS/ccs/tools/compiler/dmed/HTML/16008.html">#16008-D</a>  file "D:/TI/CCS/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/lib/rts2800_ml.lib<_lock.c.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line

加载rts2800_ml.lib库时编译出现这些问题如何解决

  • 这个帖子对应的操作,我已经尝试过,并且,只是添加了这个库之后出现这个报错,代码工程都是新建的,编译无错误警告,就是添加这个库之后出现的错误

  • 完整报错如下:

    error #16008-D: file "./main.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line
    error #16008-D: file "./bsp/bsp.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./bsp/sci/sci_fifo.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_ADC_cal.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Adc.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_CodeStartBranch.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_CpuTimers.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_DBGIER.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_DMA.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_DefaultIsr.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_DisInt.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_ECan.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_ECap.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_EPwm.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_EQep.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Gpio.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_I2C.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Mcbsp.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_MemCopy.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_PieCtrl.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_PieVect.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Sci.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Spi.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_SysCtrl.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_Xintf.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "./source/DSP2833x_usDelay.obj" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    error #16008-D: file "D:/TI/CCS/ccs/tools/compiler/ti-cgt-c2000_20.2.2.LTS/lib/rts2800_ml.lib<memset.c.obj>" specifies ISA revision "C2800", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line
    "../F28335.cmd", line 65: warning #10068-D: no matching section
    "../F28335.cmd", line 66: warning #10068-D: no matching section
    error #10010: errors encountered during linking; "IAP_BOOT.out" not built

    >> Compilation failure
    makefile:179: recipe for target 'IAP_BOOT.out' failed
    gmake[1]: *** [IAP_BOOT.out] Error 1
    makefile:175: recipe for target 'all' failed
    gmake: *** [all] Error 2

    **** Build Finished ****

  • 感谢你,我已经解决这个问题了,现在有出现一个新的问题,在生成BIN文件的时候,警告如下:
    warning: section IAP_APP.out(.econst) at 0630000h falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(.text) at 0640000h falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(ramfuncs) at 0640f58h falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(.cinit) at 0650000h falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(csm_rsvd) at 066ff00h falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(codestart) at 066ffech falls in unconfigured memory (skipped)
    warning: section IAP_APP.out(csmpasswds) at 066fff0h falls in unconfigured memory (skipped)

  • 感谢你,我已经解决这个问题了

    谢谢反馈

    现在有出现一个新的问题,在生成BIN文件的时候,警告如下:

    新问题的话,请您详细说明后,发新帖,谢谢

  • https://e2echina.ti.com/support/microcontrollers/c2000/f/c2000-microcontrollers-forum/206276/tms320f28335-bin新问题链接如下

  • 好的,我来看一下