This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,现在我手上有一个有一个LAUNCHXL-F280025C开发板,改了很多次程序都没有CAN信号输出,示例程序用过也不行,想问一下你们这边有没有程序只要能实现ftcan发的信号can卡能收到,can卡发的信号板子能收到,内容无所谓
该板子是有板载CAN收发器的
can卡
您指的是USB-CAN转换器?那您可以参考f2837xd的例程,can_ex4_simple_transmit 和can_ex5_simple_receive
C:\ti\c2000\C2000Ware_3_04_00_00\driverlib\f2837xd\examples\cpu1\can
下面是我使用USB-CAN和28379D launchpad通信成功的截图
...
谢谢您的回复,应该是我表述的有些问题,我现在遇到的问题是开发板没有CAN信号输出,上位机与板子无法通讯,示例1到示例4都用过,用示波器测出来只是一个电平,想问一下你们这边有程序只需要CAN 信号能够接受和发送即可,内容无所谓。
我现在遇到的问题是开发板没有CAN信号输出,上位机与板子无法通讯,
我有些没太理解您的意思。请问您现在硬件部分以及相关连接是怎么样的呢?能否给出拍照或截图?