This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应用I2C怎么进行读写,发送帧应包括 :从机地址-内存地址高-内存地址低-数据
从机地址: I2C_setSlaveAddress(I2C0_BASE,SLAVE_ADDRESS_Write>>1,I2C_MASTER_WRITE);这样发送对不?
内存地址高:
内存地址低:我不知道怎么配置,
发送数据:I2C_putMasterData(I2C0_BASE, 0x0F); I2C_setMasterConfig(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);不知道对不对,每次发送都要写I2C_setMasterConfig(I2C0_BASE, I2C_MASTER_CMD_SINGLE_SEND);吗;
0049CPU的I2C写操作:
p->pI2cRegs->I2CCNT = 2 + p->Txd_num; //Txd_num < 8; 在CM中怎么体现,如何实现多数据发送
p->pI2cRegs->I2CFFTX.bit.TXFFRST = 1;
p->pI2cRegs->I2CDXR.all= p->Addr >> 8;
p->pI2cRegs->I2CDXR.all = p->Addr & 0x00FF;
for (i = 0; i < p->Txd_num; i++) p->pI2cRegs->I2CDXR.all = p->Msg_Buff[i];
p->pI2cRegs->I2CMDR.all = 0x6E20;
目前还没有,我在E2E上发帖了,您可以跟踪一下
https://e2e.ti.com/support/microcontrollers/c2000-microcontrollers-group/c2000/f/c2000-microcontrollers-forum/1028768/tms320f28388d-i2c-registers
//############################################################################# // // FILE: cm_common_config_c28x.c // // TITLE: C28x Common Configurations to be used for the CM Side. // //! \addtogroup driver_example_list //! <h1>C28x Common Configurations</h1> //! //! This example configures the GPIOs and Allocates the shared peripherals //! according to the defines selected by the users. //! // //############################################################################# // $TI Release: F2838x Support Library v3.04.00.00 $ // $Release Date: Fri Feb 12 19:08:49 IST 2021 $ // $Copyright: // Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/ // // Redistribution and use in source and binary forms, with or without // modification, are permitted provided that the following conditions // are met: // // Redistributions of source code must retain the above copyright // notice, this list of conditions and the following disclaimer. // // Redistributions in binary form must reproduce the above copyright // notice, this list of conditions and the following disclaimer in the // documentation and/or other materials provided with the // distribution. // // Neither the name of Texas Instruments Incorporated nor the names of // its contributors may be used to endorse or promote products derived // from this software without specific prior written permission. // // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. // $ //############################################################################# // // Included Files // #include "driverlib.h" #include "device.h" void main(void) { // // Initialize device clock and peripherals // Device_init(); // // Boot CM core // #ifdef _FLASH Device_bootCM(BOOTMODE_BOOT_TO_FLASH_SECTOR0); #else Device_bootCM(BOOTMODE_BOOT_TO_S0RAM); #endif // // Disable pin locks and enable internal pull-ups. // Device_initGPIO(); #ifdef ETHERNET // // Set up EnetCLK to use SYSPLL as the clock source and set the // clock divider to 2. // // This way we ensure that the PTP clock is 100 MHz. Note that this value // is not automatically/dynamically known to the CM core and hence it needs // to be made available to the CM side code beforehand. SysCtl_setEnetClk(SYSCTL_ENETCLKOUT_DIV_2, SYSCTL_SOURCE_SYSPLL); // // Configure the GPIOs for ETHERNET. // // // MDIO Signals // GPIO_setPinConfig(GPIO_105_ENET_MDIO_CLK); GPIO_setPinConfig(GPIO_106_ENET_MDIO_DATA); // // Use this only for RMII Mode //GPIO_setPinConfig(GPIO_73_ENET_RMII_CLK); // // //MII Signals // GPIO_setPinConfig(GPIO_109_ENET_MII_CRS); GPIO_setPinConfig(GPIO_110_ENET_MII_COL); GPIO_setPinConfig(GPIO_75_ENET_MII_TX_DATA0); GPIO_setPinConfig(GPIO_122_ENET_MII_TX_DATA1); GPIO_setPinConfig(GPIO_123_ENET_MII_TX_DATA2); GPIO_setPinConfig(GPIO_124_ENET_MII_TX_DATA3); // //Use this only if the TX Error pin has to be connected //GPIO_setPinConfig(GPIO_46_ENET_MII_TX_ERR); // GPIO_setPinConfig(GPIO_118_ENET_MII_TX_EN); GPIO_setPinConfig(GPIO_114_ENET_MII_RX_DATA0); GPIO_setPinConfig(GPIO_115_ENET_MII_RX_DATA1); GPIO_setPinConfig(GPIO_116_ENET_MII_RX_DATA2); GPIO_setPinConfig(GPIO_117_ENET_MII_RX_DATA3); GPIO_setPinConfig(GPIO_113_ENET_MII_RX_ERR); GPIO_setPinConfig(GPIO_112_ENET_MII_RX_DV); GPIO_setPinConfig(GPIO_44_ENET_MII_TX_CLK); GPIO_setPinConfig(GPIO_111_ENET_MII_RX_CLK); // //Power down pin to bring the external PHY out of Power down // GPIO_setDirectionMode(108, GPIO_DIR_MODE_OUT); GPIO_setPadConfig(108, GPIO_PIN_TYPE_PULLUP); GPIO_writePin(108,1); // //PHY Reset Pin to be driven High to bring external PHY out of Reset // GPIO_setDirectionMode(119, GPIO_DIR_MODE_OUT); GPIO_setPadConfig(119, GPIO_PIN_TYPE_PULLUP); GPIO_writePin(119,1); #endif #ifdef MCAN // // Setting the MCAN Clock. // SysCtl_setMCANClk(SYSCTL_MCANCLK_DIV_4); // // Configuring the GPIOs for MCAN. // GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANRXA); GPIO_setPinConfig(DEVICE_GPIO_CFG_MCANTXA); #endif #ifdef CANA // // Configuring the GPIOs for CAN A. // GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXA); GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXA); // // Allocate Shared Peripheral CAN A to the CM Side. // SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_A,0x1U); #endif #ifdef CANB // // Configuring the GPIOs for CAN B. // GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXB); GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXB); // // Allocate Shared Peripheral CAN B to the CM Side. // SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_B,0x1U); #endif #ifdef UART // // Configure GPIO85 as the UART Rx pin. // GPIO_setPinConfig(GPIO_85_UARTA_RX); GPIO_setDirectionMode(85, GPIO_DIR_MODE_IN); GPIO_setPadConfig(85, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(85, GPIO_QUAL_ASYNC); // // Configure GPIO84 as the UART Tx pin. // GPIO_setPinConfig(GPIO_84_UARTA_TX); GPIO_setDirectionMode(84, GPIO_DIR_MODE_OUT); GPIO_setPadConfig(84, GPIO_PIN_TYPE_STD); GPIO_setQualificationMode(84, GPIO_QUAL_ASYNC); #endif #ifdef USB #ifdef USE_20MHZ_XTAL // // Set up the auxiliary PLL so a 60 MHz output clock is provided to the USB module. // This fixed frequency is required for all USB operations. // SysCtl_setAuxClock(SYSCTL_AUXPLL_OSCSRC_XTAL | SYSCTL_AUXPLL_IMULT(48) | SYSCTL_REFDIV(2U) | SYSCTL_ODIV(4U) | SYSCTL_AUXPLL_DIV_2 | SYSCTL_AUXPLL_ENABLE | SYSCTL_DCC_BASE_0); #else // // Set up the auxiliary PLL so a 60 MHz output clock is provided to the USB module. // This fixed frequency is required for all USB operations. // SysCtl_setAuxClock(SYSCTL_AUXPLL_OSCSRC_XTAL | SYSCTL_AUXPLL_IMULT(48) | SYSCTL_REFDIV(2U) | SYSCTL_ODIV(5U) | SYSCTL_AUXPLL_DIV_2 | SYSCTL_AUXPLL_ENABLE | SYSCTL_DCC_BASE_0); #endif // // Allocate Shared Peripheral USB to the CM Side. // SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_USBA, 1); GPIO_setPinConfig(GPIO_0_GPIO0); GPIO_setPadConfig(0, GPIO_PIN_TYPE_STD); GPIO_setDirectionMode(0, GPIO_DIR_MODE_OUT); GPIO_setMasterCore(0, GPIO_CORE_CM); // // Set the master core of GPIOs to CM. // GPIO_setMasterCore(42, GPIO_CORE_CM); GPIO_setMasterCore(43, GPIO_CORE_CM); GPIO_setMasterCore(46, GPIO_CORE_CM); GPIO_setMasterCore(47, GPIO_CORE_CM); GPIO_setMasterCore(120, GPIO_CORE_CM); GPIO_setMasterCore(121, GPIO_CORE_CM); // // Set the USB DM and DP GPIOs. // GPIO_setAnalogMode(42, GPIO_ANALOG_ENABLED); GPIO_setAnalogMode(43, GPIO_ANALOG_ENABLED); // // Set the direction for VBUS and ID. // GPIO_setDirectionMode(46, GPIO_DIR_MODE_IN); GPIO_setDirectionMode(47, GPIO_DIR_MODE_IN); // // Configure the Power Fault. // GPIO_setMasterCore(120, GPIO_CORE_CM); GPIO_setDirectionMode(120, GPIO_DIR_MODE_IN); // // Configure the External Power Signal Enable. // GPIO_setMasterCore(121, GPIO_CORE_CM); GPIO_setDirectionMode(121, GPIO_DIR_MODE_OUT); GPIO_writePin(121, 1); // // Set the CM Clock to run at 120MHz. // The CM Clock is a fractional multiple of the AUXPLL Clock (120 Mhz) from // which the USB Clock (60 MHz) is derived. // SysCtl_setCMClk(SYSCTL_CMCLKOUT_DIV_1, SYSCTL_SOURCE_AUXPLL); #endif }
I2C的例程,cpu里面都没有设置GPIO,是不是I2C本身就有问题,当时测试都没过