This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: ADC模块测试值偏差较大

Part Number: TMS320F28335


产线测试,TMS320F28335的模拟信号采集测试不良,测试值偏差较大,产线测试无法通过。

测试发现ADC采样值一直是临界值附近,具体数据如下表。切换未使用的芯片,测试正常。

请问是什么问题?有什么解决建议?

失效项 原测试值(FAIL) 更换DSP后测试值(PASS) Up limit Lower limit 对应DSP PIN脚
模拟信号采集:X90-8输入-1V 读取AD采样电压A -1.205566 -0.861328 -0.8 -1.2 PIN 49
模拟信号采集:X90-13输入-1V 读取AD采样电压A -1.210449 -0.862792 -0.8 -1.2 42
模拟信号采集:X90-14输入-1V 读取AD采样电压A -1.230712 -0.879394 -0.8 -1.2 46
模拟信号采集:X90-15输入-1V 读取AD采样电压A -1.205078 -0.861328 -0.8 -1.2 47
模拟信号采集:X91-7输入-1V 读取AD采样电压A -1.285839 -0.805615 -0.8 -1.2 51
模拟信号采集:X91-7输入1V 读取AD采样电压A 0.754346 1.192188 1.2 0.8 51
模拟信号采集:X91-8输入-1V 读取AD采样电压A -1.279687 -0.804589 -0.8 -1.2 52
模拟信号采集:X91-8输入1V 读取AD采样电压A 0.764941 1.194239 1.2 0.8 52
模拟信号采集:X91-9输入-1V 读取AD采样电压A -1.204101 -0.863036 -0.8 -1.2 48