Part Number: TMS320F280049

根据图示进行通信时,MCU2的所有SCI相关引脚都有数据信号,但MCU1的SCI-A的TX引脚经常没有数据发送,重新上电几次后MCU1的SCI-A又可以重新通信
每次开机都要连续重新上电几次才能正常根据图示通信,两款芯片均为TMS320F280049芯片
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280049

根据图示进行通信时,MCU2的所有SCI相关引脚都有数据信号,但MCU1的SCI-A的TX引脚经常没有数据发送,重新上电几次后MCU1的SCI-A又可以重新通信
每次开机都要连续重新上电几次才能正常根据图示通信,两款芯片均为TMS320F280049芯片
两块板子的硬件都相同吗?有没有互换一下位置测试一下?或者说,硬件上能确保MCU1能运行正常吗?
两块板子硬件相同,当我用XDS110调试器,调试MCU2时,MCU2的所有SCI都正常,而MCU1的SCI-A的发送端没有任何数据,其余SCI的数据正常
当我用XDS110调试器调试MCU1时,MCU1的所有SCI都正常,而MCU2的SCI-A的发送端没有任何数据,其余SCI的数据正常
当其中一个不正常时,重复上电又都能正常通信
MCU的代码都是从电脑接收到SCI-A的数据时将数据从SCI-B发送给另一个MCU,另一个MCU在SCI-B接收到数据时将数据从SCI-A发送到电脑
以下是SCI-A的初始化
void HAL_setupSCI(void)
{
//
// GPIO28 is the SCI Rx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);
//
// GPIO29 is the SCI Tx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);
//
// Map the ISR to the wake interrupt.
//
Interrupt_register(INT_SCIA_TX, &sciaTxISR);
Interrupt_register(INT_SCIA_RX, &sciaRxISR);
//
// Initialize SCIA and its FIFO.
//
SCI_performSoftwareReset(SCIA_BASE);
//
// 50000000 is the LSPCLK or the Clock used for the SCI Module
// 57600 is the Baudrate desired of the SCI module
// 1 stop bit, No parity, 8 char bits,
//
SCI_setConfig(SCIA_BASE, LSPCLK_FREQ_H, 19200,
(SCI_CONFIG_WLEN_8 |
SCI_CONFIG_STOP_ONE |
SCI_CONFIG_PAR_NONE));
//
//No loopback
//
SCI_disableLoopback(SCIA_BASE);
SCI_resetChannels(SCIA_BASE);
SCI_resetRxFIFO(SCIA_BASE);
SCI_resetTxFIFO(SCIA_BASE);
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
SCI_enableFIFO(SCIA_BASE);
SCI_enableModule(SCIA_BASE);
SCI_performSoftwareReset(SCIA_BASE);
//
// Set the transmit FIFO level to 0 and the receive FIFO level to 2.
// Enable the TXFF and RXFF interrupts.
//
SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX0, SCI_FIFO_RX1);
SCI_enableInterrupt(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
//
// Clear the SCI interrupts before enabling them.
//
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
//
// Enable the interrupts in the PIE: Group 9 interrupts 1 & 2.
//
Interrupt_enable(INT_SCIA_RX);
Interrupt_enable(INT_SCIA_TX);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
以下是SCI-A的中断服务函数
发送中断:
interrupt void sciaTxISR(void)
{
//
// Disable the TXRDY interrupt.
//
SCI_disableInterrupt(SCIA_BASE, SCI_INT_TXFF);
while (SciTxPointEnd != SciTxPointHead) {
SCI_writeCharBlockingFIFO(SCIA_BASE,(uint16_t)SciTxBuf[SciTxPointEnd]);
SciTxPointEnd ++ ;
if (SciTxPointEnd == TxLen)
SciTxPointEnd = 0;
}
SciTxPointEnd = SciTxPointHead = 0;
memset(SciTxBuf,0,TxLen);
//
// Acknowledge the PIE interrupt.
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
接收中断:
interrupt void sciaRxISR(void)
{
//
// Read characters from the FIFO.
//
//每次中断接收到数据SciRxPointHead就相当于指针在数组上后移一位
//如果SciRxPointHead已经指到数组最后一位,那么又重头开始指
SciRxBuf[SciRxPointHead] = SCI_readCharBlockingFIFO(SCIA_BASE);
SciRxPointHead ++;
if (SciRxPointHead == RxLen)
SciRxPointHead = 0;
//
// Clear the SCI RXFF interrupt and acknowledge the PIE interrupt.
//
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
以下是SCI-B的初始化代码
void HAL_setupSCIB(void)
{
//
// GPIO13 is the SCI Rx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDB);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDB, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDB, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDB, GPIO_QUAL_ASYNC);
//
// GPIO12 is the SCI Tx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDB);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDB, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDB, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDB, GPIO_QUAL_ASYNC);
//
// Map the ISR to the wake interrupt.
//
Interrupt_register(INT_SCIB_TX, &scibTxISR);
Interrupt_register(INT_SCIB_RX, &scibRxISR);
//
// Initialize SCIB and its FIFO.
//
SCI_performSoftwareReset(SCIB_BASE);
//
// 50000000 is the LSPCLK or the Clock used for the SCI Module
// 57600 is the Baudrate desired of the SCI module
// 1 stop bit, No parity, 8 char bits,
//
SCI_setConfig(SCIB_BASE, LSPCLK_FREQ_H, 19200,
(SCI_CONFIG_WLEN_8 |
SCI_CONFIG_STOP_ONE |
SCI_CONFIG_PAR_NONE));
//
//No loopback
//
SCI_disableLoopback(SCIB_BASE);
SCI_resetChannels(SCIB_BASE);
SCI_resetRxFIFO(SCIB_BASE);
SCI_resetTxFIFO(SCIB_BASE);
SCI_clearInterruptStatus(SCIB_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
SCI_enableFIFO(SCIB_BASE);
SCI_enableModule(SCIB_BASE);
SCI_performSoftwareReset(SCIB_BASE);
//
// Set the transmit FIFO level to 0 and the receive FIFO level to 2.
// Enable the TXFF and RXFF interrupts.
//
SCI_setFIFOInterruptLevel(SCIB_BASE, SCI_FIFO_TX0, SCI_FIFO_RX1);
SCI_enableInterrupt(SCIB_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
//
// Clear the SCI interrupts before enabling them.
//
SCI_clearInterruptStatus(SCIB_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
//
// Enable the interrupts in the PIE: Group 9 interrupts 3 & 4.
//
Interrupt_enable(INT_SCIB_RX);
Interrupt_enable(INT_SCIB_TX);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
以下是SCI-B的中断服务函数
发送中断:
interrupt void scibTxISR(void)
{
//
// Disable the TXRDY interrupt.
//
SCI_disableInterrupt(SCIB_BASE, SCI_INT_TXFF);
while (ScibTxPointEnd != ScibTxPointHead) {
SCI_writeCharBlockingFIFO(SCIB_BASE,(uint16_t)ScibTxBuf[ScibTxPointEnd]);
ScibTxPointEnd ++ ;
if (ScibTxPointEnd == TxLen)
ScibTxPointEnd = 0;
}
ScibTxPointEnd = ScibTxPointHead = 0;
memset(ScibTxBuf,0,TxLen);
//
// Acknowledge the PIE interrupt.
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
接收中断:
interrupt void scibRxISR(void)
{
//
// Read characters from the FIFO.
//
//
//
ScibRxBuf[ScibRxPointHead] = SCI_readCharBlockingFIFO(SCIB_BASE);
ScibRxPointHead ++;
if (ScibRxPointHead == RxLen)
ScibRxPointHead = 0;
//
// Clear the SCI RXFF interrupt and acknowledge the PIE interrupt.
//
SCI_clearInterruptStatus(SCIB_BASE, SCI_INT_RXFF);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
循环事件中的测试代码:
void SCI_Receive_Debug(void)
{
//SCIA的接收
while(SciRxPointHead != SciRxPointEnd){
//正在接收数据
ReceiveCMD[SciDataRxLen] = SciRxBuf[SciRxPointEnd];//记录接收内容
SciDataRxLen ++;//记录接收长度
SciRxPointEnd ++;
if (SciRxPointEnd == RxLen){
SciRxPointEnd = 0;
}
if(SciDataRxLen == RxLen){
SciDataRxLen = 0;
}
}
if(ReceiveCMD[0] != 0x00)//无论A接收到什么,都从B重新发出
{
SendMessageToSCIB(SCIB_BASE,ReceiveCMD);
memset(ReceiveCMD,0,RxLen);
SciDataRxLen = 0;
}
//SCIB的接收
while(ScibRxPointHead != ScibRxPointEnd)
{
//正在接收数据
ReceiveCMDB[SciDataRxLen] = ScibRxBuf[ScibRxPointEnd];//记录接收内容
SciDataRxLen ++;//记录接收长度
ScibRxPointEnd ++;
if (ScibRxPointEnd == RxLen){
ScibRxPointEnd = 0;
}
if(SciDataRxLen == RxLen){
SciDataRxLen = 0;
}
}
if(ReceiveCMDB[0] != 0x00)//无论B接收到什么,都从A重新发出
{
SendMessageToSCI(SCIA_BASE,ReceiveCMDB);
memset(ReceiveCMDB,0,RxLen);
SciDataRxLen = 0;
}
}你好,这边看了一下你的程序,应该没有什么问题,“重启能运行”这点也基本说明程序可以运行。但是这个现象确实没有什么根据,我这边建议你在英文E2E论坛上咨询一下这个问题,英文论坛的工程师可能有其他建议可以参考。
已经找到问题在哪了,两个芯片通信时IO配置有问题,输出IO应配置为开漏输出,输入IO应配置为内部上拉输入