Part Number: TMS320F28377D
你好,我在第一次使用TMS320F28377D芯片,想要利用C2PROG通过SCI串口将程序烧写进芯片中,将GPIO72置高,GPIO84置低,断电重启,照理说进入了SCI_Bootloader模式,但是烧写不成功,其中hex文件是由CCS生成的,串口也能正常通讯。以下是烧写的截图
在之前使用28335芯片时,可以烧写成功。
在这种情况下,我的问题如下:1、我这种行为应该称为一次Bootloader吧?应该不需要改动cmd文件吧?因为我记得28335不需要改动cmd配置即可烧写,还是说28335也需要改动cmd文件,只是因为我看书不认真,没注意?
2、烧写不成功的原因有哪些?比如:需要修改文件配置,而我没有做?如果是这种原因,我希望您能指导我如何配置;我将我的cmd代码附上,麻烦您看一下;
3、官方提供的例程中,有一个F2837xD_sci_flash_kernels的例程,这个例程的内容应该是二次bootloader吧?还是说它其实是一次bootloader,我应该按照这个例程学习?
我问的问题有点新手,麻烦您了,谢谢。
MEMORY
{
PAGE 0 : /* Program Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
/* BEGIN is used for the "boot to Flash" bootloader mode IPCBootCPU*/
BEGIN : origin = 0x080000, length = 0x000002
RAMM0 : origin = 0x000122, length = 0x0002DE
RAMD0 : origin = 0x00B000, length = 0x000800
RAMLS0 : origin = 0x008000, length = 0x000800
RAMLS1 : origin = 0x008800, length = 0x000800
RAMLS2 : origin = 0x009000, length = 0x000800
RAMLS3 : origin = 0x009800, length = 0x000800
RAMLS4 : origin = 0x00A000, length = 0x000800
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
FLASHC : origin = 0x084000, length = 0x002000 /* on-chip Flash */
FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
FLASHN : origin = 0x0BE000, length = 0x002000 /* on-chip Flash */
PAGE 1 : /* Data Memory */
/* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */
RAMD1 : origin = 0x00B800, length = 0x000800
RAMLS5 : origin = 0x00A800, length = 0x000800
/**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**CPU1**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**/
RAMGS0 : origin = 0x00C000, length = 0x001000
RAMGS1 : origin = 0x00D000, length = 0x001000
RAMGS2 : origin = 0x00E000, length = 0x001000
// RAMGS3 : origin = 0x00F000, length = 0x001000
// RAMGS4 : origin = 0x010000, length = 0x001000
// RAMGS5 : origin = 0x011000, length = 0x001000
RAMGS345 : origin = 0x00F000, length = 0x003000
// RAMGS6 : origin = 0x012000, length = 0x001000
RAMGS6_0 : origin = 0x012000, length = 0x000100
RAMGS6_1 : origin = 0x012100, length = 0x000100
RAMGS6_2 : origin = 0x012200, length = 0x000800
RAMGS6_3 : origin = 0x012A00, length = 0x000080
RAMGS6_4 : origin = 0x012A80, length = 0x000040
RAMGS6_5 : origin = 0x012AC0, length = 0x000040
RAMGS6_6 : origin = 0x012B00, length = 0x000500
RAMGS7 : origin = 0x013000, length = 0x001000
RAMGS8 : origin = 0x014000, length = 0x001000
RAMGS9 : origin = 0x015000, length = 0x001000
/**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**CPU2**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**/
RAMGS10 : origin = 0x016000, length = 0x001000
RAMGS11 : origin = 0x017000, length = 0x001000
// RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS12_0 : origin = 0x018000, length = 0x000800
RAMGS12_1 : origin = 0x018800, length = 0x000800
RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
RAMGS15 : origin = 0x01B000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400
CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHB PAGE = 0, ALIGN(4)
.pinit : > FLASHB, PAGE = 0, ALIGN(4)
.text : >> FLASHB | FLASHC | FLASHD | FLASHE PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : >> RAMLS5 | RAMGS0 | RAMGS1 PAGE = 1
.esysmem : > RAMLS5 PAGE = 1
/* Initalized sections go in Flash */
.econst : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
.switch : > FLASHB PAGE = 0, ALIGN(4)
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
Filter_RegsFile : > RAMGS0, PAGE = 1
SHARERAMGS0 : > RAMGS0, PAGE = 1
SHARERAMGS1 : > RAMGS1, PAGE = 1
SHARERAMGS2 : > RAMGS2, PAGE = 1
// SHARERAMGS3 : > RAMGS3, PAGE = 1
// SHARERAMGS4 : > RAMGS4, PAGE = 1
// SHARERAMGS5 : > RAMGS5, PAGE = 1
// SHARERAMGS6 : > RAMGS6, PAGE = 1
SHARERAMGS7 : > RAMGS7, PAGE = 1
SHARERAMGS8 : > RAMGS8, PAGE = 1
SHARERAMGS9 : > RAMGS9, PAGE = 1
SHARERAMGS10 : > RAMGS10, PAGE = 1
SHARERAMGS11 : > RAMGS11, PAGE = 1
// SHARERAMGS12 : > RAMGS12, PAGE = 1
SHARERAMGS13 : > RAMGS13, PAGE = 1
SHARERAMGS14 : > RAMGS14, PAGE = 1
SHARERAMGS15 : > RAMGS15, PAGE = 1
/* Allocate DMA-accessible RAM sections: */
DMARAMGS345 : >RAMGS345 PAGE = 1
GSRAM_SCOPE : >RAMGS8 PAGE = 1
/* CPU1:R/W CPU2:R*/
C1SHRAM_SETUP : > RAMGS6_0 PAGE = 1
C1SHRAM_RUNTIME : > RAMGS6_1 PAGE = 1
C1SHRAM_REAL : > RAMGS6_2 PAGE = 1
C1SHRAM_PWM : > RAMGS6_3 PAGE = 1
C1SHRAM_TASKTIME : > RAMGS6_4 PAGE = 1
C1SHRAM_OUTPUT : > RAMGS6_5 PAGE = 1
C1SHRAM_C1TOC2 : > RAMGS6_6 PAGE = 1
/* CPU1:R CPU2:R/W*/
C2SHRAM_USB : > RAMGS12_0 PAGE = 1
C2SHRAM_R12_RCV : > RAMGS12_1 PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHD,
RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
/* The following section definitions are required when using the IPC API Drivers */
GROUP : > CPU1TOCPU2RAM, PAGE = 1
{
PUTBUFFER
PUTWRITEIDX
GETREADIDX
}
GROUP : > CPU2TOCPU1RAM, PAGE = 1
{
GETBUFFER : TYPE = DSECT
GETWRITEIDX : TYPE = DSECT
PUTREADIDX : TYPE = DSECT
}
/* The following section definition are for SDFM examples */
// Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
// Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
// Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
// Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444
// Difference_RegsFile : >RAMGS5, PAGE = 1, fill=0x3333
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/