This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: 串口烧写hex出现问题,一次bootloader怎么配置

Part Number: TMS320F28377D

你好,我在第一次使用TMS320F28377D芯片,想要利用C2PROG通过SCI串口将程序烧写进芯片中,将GPIO72置高,GPIO84置低,断电重启,照理说进入了SCI_Bootloader模式,但是烧写不成功,其中hex文件是由CCS生成的,串口也能正常通讯。以下是烧写的截图

在之前使用28335芯片时,可以烧写成功。

在这种情况下,我的问题如下:1、我这种行为应该称为一次Bootloader吧?应该不需要改动cmd文件吧?因为我记得28335不需要改动cmd配置即可烧写,还是说28335也需要改动cmd文件,只是因为我看书不认真,没注意?

2、烧写不成功的原因有哪些?比如:需要修改文件配置,而我没有做?如果是这种原因,我希望您能指导我如何配置;我将我的cmd代码附上,麻烦您看一下;

3、官方提供的例程中,有一个F2837xD_sci_flash_kernels的例程,这个例程的内容应该是二次bootloader吧?还是说它其实是一次bootloader,我应该按照这个例程学习?

我问的问题有点新手,麻烦您了,谢谢。

MEMORY
{
PAGE 0 :  /* Program Memory */
          /* Memory (RAM/FLASH) blocks can be moved to PAGE1 for data allocation */
          /* BEGIN is used for the "boot to Flash" bootloader mode   IPCBootCPU*/

   BEGIN           	: origin = 0x080000, length = 0x000002
   RAMM0           	: origin = 0x000122, length = 0x0002DE
   RAMD0           	: origin = 0x00B000, length = 0x000800
   RAMLS0          	: origin = 0x008000, length = 0x000800
   RAMLS1          	: origin = 0x008800, length = 0x000800
   RAMLS2      		: origin = 0x009000, length = 0x000800
   RAMLS3      		: origin = 0x009800, length = 0x000800
   RAMLS4      		: origin = 0x00A000, length = 0x000800
   RESET           	: origin = 0x3FFFC0, length = 0x000002

   /* Flash sectors */
   FLASHA           : origin = 0x080002, length = 0x001FFE	/* on-chip Flash */
   FLASHB           : origin = 0x082000, length = 0x002000	/* on-chip Flash */
   FLASHC           : origin = 0x084000, length = 0x002000	/* on-chip Flash */
   FLASHD           : origin = 0x086000, length = 0x002000	/* on-chip Flash */
   FLASHE           : origin = 0x088000, length = 0x008000	/* on-chip Flash */
   FLASHF           : origin = 0x090000, length = 0x008000	/* on-chip Flash */
   FLASHG           : origin = 0x098000, length = 0x008000	/* on-chip Flash */
   FLASHH           : origin = 0x0A0000, length = 0x008000	/* on-chip Flash */
   FLASHI           : origin = 0x0A8000, length = 0x008000	/* on-chip Flash */
   FLASHJ           : origin = 0x0B0000, length = 0x008000	/* on-chip Flash */
   FLASHK           : origin = 0x0B8000, length = 0x002000	/* on-chip Flash */
   FLASHL           : origin = 0x0BA000, length = 0x002000	/* on-chip Flash */
   FLASHM           : origin = 0x0BC000, length = 0x002000	/* on-chip Flash */
   FLASHN           : origin = 0x0BE000, length = 0x002000	/* on-chip Flash */

PAGE 1 : /* Data Memory */
         /* Memory (RAM/FLASH) blocks can be moved to PAGE0 for program allocation */

   BOOT_RSVD       : origin = 0x000002, length = 0x000120     /* Part of M0, BOOT rom will use this for stack */
   RAMM1           : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAMD1           : origin = 0x00B800, length = 0x000800

   RAMLS5      : origin = 0x00A800, length = 0x000800

	/**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**CPU1**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**/
   RAMGS0      : origin = 0x00C000, length = 0x001000
   RAMGS1      : origin = 0x00D000, length = 0x001000
   RAMGS2      : origin = 0x00E000, length = 0x001000
// RAMGS3      : origin = 0x00F000, length = 0x001000
// RAMGS4      : origin = 0x010000, length = 0x001000
// RAMGS5      : origin = 0x011000, length = 0x001000
   RAMGS345    : origin = 0x00F000, length = 0x003000
//   RAMGS6      : origin = 0x012000, length = 0x001000
   RAMGS6_0      : origin = 0x012000, length = 0x000100
   RAMGS6_1      : origin = 0x012100, length = 0x000100
   RAMGS6_2      : origin = 0x012200, length = 0x000800
   RAMGS6_3      : origin = 0x012A00, length = 0x000080
   RAMGS6_4      : origin = 0x012A80, length = 0x000040
   RAMGS6_5      : origin = 0x012AC0, length = 0x000040
   RAMGS6_6      : origin = 0x012B00, length = 0x000500
   RAMGS7      : origin = 0x013000, length = 0x001000
   RAMGS8      : origin = 0x014000, length = 0x001000
   RAMGS9      : origin = 0x015000, length = 0x001000

	/**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**CPU2**↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓↓**/
   RAMGS10     : origin = 0x016000, length = 0x001000
   RAMGS11     : origin = 0x017000, length = 0x001000
//   RAMGS12     : origin = 0x018000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS12_0   : origin = 0x018000, length = 0x000800
   RAMGS12_1   : origin = 0x018800, length = 0x000800
   RAMGS13     : origin = 0x019000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS14     : origin = 0x01A000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */
   RAMGS15     : origin = 0x01B000, length = 0x001000     /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */



   CPU2TOCPU1RAM   : origin = 0x03F800, length = 0x000400
   CPU1TOCPU2RAM   : origin = 0x03FC00, length = 0x000400
}

SECTIONS
{
   /* Allocate program areas: */
   .cinit              : > FLASHB      PAGE = 0, ALIGN(4)
   .pinit              : > FLASHB,     PAGE = 0, ALIGN(4)
   .text               : >> FLASHB | FLASHC | FLASHD | FLASHE      PAGE = 0, ALIGN(4)
   codestart           : > BEGIN       PAGE = 0, ALIGN(4)

   /* Allocate uninitalized data sections: */
   .stack              : > RAMM1        PAGE = 1
   .ebss               : >> RAMLS5 | RAMGS0 | RAMGS1       PAGE = 1
   .esysmem            : > RAMLS5       PAGE = 1

   /* Initalized sections go in Flash */
   .econst             : >> FLASHF | FLASHG | FLASHH      PAGE = 0, ALIGN(4)
   .switch             : > FLASHB      PAGE = 0, ALIGN(4)

   .reset              : > RESET,     PAGE = 0, TYPE = DSECT /* not used, */

   Filter_RegsFile     : > RAMGS0,	   PAGE = 1

   SHARERAMGS0		: > RAMGS0,		PAGE = 1
   SHARERAMGS1		: > RAMGS1,		PAGE = 1
   SHARERAMGS2		: > RAMGS2,		PAGE = 1
//   SHARERAMGS3		: > RAMGS3,		PAGE = 1
//   SHARERAMGS4		: > RAMGS4,		PAGE = 1
//   SHARERAMGS5		: > RAMGS5,		PAGE = 1
//   SHARERAMGS6		: > RAMGS6,		PAGE = 1
   SHARERAMGS7		: > RAMGS7,		PAGE = 1
   SHARERAMGS8		: > RAMGS8,		PAGE = 1
   SHARERAMGS9		: > RAMGS9,		PAGE = 1
   SHARERAMGS10		: > RAMGS10,	PAGE = 1
   SHARERAMGS11		: > RAMGS11,	PAGE = 1
//   SHARERAMGS12		: > RAMGS12,	PAGE = 1
   SHARERAMGS13		: > RAMGS13,	PAGE = 1
   SHARERAMGS14		: > RAMGS14,	PAGE = 1
   SHARERAMGS15		: > RAMGS15,	PAGE = 1

   /* Allocate DMA-accessible RAM sections: */
   DMARAMGS345        : >RAMGS345     PAGE = 1
   GSRAM_SCOPE        : >RAMGS8       PAGE = 1

   		/* CPU1:R/W   CPU2:R*/
   C1SHRAM_SETUP      : > RAMGS6_0    PAGE = 1
   C1SHRAM_RUNTIME    : > RAMGS6_1    PAGE = 1
   C1SHRAM_REAL       : > RAMGS6_2    PAGE = 1
   C1SHRAM_PWM        : > RAMGS6_3    PAGE = 1
   C1SHRAM_TASKTIME   : > RAMGS6_4    PAGE = 1
   C1SHRAM_OUTPUT     : > RAMGS6_5    PAGE = 1
   C1SHRAM_C1TOC2        : > RAMGS6_6    PAGE = 1

     	 /* CPU1:R     CPU2:R/W*/
   C2SHRAM_USB        : > RAMGS12_0    PAGE = 1
   C2SHRAM_R12_RCV    : > RAMGS12_1    PAGE = 1


#ifdef __TI_COMPILER_VERSION__
	#if __TI_COMPILER_VERSION__ >= 15009000
	.TI.ramfunc : {} LOAD = FLASHD,
						 RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
						 PAGE = 0, ALIGN(4)
	#else
   ramfuncs            : LOAD = FLASHD,
                         RUN = RAMLS0 | RAMLS1 | RAMLS2 |RAMLS3,
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_SIZE(_RamfuncsLoadSize),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         RUN_SIZE(_RamfuncsRunSize),
                         RUN_END(_RamfuncsRunEnd),
                         PAGE = 0, ALIGN(4)    
    #endif
#endif

   /* The following section definitions are required when using the IPC API Drivers */
    GROUP : > CPU1TOCPU2RAM, PAGE = 1
    {
        PUTBUFFER
        PUTWRITEIDX
        GETREADIDX
    }

    GROUP : > CPU2TOCPU1RAM, PAGE = 1
    {
        GETBUFFER :    TYPE = DSECT
        GETWRITEIDX :  TYPE = DSECT
        PUTREADIDX :   TYPE = DSECT
    }

   /* The following section definition are for SDFM examples */
//   Filter1_RegsFile : > RAMGS1,	PAGE = 1, fill=0x1111
//   Filter2_RegsFile : > RAMGS2,	PAGE = 1, fill=0x2222
//   Filter3_RegsFile : > RAMGS3,	PAGE = 1, fill=0x3333
//   Filter4_RegsFile : > RAMGS4,	PAGE = 1, fill=0x4444
//   Difference_RegsFile : >RAMGS5, 	PAGE = 1, fill=0x3333
}

/*
//===========================================================================
// End of file.
//===========================================================================
*/