Other Parts Discussed in Thread: SYSCONFIG, CONTROLSUITE, UNIFLASH
关于F280049C加密问题
1:ASM文件是用SYSCONFIG产生的ASM文件和CMD文件
- ASM文件内容:
文件说明内容只是修改了红色部分
密码1,3,4修改为12345678
其它内容一字不改
; ----------------------------------------------------------------------
; Zone 1
;----------------------------------------------------------------------
.sect "dcsm_otp_z1_linkpointer"
.retain
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.sect "dcsm_otp_z1_pswdlock"
.retain
.long 0xFB7FFFFF
.long 0x7FFFFFFF ;Reserved
.sect "dcsm_otp_z1_crclock"
.retain
.long 0x4BFFFFFF
.long 0x3FFFFFFF ;Reserved
;; .sect "dcsm_otp_z1_gpreg"
;; .retain
;; .long 0x5AFF1820 ;Z1OTP_BOOTPIN_CONFIG
;; .long 0x5AFFFFfF ;Z1OTP_GPREG2
;; .sect "dcsm_otp_z1_bootctrl"
;; .retain
;; .long 0x00000000 ;Z1OTP_BOOTDEF_LOW
;; .long 0xFFFFFFFF ;Z1OTP_BOOTDEF_HIGH
.sect "dcsm_zsel_z1"
.retain
.long 0x000000FF ;Z1-EXEONLYRAM
.long 0x0000FFFF ;Z1-EXEONLYSECT
.long 0x0000AAAA ;Z1-GRABRAM
.long 0xAAAAAAAA ;Z1-GRABSECT
.long 0x12345678
.long 0x47FFFFFF
.long 0x12345678
.long 0x12345678
.sect "b1_dcsm_otp_z1_linkpointer"
.retain
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.sect "b1_dcsm_zsel_z1"
.retain
.long 0xFFFFFFFF ;Reserved
.long 0x0000FFFF ;Bank 1 Z1-EXEONLYSECT
.long 0xFFFFFFFF ;Reserved
.long 0xAAAAAAAA ;Bank 1 Z1-GRABSECT
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
;----------------------------------------------------------------------
; For code security operation,after development has completed, prior to
; production, all other zone select block locations should be programmed
; to 0x0000 for maximum security.
; If the first zone select block at offset 0x10 is used, the section
; "dcsm_rsvd_z1" can be used to program these locations to 0x0000.
; This code is commented out for development.
; .sect "dcsm_rsvd_z1"
; .loop (1e0h)
; .int 0x0000
; .endloop
;----------------------------------------------------------------------
; Zone 2
;----------------------------------------------------------------------
.sect "dcsm_otp_z2_linkpointer"
.retain
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.sect "dcsm_otp_z2_pswdlock"
.retain
.long 0xBF7FFFFF
.long 0x77FFFFFF ;Reserved
.sect "dcsm_otp_z2_crclock"
.retain
.long 0x0FFFFFFF
.long 0x37FFFFFF ;Reserved
;; .sect "dcsm_otp_z2_gpreg"
;; .retain
;; .long 0x5AFF1820 ;Z2OTP_BOOTPIN_CONFIG
;; .long 0x5AFFFFfF ;Z2OTP_GPREG2
;; .sect "dcsm_otp_z2_bootctrl"
;; .retain
;; .long 0x00000000 ;Z2OTP_BOOTDEF_LOW
;; .long 0xFFFFFFFF ;Z2OTP_BOOTDEF_HIGH
.sect "dcsm_zsel_z2"
.retain
.long 0x000000FF ;z2-EXEONLYRAM
.long 0x0000FFFF ;z2-EXEONLYSECT
.long 0x0000AAAA ;z2-GRABRAM
.long 0xAAAAAAAA ;z2-GRABSECT
.long 0x12345678
.long 0xE3FFFFFF
.long 0x12345678
.long 0x12345678
.sect "b1_dcsm_otp_z2_linkpointer"
.retain
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.long 0x1FFFFFFF
.long 0xFFFFFFFF ;Reserved
.sect "b1_dcsm_zsel_z2"
.retain
.long 0xFFFFFFFF ;Reserved
.long 0x0000FFFF ;Bank 1 Z2-EXEONLYSECT
.long 0xFFFFFFFF ;Reserved
.long 0xAAAAAAAA ;Bank 1 Z2-GRABSECT
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
.long 0xFFFFFFFF ;Reserved
;----------------------------------------------------------------------
; For code security operation,after development has completed, prior to
; production, all other zone select block locations should be programmed
; to 0x0000 for maximum security.
; If the first zone select block at offset 0x10 is used, the section
; "dcsm_rsvd_z2" can be used to program these locations to 0x0000.
; This code is commented out for development.
; .sect "dcsm_rsvd_z2"
; .loop (1e0h)
; .int 0x0000
; .endloop
;----------------------------------------------------------------------
; End of file
;----------------------------------------------------------------------
1.2 CMD文件内容生成后没动过
1.3 然后进行编译,得到MAP文件和OUT文件
/* this linker command file is to be included if user wants to use the DCSM feature on the device
* DCSM means Dual Zone Code Security Module.
* This linker command file works as an addendum ot the already existing Flash/RAM linker command file
* that the project has.
* The sections in the *_ZoneSelectBlock.asm source file is linked as per the commands given in the file
* NOTE - please note fill=0xFFFF, this helps if users include this file in the project by mistake and
* doesn't provide the needed proper *_ZoneSelectBlock.asm sources .
* Please refer to the Blinky DCSM example in the controlsuite examples for proper usage of this.
*
* Once users are confident that they want to program the passwords in OTP, the DSECT section type can be removed.
*
*/
MEMORY
{
PAGE 0 : /* Program Memory */
/* Z1 OTP. LinkPointers */
DCSM_OTP_Z1_LINKPOINTER : origin = 0x78000, length = 0x00000C
/* Z1 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z1_GPREG : origin = 0x7800C, length = 0x000004
/* Z1 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z1_PSWDLOCK : origin = 0x78010, length = 0x000004
/* Z1 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z1_CRCLOCK : origin = 0x78014, length = 0x000004
/* Z1 OTP. RESERVED/BOOTCTRL */
DCSM_OTP_Z1_BOOTCTRL : origin = 0x7801C, length = 0x000004
/* DCSM Z1 Zone Select Contents (!!Movable!!) */
/* Z1 OTP. Z1 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z1_P0 : origin = 0x78020, length = 0x000010
/* Z2 OTP. LinkPointers */
DCSM_OTP_Z2_LINKPOINTER : origin = 0x78200, length = 0x00000C
/* Z2 OTP. GPREG1/GPREG2 */
DCSM_OTP_Z2_GPREG : origin = 0x7820C, length = 0x000004
/* Z2 OTP. PSWDLOCK/RESERVED */
DCSM_OTP_Z2_PSWDLOCK : origin = 0x78210, length = 0x000004
/* Z2 OTP. CRCLOCK/RESERVED */
DCSM_OTP_Z2_CRCLOCK : origin = 0x78214, length = 0x000004
/* Z2 OTP. GPREG3/BOOTCTRL */
DCSM_OTP_Z2_BOOTCTRL : origin = 0x7821C, length = 0x000004
/* DCSM Z2 Zone Select Contents (!!Movable!!) */
/* Z2 OTP. Z2 password locations / Flash and RAM partitioning */
DCSM_ZSEL_Z2_P0 : origin = 0x78220, length = 0x000010
/* BANK1 */
/* B1 Z1 OTP. LinkPointers */
B1_DCSM_OTP_Z1_LINKPOINTER : origin = 0x78400, length = 0x00000C
/* DCSM B1 Z1 Zone Select Contents (!!Movable!!) */
/* B1 Z1 OTP. Flash partitioning */
B1_DCSM_ZSEL_Z1_P0 : origin = 0x78420, length = 0x000010
/* B1 Z2 OTP. LinkPointers */
B1_DCSM_OTP_Z2_LINKPOINTER : origin = 0x78600, length = 0x00000C
/* DCSM B1 Z2 Zone Select Contents (!!Movable!!) */
/* B1 Z2 OTP. Flash partitioning */
B1_DCSM_ZSEL_Z2_P0 : origin = 0x78620, length = 0x000010
}
SECTIONS
{
dcsm_otp_z1_linkpointer : > DCSM_OTP_Z1_LINKPOINTER PAGE = 0
dcsm_otp_z1_gpreg : > DCSM_OTP_Z1_GPREG PAGE = 0, type = DSECT
dcsm_otp_z1_pswdlock : > DCSM_OTP_Z1_PSWDLOCK PAGE = 0
dcsm_otp_z1_crclock : > DCSM_OTP_Z1_CRCLOCK PAGE = 0
dcsm_otp_z1_bootctrl : > DCSM_OTP_Z1_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z1 : > DCSM_ZSEL_Z1_P0 PAGE = 0
dcsm_otp_z2_linkpointer : > DCSM_OTP_Z2_LINKPOINTER PAGE = 0
dcsm_otp_z2_gpreg : > DCSM_OTP_Z2_GPREG PAGE = 0, type = DSECT
dcsm_otp_z2_pswdlock : > DCSM_OTP_Z2_PSWDLOCK PAGE = 0
dcsm_otp_z2_crclock : > DCSM_OTP_Z2_CRCLOCK PAGE = 0
dcsm_otp_z2_bootctrl : > DCSM_OTP_Z2_BOOTCTRL PAGE = 0, type = DSECT
dcsm_zsel_z2 : > DCSM_ZSEL_Z2_P0 PAGE = 0
b1_dcsm_otp_z1_linkpointer : > B1_DCSM_OTP_Z1_LINKPOINTER PAGE = 0
b1_dcsm_zsel_z1 : > B1_DCSM_ZSEL_Z1_P0 PAGE = 0
b1_dcsm_otp_z2_linkpointer : > B1_DCSM_OTP_Z2_LINKPOINTER PAGE = 0
b1_dcsm_zsel_z2 : > B1_DCSM_ZSEL_Z2_P0 PAGE = 0
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
1.3 然后进行编译,得到MAP文件和OUT文件
SyncSocRegsFile
* 1 00007940 00000006 UNINITIALIZED
00007940 00000006 f28004x_globalvariabledefs.obj (SyncSocRegsFile)
dcsm_otp_z1_gpreg
* 0 0007800c 00000000 DSECT
dcsm_otp_z1_pswdlock
* 0 00078010 00000004
00078010 00000004 dcsm.obj (dcsm_otp_z1_pswdlock)
dcsm_otp_z1_crclock
* 0 00078014 00000004
00078014 00000004 dcsm.obj (dcsm_otp_z1_crclock)
dcsm_otp_z1_bootctrl
* 0 0007801c 00000000 DSECT
dcsm_zsel_z1
* 0 00078020 00000010
00078020 00000010 dcsm.obj (dcsm_zsel_z1)
dcsm_otp_z2_linkpointer
* 0 00078200 0000000c
00078200 0000000c dcsm.obj (dcsm_otp_z2_linkpointer)
dcsm_otp_z2_gpreg
* 0 0007820c 00000000 DSECT
dcsm_otp_z2_pswdlock
* 0 00078210 00000004
00078210 00000004 dcsm.obj (dcsm_otp_z2_pswdlock)
dcsm_otp_z2_crclock
* 0 00078214 00000004
00078214 00000004 dcsm.obj (dcsm_otp_z2_crclock)
dcsm_otp_z2_bootctrl
* 0 0007821c 00000000 DSECT
dcsm_zsel_z2
* 0 00078220 00000010
00078220 00000010 dcsm.obj (dcsm_zsel_z2)
b1_dcsm_otp_z1_linkpointer
* 0 00078400 0000000c
00078400 0000000c dcsm.obj (b1_dcsm_otp_z1_linkpointer)
b1_dcsm_zsel_z1
* 0 00078420 00000010
00078420 00000010 dcsm.obj (b1_dcsm_zsel_z1)
b1_dcsm_otp_z2_linkpointer
* 0 00078600 0000000c
00078600 0000000c dcsm.obj (b1_dcsm_otp_z2_linkpointer)
b1_dcsm_zsel_z2
* 0 00078620 00000010
00078620 00000010 dcsm.obj (b1_dcsm_zsel_z2)
1.4 下载程序到FLASH后,程序不运行了.
1.5 想再次下载程序,芯片锁死了
对应的CCS设置为下图
下载程序图
1.5 用UNIFLASH软件