This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: TI有个10KW参考设计的文档,叫《TIDA-01606_GateDriver_SCH.pdf》它是不是缺少了MOS管的驱动芯片,并且为什么它驱动上管不需要自举电容?

Part Number: TMS320F28335

文件里驱动芯片只有 ISO5852SDWR 和 UCC5320SCD 。关于这两个芯片有几个问题想求教。

1、这两个芯片看上去并不能驱动上管?因为它看上去也就20V,上管的驱动需要自举电容踩在母线电压上面吧?电压需要VBUS+VGS,例如,IR2110的HB脚为500V+自举20V

2、如果它不能驱动上管,那ISO5852SDWR它这个去饱和的引脚有什么意义?

3、 UCC5320SCD 它还搞个什么-5V,感觉要直接接在IGBT的栅级一样,但它的周围没看到有自举电容的设计和HB HS这样的引脚。