Other Parts Discussed in Thread: C2000WARE
按照下图3进行配置,下面是我电路的实际波形,绿色是PWM1A的驱动,紫色是PWM1B的驱动,黄色是引出的CTRIPOUT信号,现在有个问题 ,PWM1A是设置的TZA.FORCE LOW 动作,但是可以看到CTRIP信号到来时,经过了一定时间的延时,PWM1A才关断,延时时间好像跟我设置的DBRED(80ns)差不多,但是理论上TZA不经过DB的呀,不该有这个延时呀。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
按照下图3进行配置,下面是我电路的实际波形,绿色是PWM1A的驱动,紫色是PWM1B的驱动,黄色是引出的CTRIPOUT信号,现在有个问题 ,PWM1A是设置的TZA.FORCE LOW 动作,但是可以看到CTRIP信号到来时,经过了一定时间的延时,PWM1A才关断,延时时间好像跟我设置的DBRED(80ns)差不多,但是理论上TZA不经过DB的呀,不该有这个延时呀。
你好,你测试的是CMPSS模块控制TZ模块拉低PWMA吗?看波形似乎看不出两者有什么动作关系啊。TZ是one ***?关键两种模式似乎都跟图片上的波形对不起了啊
有没有参考过TI例程:C:\ti\c2000\C2000Ware_4_00_00_00\driverlib\f2837xd\examples\cpu1\epwm
// Included Files //pin define Cmpss3 CMP3IN_P to B2 vo_sense to A1 改EPWM6的话 ADC soc信号要改 EPWMENCK信号要改 TRIP路径EPWM bar ET事件 低输入时不正常 //PWM1A TZA-FORCE LO 1B 在AQ中 T1事件动作通过同步TRIP EVENT #include "F28x_Project.h" // Defines // //definitions for selecting DACH reference #define REFERENCE_VDDA 0 #define REFERENCE_VDAC 1 //definitions for COMPH input selection #define NEGIN_DAC 0 #define NEGIN_PIN 1 //definitions for CTRIPH/CTRIPOUTH output selection #define CTRIP_ASYNCH 0 #define CTRIP_SYNCH 1 #define CTRIP_FILTER 2 #define CTRIP_LATCH 3 int i=0; //ADC定义 #define Vo_ref 2470 //12V 2460 float Vo_ave=0; #define chanel 1 #define acqps 29 //采样窗 (acqps+1)*sysclk *5ns //斜坡定义 #define slopeval 10 /* Required slope compensation */ #define dacval 8000 // // Function Prototypes // void InitAdc(void); void InitCMPSS(void); void InitEPWM(void); void pid_init(void); interrupt void adc_isr(void); // // Main // void main(void) { // // Step 1. Initialize System Control: // PLL, WatchDog, enable Peripheral Clocks // This example function is found in the F2837xD_SysCtrl.c file. // InitSysCtrl(); // // Step 2. Initialize GPIO: // This example function is found in the F2837xD_Gpio.c file and // illustrates how to set the GPIO to it's default state. // InitGpio(); // // Step 3. Clear all interrupts and initialize PIE vector table: // Disable CPU interrupts DINT; // Initialize the PIE control registers to their default state. // The default state is all PIE interrupts disabled and flags // are cleared. // This function is found in the F2837xD_PieCtrl.c file. InitPieCtrl(); // Disable CPU interrupts and clear all CPU interrupt flags: IER = 0x0000; IFR = 0x0000; /* DSP28377D_PieVect.c */ InitPieVectTable(); /* Interrupt re-mapped to ISR function */ EALLOW; PieVectTable.ADCA1_INT = &adc_isr; EDIS; InitAdc(); /* Enable ADCA1INT1 in PIE */ PieCtrlRegs.PIEIER1.bit.INTx1 = 1;/* Enable INT 1.1 in the PIE */ IER |= M_INT1;/* Enable CPU Interrupt 1 */ EINT;/* Enable Global interrupt INTM */ ERTM;/* Enable Global realtime interrupt DBGM */ // Configure Comparator COMP3H to accept POS input from pin and NEG input // from DAC InitEPWM(); InitEPwm1Gpio(); InitCMPSS(); // Configure GPIO5() to output OUTPUTXBAR3 // GPIO_SetupPinMux(5, GPIO_MUX_CPU1, 3); //观察ctripout值 gpio5 // Configure COMP3 to feed TRIP4 EPWM DC trip input // pid_init(); while(1) { ; } } // // InitCMPSS - Initialize CMPSS3 and configure settings // void InitAdc(void) { //ADC时钟开启 EALLOW; CpuSysRegs.PCLKCR13.bit.ADC_A=1; EDIS; EALLOW; AdcaRegs.ADCCTL2.bit.PRESCALE = 6; //set ADCCLK divider to /4 AdcSetMode(ADC_ADCA, ADC_RESOLUTION_12BIT, ADC_SIGNALMODE_SINGLE); AdcaRegs.ADCSOC0CTL.bit.CHSEL =chanel; //SOC0 will convert ADCINA1 AdcaRegs.ADCSOC0CTL.bit.ACQPS = acqps; //SOC0 will use sample duration of 20 SYSCLK cycles AdcaRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //SOC0 will begin conversion on ePWM1 SOCA 5 EPWM1A AdcaRegs.ADCSOC1CTL.bit.CHSEL =chanel; //SOC0 will convert ADCINA1 AdcaRegs.ADCSOC1CTL.bit.ACQPS = acqps; //SOC0 will use sample duration of 20 SYSCLK cycles AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //SOC0 will begin conversion on ePWM1 SOCA AdcaRegs.ADCSOC2CTL.bit.CHSEL =chanel; //SOC0 will convert ADCINA1 AdcaRegs.ADCSOC2CTL.bit.ACQPS = acqps; //SOC0 will use sample duration of 20 SYSCLK cycles AdcaRegs.ADCSOC2CTL.bit.TRIGSEL = 5; //SOC0 will begin conversion on ePWM1 SOCA AdcaRegs.ADCSOC3CTL.bit.CHSEL =chanel; //SOC0 will convert ADCINA1 AdcaRegs.ADCSOC3CTL.bit.ACQPS = acqps; //SOC0 will use sample duration of 20 SYSCLK cycles AdcaRegs.ADCSOC3CTL.bit.TRIGSEL = 5; //SOC0 will begin conversion on ePWM1 SOCA AdcaRegs.ADCINTSEL1N2.bit.INT1SEL = 0; //end of SOC0 will set INT1 flag AdcaRegs.ADCINTSEL1N2.bit.INT1E = 1; //enable INT1 flag AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //make sure INT1 flag is cleared //Set pulse positions to late AdcaRegs.ADCCTL1.bit.INTPULSEPOS = 1; //power up the ADC AdcaRegs.ADCCTL1.bit.ADCPWDNZ = 1; //delay for 1ms to allow ADC time to power up DELAY_US(1000); EDIS; } void InitCMPSS(void) { EALLOW; CpuSysRegs.PCLKCR14.bit.CMPSS3 = 0; //禁用时钟 //将CMPSS分配给CPU1 DevCfgRegs.CPUSEL12.bit.CMPSS3 = 0; CpuSysRegs.PCLKCR14.bit.CMPSS3 = 1; //启用时钟 EDIS; EALLOW; // //Enable CMPSS // Cmpss3Regs.COMPCTL.bit.COMPDACE = 1; //NEG signal comes from DAC // Cmpss3Regs.COMPCTL.bit.COMPHSOURCE = NEGIN_DAC; // //Use VDDA as the reference for DAC // Cmpss3Regs.COMPDACCTL.bit.SELREF = REFERENCE_VDDA; //VDDA的值是多少 3.3 //选择同步或异步比较器触发 // Cmpss3Regs.COMPCTL.bit.ASYNCHEN = 0; //High comparator asynchronous path enable. Allows asynchronous comparator output to feed into OR gate with latched digital filter signal when CTRIPHSEL=3 or CTRIPOUTHSEL=3 // // Configure CTRIPOUT path // Asynch output feeds CTRIPH and CTRIPOUTH // Cmpss3Regs.COMPCTL.bit.COMPHINV=0; // 0比较器同相输出 1 比较器反相输出 //配置数字滤波器 //最大SAMPWIN值提供最大数量的样本(5位) Cmpss3Regs.CTRIPHFILCTL.bit.SAMPWIN = 20 ; // 0x1F & 0x00; //最大THRESH值需要整个窗口的静态值 //(5 位 THRESH 应该大于 SAMPWIN 的一半) Cmpss3Regs.CTRIPHFILCTL.bit.THRESH = 17 ; //0x1F & 0x01 //最大 CLKPRESCALE 值提供样本之间的最长时间(12 位) Cmpss3Regs.CTRIPHFILCLKCTL.bit.CLKPRESCALE =2 ; //234 2 10 7 0x3FF & 0x001; //重置过滤逻辑并开始过滤 Cmpss3Regs.CTRIPHFILCTL.bit.FILINIT = 1; //清除锁存器 Cmpss3Regs.COMPSTSCLR.bit.HSYNCCLREN=1; //1 EPWMSYNCPER will reset latch Cmpss3Regs.COMPSTSCLR.bit.HLATCHCLR = 1; //清除锁存值 //输出路径 Cmpss3Regs.COMPCTL.bit.CTRIPHSEL = CTRIP_ASYNCH; // Cmpss3Regs.COMPCTL.bit.CTRIPHSEL = CTRIP_FILTER; Cmpss3Regs.COMPCTL.bit.CTRIPOUTHSEL = CTRIP_ASYNCH; // Cmpss3Regs.COMPCTL.bit.CTRIPOUTHSEL = CTRIP_FILTER; // Cmpss3Regs.COMPHYSCTL.bit.COMPHYS=2; //设置 滞环宽度 //同步清除使能 // Cmpss3Regs.COMPSTSCLR.bit.HSYNCCLREN = 1; // // Configure CTRIPOUTH output pin // Configure OUTPUTXBAR3 to be CTRIPOUT1H // OutputXbarRegs.OUTPUT3MUX0TO15CFG.bit.MUX4 = 0; // //Enable OUTPUTXBAR3 Mux for Output // OutputXbarRegs.OUTPUT3MUXENABLE.bit.MUX4 = 1; // //DAC source select. Determines whether DACHVALA is updated from DACHVALS or from the ramp generator // Cmpss3Regs.COMPDACCTL.bit.DACSOURCE = 1; // 0 DAC updated from DACHVALS, 1 DAC updated from the ramp generator Cmpss3Regs.COMPDACCTL.bit.RAMPLOADSEL=1; //斜坡加载模式 Ramp load select. Determines whether RAMPSTS is updated from RAMPMAXREFA or RAMPMAXREFS when COMPSTS[COMPHSTS] is triggered. Cmpss3Regs.COMPDACCTL.bit.SWLOADSEL=1; /*Software load select. Determines whether DACxVALA is updated from DACxVALS on SYSCLK or EPWMSYNCPER. 0 DACxVALA is updated from DACxVALS on SYSCLK 1 DACxVALA is updated from DACxVALS on EPWMSYNCPER */ // //Ramp generator source select. Determines which EPWMSYNCPER signal is used within the CMPSS module // Cmpss3Regs.COMPDACCTL.bit.RAMPSOURCE = 0; // 0 EPWM1SYNCPER, 3 EPWM4SYNCPER 更改EPWM需要修改 Ramp generator source select. Determines which EPWMSYNCPER // signal is used within the CMPSS module EDIS; Cmpss3Regs.RAMPDECVALS = slopeval; // Cmpss3Regs.RAMPMAXREFS = dacval; //2048==> 2048/16 *3.3(ref) /4096=dacout 0.07 } // // InitEPWM - Initialize EPWM1 module settings // void InitEPWM(void) { EALLOW; // ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV=1; //EPWM分频器 CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 0; // //Configure EPWM to run at SYSCLK // // ClkCfgRegs.PERCLKDIVSEL.bit.EPWMCLKDIV = 0; EPwm1Regs.TBCTL.bit.CLKDIV = 0; EPwm1Regs.TBCTL.bit.HSPCLKDIV = 0; //Initialize dummy values for EPWM CTR/PRD // EPwm1Regs.TBCTR = 0; EPwm1Regs.TBPRD = 117; // 850kHz PWM CpuSysRegs.PCLKCR0.bit.TBCLKSYNC = 1; EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading禁止计数器装载相位寄存器的值 EPwm1Regs.TBPHS.bit.TBPHS= 0;/* Set Phase register to zero */ EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE; // Sync down-stream module EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW; //影子装载模式 EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW; EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO; // Load on Zero在CTR=0时,影子寄存器装载 EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO; // //Configure TRIP4 to be CTRIP3H // EPwmXbarRegs.TRIP4MUX0TO15CFG.bit.MUX4 = 0; // 0.4 是CMPSS3的CTRIPH //Enable TRIP4 Mux for Output // EPwmXbarRegs.TRIP4MUXENABLE.bit.MUX4 = 1; // Enable PWM // EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; EPwm1Regs.CMPA.bit.CMPA =95; //max duty limit 97/117 考虑了死区 0.82最大占空比 EPwm1Regs.CMPB.bit.CMPB =95; //max duty limit 97/117 考虑了死区 0.82最大占空比 // Set actions AQ也配置 实际上A是通过跳闸 // EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // Set PWM1A on event A, up count EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Clear PWM1A on event A, up count 限制最大占空比防止一直高电平 // EPwm1Regs.AQCTLA2.bit.T1U = AQ_CLEAR; // Action when event occurs on T2 in UP-Count EPwm1Regs.AQCTLB.bit.ZRO = AQ_SET; // Set PWM1B on event B, up count EPwm1Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Set PWM1B on event B, up count 最小占空比限制 EPwm1Regs.AQCTLB2.bit.T1U = AQ_CLEAR; // Action when event occurs on T2 in UP-Count 1:DCAEVT2发生时动作 EPwm1Regs.AQTSRCSEL.bit.T1SEL = 3; // 0:DCAEVT1, 1:DCAEVT2, 2:DCBEVT1, 3:DCBEVT2 有TI T2事件 DCAEVT2事件被配置为异步跳闸 能否应用于B的T1事件触发 // //---------------------------- Active Low PWMs - Setup Deadband // // EPwm1Regs.DBCTL.bit.HALFCYCLE = 1; // Half cycle clocking enabled EPwm1Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE; EPwm1Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC; EPwm1Regs.DBCTL.bit.DEDB_MODE=0; //EPwm1Regs.DBCTL.bit.IN_MODE = DBA_ALL; EPwm1Regs.DBCTL.bit.IN_MODE =DBA_RED_DBB_FED; //A RED B FED+invert EPwm1Regs.DBRED.bit.DBRED = 8; //死区时间 DBFED × TTBCLK(10nS @100Mhz) EPwm1Regs.DBFED.bit.DBFED = 10; //-----ET------------------------触发ADC采样----------------------- EPwm1Regs.ETSEL.bit.SOCAEN = 1; /* Enable SOC on A group */ EPwm1Regs.ETSEL.bit.SOCASEL =1; //001: Enable event time-base counter equal to zero. (TBCTR = 0x00) EPwm1Regs.ETPS.bit.SOCPSSEL = 1; //EPWMxSOC A/B Pre-Scale Selection Bits 预分频 // EPwm1Regs.ETPS.bit.INTPSSEL=1; //EPWM int中断 // EPwm1Regs.ETPS.bit.SOCAPRD=1; EPwm1Regs.ETSOCPS.bit.SOCAPRD2 = 4; /* Generate pulse on 6st event */ // EPwm1Regs.ETCLR.bit.SOCA=1; //清除SOCA中断标志位 EPwm1Regs.TZSEL.bit.DCAEVT2 = 1; // Enable DCAEVT2 as a CBC trip source for this ePWM module EPwm1Regs.TZCBCCLR.bit.DCAEVT2 = 1; // Clear Flag for Digital Compare Output A Event 2 selected for CBC EPwm1Regs.TZCLR.bit.DCAEVT2=1 ; // Clear Flag for Digital Compare Output A Event 2 // 0: Writing 0 has no effect. This bit always reads back 0. // 1: Writing 1 clears the DCAEVT2 event trip condition. EPwm1Regs.TZCLR.bit.CBC=1 ; //Clear Flag for Cycle-By-Cycle (CBC) Trip Latch 清除中断标志TZFLG // 0: Has no effect. Always reads back a 0. // 1: Clears this Trip (set) condition. EPwm1Regs.TZCLR.bit.CBCPULSE=0; //00: CTR = zero pulse clears CBC trip latch. (Same as legacy designs.) //------------------B通道 DCBEVT2-------------------------------------- // EPwm1Regs.TZSEL.bit.DCBEVT2 = 1; // Enable DCAEVT2 as a CBC trip source for this ePWM module // EPwm1Regs.TZCBCCLR.bit.DCBEVT2 = 1; // Clear Flag for Digital Compare Output A Event 2 selected for CBC // EPwm1Regs.TZCLR.bit.DCBEVT2=1 ; // // EPwm1Regs.TZCLR.bit.CBCPULSE=0; //00: CTR = zero pulse clears CBC trip latch. (Same as legacy designs.) EPwm1Regs.TZCTL.bit.TZA = TZ_FORCE_LO; /* EPWM1A will go low 这是锁存的*/ // EPwm1Regs.TZCTL.bit.TZB = TZ_FORCE_LO;/* EPWM1B will go low */ EPwm1Regs.TZCTL.bit.TZB = TZ_NO_CHANGE; /* EPWM1B has no action 在AQ中动作*/ // EPwm1Regs.TZCTL.bit.DCAEVT2 = TZ_FORCE_LO; // 10: Force EPWMxA to a low state 保护不用 通过T1 T2事件进行动作 可以避免直通 这是不锁存的 // EPwm1Regs.TZCTL.bit.DCBEVT2 = TZ_NO_CHANGE; // 11: Do Nothing, trip action is disabled // EPwm1Regs.TZCTL.bit.DCAEVT2 = TZ_NO_CHANGE; //屏蔽DCA B动作 采用TZAB动作 // EPwm1Regs.TZCTL2.bit.ETZE = 1; //0: Use trip action from TZCTL (legacy EPWM compatibility) 1: Use trip action defined in TZCTL2, TZCTLDCA and TZCTLDCB. Settings in TZCTL are ignored EPwm1Regs.DCTRIPSEL.bit.DCAHCOMPSEL = 3; // Trip IN4 3 EPwm1Regs.DCTRIPSEL.bit.DCBHCOMPSEL = 3; // Trip 4 3 EPwm1Regs.TZDCSEL.bit.DCAEVT2 = TZ_DCAH_HI; /*000: Event disabled DCAH为高 产生一个DCAEVT2事件 001: DCAH = low, DCAL = don't care 010: DCAH = high, DCAL = don't care 011: DCAL = low, DCAH = don't care 100: DCAL = high, DCAH = don't care 101: DCAL = high, DCAH = low */ EPwm1Regs.TZDCSEL.bit.DCBEVT2 = TZ_DCBH_HI; //TRIP4 产生DCAH与DCBH事件,DCAH配置CBC跳闸触发TZA ,DCBH配置为事件T1 用于B pwm EPwm1Regs.DCACTL.bit.EVT2SRCSEL =1; // 0: Source Is DCAEVT2 Signal; 1: Source Is DCEVTFILT Signal TZ路径 EPwm1Regs.DCACTL.bit.EVT2FRCSYNCSEL =1; // 0: Source is synchronized with EPWMCLK; 1: Source is passed through asynchronously 通过sync生成DCAEVT2.FORCE EPwm1Regs.DCBCTL.bit.EVT2SRCSEL =0; // 0: Source Is DCBEVT2 Signal; 1: Source Is DCEVTFILT Signal EPwm1Regs.DCBCTL.bit.EVT2FRCSYNCSEL = 1; // 0: Source is synchronized with EPWMCLK; 1: Source is passed through asynchronously //---空窗设置---事件过滤--可不配置-------------------------------------------------------------------------- EPwm1Regs.DCFCTL.bit.SRCSEL = 1; // 01: Source Is DCAEVT2 Signal EPwm1Regs.DCFCTL.bit.BLANKE = 1; // 1: Blanking window is enabled EPwm1Regs.DCFCTL.bit.BLANKINV = 0; // 0: Blanking window not inverted; 1: Blanking window inverted EPwm1Regs.DCFCTL.bit.PULSESEL = 1; // 01: Time-base counter equal to zero //PWMSYNCSEL EPwm1Regs.HRPCTL.bit.PWMSYNCSELX = 0; // EPWMSYNCPER is defined by PWMSYNCSEL 0 EPWM1 EPwm1Regs.HRPCTL.bit.PWMSYNCSEL = 1; // 1:CTR = zero; 0:CTR = PRD EDIS; EPwm1Regs.DCFOFFSET =0; EPwm1Regs.DCFWINDOW = 20; //DCFWINDOW*TB_WINDOW(10nS @100Mhz) } struct pid{ double err; //定义偏差值 double err_last; //定义上一个偏差值 double err_pre; //定义上上一个偏差值 double Kp,Ki,Kd; //定义比例,积分,微分系数 double det_err_pi; double out_pi; } pid; //初始化变量 void pid_init() { pid.err=0; pid.err_last=0; pid.err_pre=0; pid.Kp=1.2; //kp=0.05;ki=0.01 PI参数调节 0.02 0.0015 pid.Ki=0.05; // pid.Kd=1; pid.out_pi=0; //初始duty pid.det_err_pi=0; } interrupt void adc_isr(void) { // i++; // GpioDataRegs.GPASET.bit.GPIO12 = 1;/* Set GPIO12 (for timing purposes) */ AdcaRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;/* Clr ADCINT1 flag for next SOC */ PieCtrlRegs.PIEACK.all = PIEACK_GROUP1;/* Acknowledge interrupt to PIE */ Vo_ave=((AdcaResultRegs.ADCRESULT0)+(AdcaResultRegs.ADCRESULT1)+(AdcaResultRegs.ADCRESULT2)+(AdcaResultRegs.ADCRESULT3))>>2; pid.err=Vo_ref-Vo_ave; pid.err=0.5*(pid.err+pid.err_last); if (pid.err<=5&&pid.err>=-5) pid.err=0; pid.out_pi=pid.out_pi+pid.Kp*(pid.err-pid.err_last)+pid.Ki*pid.err; pid.err_last=pid.err; if (pid.out_pi<0) pid.out_pi=0; if (pid.out_pi>65530) pid.out_pi=65530; Cmpss3Regs.RAMPMAXREFS=(pid.out_pi); //左移4位 DAC为12位 RAMPMAXREFS的高12位to DACHVALA 所以要左移4位 // GpioDataRegs.GPACLEAR.bit.GPIO12 = 1;/* Set GPIO12 (for timing purposes) */ // ; //观察i值,判断有无进入中断 return; } /**************************************************************************** // No more. ****************************************************************************/
你好,因为我对CMPSS模块的掌握度也不高,所以需要将你的问题升级到英文E2E论坛。但由于现在是美国的节假日期间,没有工程师支持。需要等到1月3日之后才会有工程师开始接管论坛。需要麻烦你在1月3日之后再整理一个帖子发布一下新帖,到时候为你升级。(因为旧贴可能被刷下去,新帖的话系统有提示)