This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: 芯片采取flash存取代码,但不知道下面这种用法是否影响执行速度?

Part Number: TMS320F28027


#pragma CODE_SECTION(epwm2_isr, "ramfuncs");
#pragma CODE_SECTION(detectZeroCrossingClearPWMTrip , "ramfuncs");
#pragma CODE_SECTION(updateInverterPWM, "ramfuncs");

#pragma DATA_SECTION (Spwm_table,".cio");
uint16_t Spwm_table[200]={0};

__interrupt void epwm2_isr(void){

detectZeroCrossingClearPWMTrip();

updateInverterPWM(Spwm_table[cnt++]);

EPwm2Regs.ETCLR.bit.INT = 1; //写1对ETFLG[INT]状态标志位清零,从而能进行下一次中断
PieCtrlRegs.PIEACK.all=PIEACK_GROUP3;
}

问题如下:

1.因为中断函数epwm2_isr已经使用#pragma CODE_SECTION(epwm2_isr, "ramfuncs")做了定位,函数detectZeroCrossingClearPWMTrip();和updateInverterPWM(Spwm_table[cnt++]);在中断函数中被调用 

  两个被调用的函数使用和不使用#pragma CODE_SECTION对执行速度有影响不?

2.数组uint16_t Spwm_table【200】 使用和不使用#pragma DATA_SECTION定位是否对程序的执行有影响不?

此外

/* Allocate uninitalized data sections: */
.stack : > RAMM0 PAGE = 1
.ebss : > DRAML0 PAGE = 1
.esysmem : > RAMM1 |DRAML0 PAGE = 1
.cio : >> RAMM1 | DRAML0 PAGE = 1

段cio 是否对stack 和esysmem有影响?

谢谢!

  • 1、有影响,复制到ram中运行的代码运行速度要比在flash中的快很多,如果函数detectZeroCrossingClearPWMTrip();和updateInverterPWM(Spwm_table[cnt++]);的执行时间很长或者对实时性要求很高的话,影响会很明显。

    2、如果只是存储数组的话我认为虽然存取速度会相差很大,但整体影响不大。

    3、stack没有影响,esysmem有影响。话说,cio和esysmem是同一个ram分区?

  • /*
    // TI File $Revision: /main/7 $
    // Checkin $Date: July 6, 2009   17:25:36 $
    //###########################################################################
    //
    // FILE:	F28027.cmd
    //
    // TITLE:	Linker Command File For F28027 Device
    //
    //###########################################################################
    // $TI Release: 2802x C/C++ Header Files and Peripheral Examples V1.29 $
    // $Release Date: January 11, 2011 $
    //###########################################################################
    */
    
    /* ======================================================
    // For Code Composer Studio V2.2 and later
    // ---------------------------------------
    // In addition to this memory linker command file,
    // add the header linker command file directly to the project.
    // The header linker command file is required to link the
    // peripheral structures to the proper locations within
    // the memory map.
    //
    // The header linker files are found in <base>\DSP2802_Headers\cmd
    //
    // For BIOS applications add:      DSP2802x_Headers_BIOS.cmd
    // For nonBIOS applications add:   DSP2802x_Headers_nonBIOS.cmd
    ========================================================= */
    
    /* ======================================================
    // For Code Composer Studio prior to V2.2
    // --------------------------------------
    // 1) Use one of the following -l statements to include the
    // header linker command file in the project. The header linker
    // file is required to link the peripheral structures to the proper
    // locations within the memory map                                    */
    
    /* Uncomment this line to include file only for non-BIOS applications */
    /* -l DSP2802x_Headers_nonBIOS.cmd */
    
    /* Uncomment this line to include file only for BIOS applications */
    /* -l DSP2802x_Headers_BIOS.cmd */
    
    /* 2) In your project add the path to <base>\DSP2802x_headers\cmd to the
       library search path under project->build options, linker tab,
       library search path (-i).
    /*========================================================= */
    
    /* Define the memory block start/length for the F28027
       PAGE 0 will be used to organize program sections
       PAGE 1 will be used to organize data sections
    
       Notes:
             Memory blocks on F2802x are uniform (ie same
             physical memory) in both PAGE 0 and PAGE 1.
             That is the same memory region should not be
             defined for both PAGE 0 and PAGE 1.
             Doing so will result in corruption of program
             and/or data.
    
             The L0 memory block is mirrored - that is
             it can be accessed in high memory or low memory.
             For simplicity only one instance is used in this
             linker file.
    
             Contiguous SARAM memory blocks or flash sectors can be
             be combined if required to create a larger memory block.
    
             FLASHD      : origin = 0x3F0000, length = 0x002000
             FLASHC      : origin = 0x3F2000, length = 0x002000
             FLASHB      : origin = 0x3F4000, length = 0x002000
    */
    
    MEMORY
    {
    PAGE 0:    /* Program Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */
    
       PRAML0      : origin = 0x008000, length = 0x000800     /* on-chip RAM block L0 */
       OTP         : origin = 0x3D7800, length = 0x000400     /* on-chip OTP */
       FLASHABCD2  : origin = 0x3F1000, length = 0x006F80     /* on-chip FLASH */
       CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
       BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
       CSM_PWL_P0  : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
    
       IQTABLES    : origin = 0x3FE000, length = 0x000B50     /* IQ Math Tables in Boot ROM */
       IQTABLES2   : origin = 0x3FEB50, length = 0x00008C     /* IQ Math Tables in Boot ROM */
       IQTABLES3   : origin = 0x3FEBDC, length = 0x0000AA	  /* IQ Math Tables in Boot ROM */
    
       ROM         : origin = 0x3FF27C, length = 0x000D44     /* Boot ROM */
       RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM  */
       VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM  */
    
    PAGE 1 :   /* Data Memory */
               /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
               /* Registers remain on PAGE1                                                  */
    
       BOOT_RSVD   : origin = 0x000000, length = 0x000050     /* Part of M0, BOOT rom will use this for stack */
       RAMM0       : origin = 0x000050, length = 0x0003B0     /* on-chip RAM block M0 */
       RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
       DRAML0      : origin = 0x008800, length = 0x000800     /* on-chip RAM block L0 */
       FLASHD1     : origin = 0x3F0000, length = 0x001000
    }
    
    /* Allocate sections to memory blocks.
       Note:
             codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code
                       execution when booting to flash
             ramfuncs  user defined section to store functions that will be copied from Flash into RAM
    */
    
    SECTIONS
    {
    
       /* Allocate program areas: */
       .cinit              : > FLASHABCD2       PAGE = 0
       .pinit              : > FLASHABCD2,      PAGE = 0
       .text               : > FLASHABCD2       PAGE = 0
       codestart           : > BEGIN        PAGE = 0
       ramfuncs            : LOAD = FLASHABCD2,
                             RUN = PRAML0,
                             LOAD_START(_RamfuncsLoadStart),
                             LOAD_END(_RamfuncsLoadEnd),
                             RUN_START(_RamfuncsRunStart),
                             PAGE = 0
    
       csmpasswds          : > CSM_PWL_P0   PAGE = 0
       csm_rsvd            : > CSM_RSVD     PAGE = 0
    
       /* Allocate uninitalized data sections: */
       .stack              : > RAMM0        PAGE = 1
       .ebss               : > DRAML0       PAGE = 1
       .esysmem            : > RAMM1 |DRAML0       PAGE = 1
       .cio                : >> RAMM1 | DRAML0    PAGE = 1// //.cio    这个在HFUPS文件开头            : >> RAMM1 | DRAML0 |  DRAMLL0     PAGE = 1//    .cio                : >> RAMM0 | RAMM1 | DRAML0       PAGE = 1
    
       /* Initalized sections go in Flash */
       /* For SDFlash to program these, they must be allocated to page 0 */
       .econst             : > FLASHABCD2       PAGE = 0
       .switch             : > FLASHABCD2       PAGE = 0
    
       /* Allocate IQ math areas: */
       IQmath              : > FLASHABCD2       PAGE = 0            /* Math Code */
       IQmathTables        : > IQTABLES,    	PAGE = 0, TYPE = NOLOAD
    
       /* Uncomment the section below if calling the IQNexp() or IQexp()
          functions from the IQMath.lib library in order to utilize the
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables2    : > IQTABLES2, PAGE = 0, TYPE = NOLOAD
       {
    
                  IQmath.lib<IQNexpTable.obj> (IQmathTablesRam)
    
       }
       */
       /* Uncomment the section below if calling the IQNasin() or IQasin()
          functions from the IQMath.lib library in order to utilize the
          relevant IQ Math table in Boot ROM (This saves space and Boot ROM
          is 1 wait-state). If this section is not uncommented, IQmathTables2
          will be loaded into other memory (SARAM, Flash, etc.) and will take
          up space, but 0 wait-state is possible.
       */
       /*
       IQmathTables3    : > IQTABLES3, PAGE = 0, TYPE = NOLOAD
       {
    
                  IQmath.lib<IQNasinTable.obj> (IQmathTablesRam)
    
       }
       */
    
       /* .reset is a standard section used by the compiler.  It contains the */
       /* the address of the start of _c_int00 for C Code.   /*
       /* When using the boot ROM this section and the CPU vector */
       /* table is not needed.  Thus the default type is set here to  */
       /* DSECT  */
       .reset              : > RESET,      PAGE = 0, TYPE = DSECT
       vectors             : > VECTORS     PAGE = 0, TYPE = DSECT
    
    }
    
    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */

    F207的CMD文件代码如上,此外当我再声明两个3个200个元素的uint16类型的数据就提示有误 这是怎么回事?谢谢!

  • 这个得看看提示的错误内容是什么?内存不匹配?