Part Number: TMS320F28335
Other Parts Discussed in Thread: UNIFLASH
1.我这边debug的时候有问题,在CCS中点击debug,烧录到flash的时候,提示如下:
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface28335V2_10.out
C28xx: Error occurred during flash operation: Timed out waiting for target to halt while executing FlashAPIInterface28335V2_10.out
C28xx: Flash operation timed out waiting for the algorithm to complete. Operation cancelled.
C28xx: File Loader: Memory write failed: Unknown error
C28xx: GEL: File: F:\WORK\ZKY\105\code\demo_for_105\Debug\demo_for_105.out: Load failed.
2.使用ccxml文件testconnection时,可以成功,
3.使用unifilash解锁,提示解锁成功,密码区也都是0xffff,但是使用uniflash擦除的时候,提示如下:
.4.如果是flash锁定了,下载到sram中应该可以,但是烧写到sram中的时候,提示这个
Break at address "0x3ff9ce" with no debug information available, or outside of program code.
在汇编中就一直卡在这一句 3ff9fa: 6F00 SB 0, UNC