This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在配置好CLA后发现调用EPWM4时会报错,因此更改了CMD文件中地址的大小,发现将CLA所用的地址范围加大后调用EPWM4不再报错,但是这个时候通过在线仿真可以看到duty值不再变化。在没修改CMD文件之前duty值是在变化的,修改之后虽然duty值没有变一直为0,但是我在CLA里将GPIO12拉高,通过示波器观察GPIO12确实为高电平,因此可以认为此时CLA在运行,只不过CLA中的变量duty值不变。
应该是我修改CMD文件的地址范围导致的,这个怎么解决?duty值不变是为什么?
MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 RAMM0 : origin = 0x0000F4, length = 0x000100C RAMLS0 : origin = 0x008000, length = 0x000800 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMLS4 : origin = 0x00A000, length = 0x001800 RESET : origin = 0x3FFFC0, length = 0x000002 /* Flash sectors: you can use FLASH for program memory when the RAM is filled up*/ /* BANK 0 */ FLASH_BANK0_SEC0 : origin = 0x080000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x001000 /* on-chip Flash */ /* BANK 1 */ FLASH_BANK1_SEC0 : origin = 0x090000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC1 : origin = 0x091000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC2 : origin = 0x092000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC3 : origin = 0x093000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC4 : origin = 0x094000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC5 : origin = 0x095000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC6 : origin = 0x096000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC7 : origin = 0x097000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC8 : origin = 0x098000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC9 : origin = 0x099000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC10 : origin = 0x09A000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC11 : origin = 0x09B000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC12 : origin = 0x09C000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC13 : origin = 0x09D000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC14 : origin = 0x09E000, length = 0x001000 /* on-chip Flash */ FLASH_BANK1_SEC15 : origin = 0x09F000, length = 0x001000 /* on-chip Flash */ PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x0000F1 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMLS5 : origin = 0x00B800, length = 0x000800 RAMLS6 : origin = 0x00C000, length = 0x000800 RAMLS7 : origin = 0x00C800, length = 0x000800 RAMGS0 : origin = 0x00D000, length = 0x002000 RAMGS1 : origin = 0x00F000, length = 0x002000 RAMGS2 : origin = 0x011000, length = 0x002000 RAMGS3 : origin = 0x013000, length = 0x001FF8 // RAMGS3_RSVD : origin = 0x013FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 } /*You can arrange the .text, .cinit, .const, .pinit, .switch and .econst to FLASH when RAM is filled up.*/ SECTIONS { codestart : > BEGIN, PAGE = 0 .TI.ramfunc : > RAMM0, PAGE = 0 .text : >>RAMLS0 | RAMLS2 | RAMLS3 | RAMLS4 | RAMM0, PAGE = 0 .cinit : > RAMM0, PAGE = 0 .switch : > RAMM0, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMM1, PAGE = 1 #if defined(__TI_EABI__) .bss : > RAMLS5, PAGE = 1 .bss:output : > RAMLS5, PAGE = 1 .init_array : > RAMM0, PAGE = 0 .const : > RAMLS5, PAGE = 1 .data : > RAMLS5, PAGE = 1 .sysmem : > RAMLS5, PAGE = 1 .bss:cio : > RAMLS0, PAGE = 0 #else .pinit : > RAMM0, PAGE = 0 .ebss : > RAMLS5, PAGE = 1 .econst : > RAMLS5, PAGE = 1 .esysmem : > RAMLS5, PAGE = 1 .cio : > RAMLS0, PAGE = 0 #endif ramgs0 : > RAMGS0, PAGE = 1 ramgs1 : > RAMGS1, PAGE = 1 dclfuncs : > RAMLS5, PAGE = 1 // CLA Sections Cla1Prog : > RAMLS1, PAGE = 0 .scratchpad : > RAMLS6, PAGE = 1 .bss_cla : > RAMLS6, PAGE = 1 .const_cla : > RAMLS6, PAGE = 1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 Cla1DataRam : > RAMLS7, PAGE = 1 cla_shared : > RAMLS6, PAGE = 1 CLADataLS1 : > RAMLS6, PAGE = 1 } /* //=========================================================================== // End of file. //=========================================================================== */
没想到ram大小跟PWM寄存器的值之间有什么关系。
你更新的是cmd文件中哪个值的范围?
另外,能否单步调试看一下程序具体如何运行的?
1、报错的内容是什么?
2、每段ram在芯片中都有固定的长度,你可以看一下芯片datasheet中的表 8-1. C28x Memory Map。加大RAMLS4的话影响到后面RAMLS5甚至RAMLS6的大小了,由此可能影响了duty的内存部分。
我看到cmd文件中只有.test段是用到RAMLS4的,可以试一下通过几个内存段合并使用的方式来加大总的ram内存。