This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280021: 使用ePWM触发ADC,使用ADCINT2中断,中断程序运行不正常

Part Number: TMS320F280021

Dear all:

在使用epwm触发ADC时,使用ADCA1配置为ADCINT1中断,程序可以正常运行,相关程序如下程序如下:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
EALLOW;
PieVectTable.ADCA1_INT = &adcA1ISR; // Function for ADCA interrupt 1
EDIS;
IER |= M_INT1;//T0 ADCINT1
PieCtrlRegs.PIEIER1.bit.INTx1 = 1;// ADCINT1
EPwm1Regs.ETSEL.bit.SOCAEN = 0; // Disable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 3; // Select SOC on up-count
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.bit.CMPA = 430; // Set compare A value to 2048 counts
EPwm1Regs.TBPRD = 862; // Set period to 4096 counts
EPwm1Regs.TBCTL.bit.CTRMODE = 3; // Freeze counter
AdcaRegs.ADCSOC0CTL.bit.CHSEL = 7; // SOC0 will convert pin A1
// 0:A0 1:A1 2:A2 3:A3
// 4:A4 5:A5 6:A6 7:A7
// 8:A8 9:A9 A:A10 B:A11
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

上面测试代码中在定时中使能ePWM 开启

EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // Unfreeze, and enter up count mode

转换80个周期,每个周期时间是17.2us, 使用 LED_FLASH=1; 测试管脚来查看转换的周期和每个周期的个位。

上述程序运行正常。

但是ADCINT1已经被其他功能占用,配置到ADCINT2 中断上,使用发现就不能正常运行,相关程序如下:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
EALLOW;
PieVectTable.ADCA2_INT = &adcA2ISR; // Function for ADCA interrupt 2
EDIS;
IER |= M_INT10; //ADCINT2
PieCtrlRegs.PIEIER10.bit.INTx2 = 1;// ADCINT2
EPwm1Regs.ETSEL.bit.SOCAEN = 0; // Disable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 3; // Select SOC on up-count
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.bit.CMPA = 430; // Set compare A value to 2048 counts
EPwm1Regs.TBPRD = 862; // Set period to 4096 counts
EPwm1Regs.TBCTL.bit.CTRMODE = 3; // Freeze counter
AdcaRegs.ADCSOC1CTL.bit.CHSEL = 7; // SOC1 will convert pin A1
// 0:A0 1:A1 2:A2 3:A3
// 4:A4 5:A5 6:A6 7:A7
// 8:A8 9:A9 A:A10 B:A11
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

通过示波器测试LED_FLASH=1; 管脚上的电平转换时间是20ms,运行不正常

也没查找出是什么具体原因。

原来之前使用的是28065也是这么使用,可以正常工作,插入一段28065的程序

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
PieVectTable.ADCINT1 = &adc_isr; // ADC Signal
PieVectTable.ADCINT2 = &adc_current_isr; // ADC current
IER |= M_INT1; // T0 ADCINT1
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // ADCINT1 P1.1
PieCtrlRegs.PIEIER1.bit.INTx2 = 1; // ADCINT2
EALLOW;
AdcRegs.ADCCTL1.bit.ADCREFSEL = 1; //
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN0 = 1; //
AdcRegs.ADCSOC0CTL.bit.CHSEL = 0; //soc
// AdcRegs.ADCSOC1CTL.bit.CHSEL = 8;
AdcRegs.ADCSOC0CTL.bit.ACQPS = 25; // 25
AdcRegs.ADCSOC1CTL.bit.ACQPS = 25;
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 1; //
AdcRegs.ADCSAMPLEMODE.bit.SIMULEN2 = 1; //
AdcRegs.ADCSOC2CTL.bit.CHSEL = 1; //soc
// AdcRegs.ADCSOC3CTL.bit.CHSEL = 9;
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

28065 ADCINT1和ADCINT2都能正常运行。

请大家帮忙分析280021 上如何正常使用ADCINT2,(ADCINT1已经被占用),并且必须是在PWM触发上去ADC中断。

  • 你好,粗看了一下代码,有一句:

    AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 1; // End of SOC0 will set INT2 flag

    按照注释的说明,应该是:

    AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 0; // End of SOC0 will set INT2 flag

    你看看这么修改是否有效。

  • 注释我忘记更改了,实际我配置到SOC1上

    EPwm1Regs.ETSEL.bit.SOCAEN = 0; // Disable SOC on A group
    EPwm1Regs.ETSEL.bit.SOCASEL = 3; // Select SOC on up-count
    EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event

    EPwm1Regs.CMPA.bit.CMPA = 430; // Set compare A value to 2048 counts
    EPwm1Regs.TBPRD = 862; // Set period to 4096 counts

    EPwm1Regs.TBCTL.bit.CTRMODE = 3; // Freeze counter

    AdcaRegs.ADCSOC1CTL.bit.CHSEL = 7; // SOC0 will convert pin A1
    // 0:A0 1:A1 2:A2 3:A3
    // 4:A4 5:A5 6:A6 7:A7
    // 8:A8 9:A9 A:A10 B:A11
    // C:A12 D:A13 E:A14 F:A15
    AdcaRegs.ADCSOC1CTL.bit.ACQPS = 9; // Sample window is 10 SYSCLK cycles
    AdcaRegs.ADCSOC1CTL.bit.TRIGSEL = 5; // Trigger on ePWM1 SOCA

    AdcaRegs.ADCINTSEL1N2.bit.INT2SEL = 1; // End of SOC1 will set INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT2E = 1; // Enable INT1 flag
    AdcaRegs.ADCINTSEL1N2.bit.INT2CONT = 0; //不连续
    AdcaRegs.ADCINTFLGCLR.bit.ADCINT2 = 1; // Make sure INT1 flag is cleared

    实际可以进入ADCINT2中断,只是进入中断的时间不是EPWM的周期触发的,固定20ms

  • 看到你发布了新帖,后续将在新帖中回复:e2echina.ti.com/.../tms320f280021-2800x-adc-pie-adcint1-adcint2