Other Parts Discussed in Thread: BOOSTXL-POSMGR, LAUNCHXL-F280049C
直接用TI提供的库Pm_tformat_lib_f280049c,在仿真板LAUNCHXL-F280049C+BOOSTXL-POSMGR上与多摩川编码器通信连接,未成功,查看Pm_tformat_lib原码,是应用于F28379D的,主要区别在PWM4B接口。看英文论坛有个人问过同样的问题但他没有贴出他最后的解决方案。我自己改编Pm_tformat_lib_f2837x,代码如下,但未能成功,没有CLB生成的时钟输出。有没有玩家知道什么原因吗。
1. 接口设置CLB4_BASE改为CLB1_BASE。
void PM_tformat_setupPeriph(uint32_t devLSPCLKFreq)//
{
tformat_resetCLB();
tformat_initCLB1();
CLB_configLocalInputMux(CLB1_BASE, CLB_IN0, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN1, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN2, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN3, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN4, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN5, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN6, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configLocalInputMux(CLB1_BASE, CLB_IN7, CLB_LOCAL_IN_MUX_GLOBAL_IN);
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN0, CLB_GLOBAL_IN_MUX_EPWM4A);//wenr
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN1, CLB_GLOBAL_IN_MUX_CLB_AUXSIG0);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN2, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN3, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN4, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN5, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN6, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGlobalInputMux(CLB1_BASE, CLB_IN7, CLB_GLOBAL_IN_MUX_EPWM4A);//
CLB_configGPInputMux(CLB1_BASE, CLB_IN0, CLB_GP_IN_MUX_GP_REG);
CLB_configGPInputMux(CLB1_BASE, CLB_IN1, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN2, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN3, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN4, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN5, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN6, CLB_GP_IN_MUX_EXTERNAL);
CLB_configGPInputMux(CLB1_BASE, CLB_IN7, CLB_GP_IN_MUX_GP_REG);//CLB_GP_IN_MUX_GP_REG
CLB_enableSynchronization(CLB1_BASE, CLB_IN0);
CLB_enableSynchronization(CLB1_BASE, CLB_IN1);
CLB_selectInputFilter(CLB1_BASE, CLB_IN0, CLB_FILTER_RISING_EDGE);
CLB_selectInputFilter(CLB1_BASE, CLB_IN1, CLB_FILTER_FALLING_EDGE);
tformat_initSPIFIFO(devLSPCLKFreq); // Initialize the SPI only
tformat_initCLBXBAR(); // Initialize the CLB XBARSPI only
}
2. CLB4的OUT2、OUT3、OUT4、OUT5输出改为CLB1的输出OUT0、OUT1、OUT2、OUT3、OUT4、OUT5。
void PM_tformat_startOperation(void)//
{
EALLOW;
HWREG(CLB1_BASE + CLB_LOGICCTL + CLB_O_LOAD_EN) |= CLB_LOAD_EN_GLOBAL_EN
| CLB_LOAD_EN_STOP;
__asm(" RPT #10 || NOP");
// CLB_setOutputMask(CLB1_BASE, 0x3C, true);
CLB_setOutputMask(CLB1_BASE, 0x3f, true);//
__asm(" RPT #10 || NOP");
CLB_setGPREG(CLB1_BASE, 0x81);
}
3. GPIO
void tformat_setupGPIO(void) {
//
// GPIO1 is SPI Clk slave
//
GPIO_setMasterCore(1, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_1_EPWM1_B);
//
// GPIO24 is the SPISIMOB
//
GPIO_setMasterCore(24, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_24_SPIB_SIMO);
GPIO_setQualificationMode(24, GPIO_QUAL_ASYNC);
//
// GPIO31 is the SPISOMIB
//
GPIO_setMasterCore(31, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_31_SPIB_SOMI);
GPIO_setQualificationMode(31, GPIO_QUAL_ASYNC);
//
// GPIO22 is the SPICLKB
//
GPIO_setMasterCore(22, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_22_SPIB_CLK);
GPIO_setQualificationMode(22, GPIO_QUAL_ASYNC);
//
// GPIO27 is the SPISTEB
//
GPIO_setMasterCore(27, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_27_SPIB_STE);
GPIO_setQualificationMode(27, GPIO_QUAL_ASYNC);
//
// GPIO7 is tformat TxEN
//
GPIO_setMasterCore(7, GPIO_CORE_CPU1);
GPIO_setPinConfig(GPIO_7_OUTPUTXBAR5);
//
// GPIO28 is PwrEN
//
GPIO_setMasterCore(28, GPIO_CORE_CPU1);
GPIO_setDirectionMode(28, GPIO_DIR_MODE_OUT);
}
4. XBAR
void tformat_configXBAR(void)
{
//
// Connect InputXbar-INPUT1 to GPIO24 - SPISIMO
//
XBAR_setInputPin(XBAR_INPUT1, 24);//
XBAR_setCLBMuxConfig(XBAR_AUXSIG0, XBAR_CLB_MUX01_INPUTXBAR1);//InputXbar-INPUT1 TO XBAR_CLB_MUX01
XBAR_enableCLBMux(XBAR_AUXSIG0, XBAR_MUX01);
XBAR_setOutputMuxConfig(XBAR_OUTPUT5, XBAR_OUT_MUX01_CLB1_OUT4);//
XBAR_enableOutputMux(XBAR_OUTPUT5, XBAR_MUX01);
}
5. PWMB
tformat_configEPWM1();
6. CLOCK
#define TFORMAT_FREQ_DIVIDER 10
我对比了两者的硬件电路,F280049C的电路SPIBSIMO采样GPIO24,BOOT电路也采用GPIO24并且上拉电阻,不知道有没有影响,准备拆掉上拉电阻试试。