咨询一下,之前配置的CMPSS1经过验证能够正常使用,按照CMPSS1的程序配置CMPSS2等另外的比较器发现无法实现功能,(已经查阅对应的模拟引脚内部连接状态表P1415和EPWM触发事件多路复用器EPWM_XBAR),能给出一些可能原因嘛???我有点想不明白,其他的比较器和CMPSS1在配置上还有什么具体的区别,按道理只要注意到引脚复用,以及触发的选择就应该没问题了。。。。。。期望尽快回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
咨询一下,之前配置的CMPSS1经过验证能够正常使用,按照CMPSS1的程序配置CMPSS2等另外的比较器发现无法实现功能,(已经查阅对应的模拟引脚内部连接状态表P1415和EPWM触发事件多路复用器EPWM_XBAR),能给出一些可能原因嘛???我有点想不明白,其他的比较器和CMPSS1在配置上还有什么具体的区别,按道理只要注意到引脚复用,以及触发的选择就应该没问题了。。。。。。期望尽快回复
您好,您是否方便提供一些详细信息?比如说,在配置CMPSS2时遇到了什么问题?
嗯,目前的问题是怎么样使用三个比较器输出连接到同一个EPWM——XBAR封锁脉冲,我目前只能做到两个比较器的使用,比如CMPSS1和CMPSS2分别触发DCAEVT1和DCBEVT1两个事件,封锁一个EPWM的脉冲,而且我发现有一个问题,在使用CBC模式时,内部给定的DAC和实际值差很多,大概有0.2V差距,这个可能的问题是什么。
您好,
目前的问题是怎么样使用三个比较器输出连接到同一个EPWM——XBAR封锁脉冲,我目前只能做到两个比较器的使用,比如CMPSS1和CMPSS2分别触发DCAEVT1和DCBEVT1两个事件,封锁一个EPWM的脉冲,
多个 CMPSSS 可通过组合的输入连接到单个 ePWM。 请参见下图:
而且我发现有一个问题,在使用CBC模式时,内部给定的DAC和实际值差很多,大概有0.2V差距,这个可能的问题是什么。
您能再解释一下吗?该问题是在 DAC 静态驱动时还是在斜坡发生器?