This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我现在正在学习使用28377D和SYSBIOS,遇见几个问题:
1.关于Task模块,请问,如何实现6个任务(编号1-6),按优先级顺序执行一遍,然后返回任务1继续循环执行?
目前我的方法是:在每个任务里加while(1),程序放在while中,然后在程序的最后(即一次while循环结束之前)使用Task_setPri调整任务的优先级,请问有优化解决方案吗?
2.关于Hwi和中断向量表的问题:28377D技术手册给出了详细的中断映射,例如Int1.7对应timer0,Int1.13对应IPC0,Int9.5对应CANA_0,但是sysbios API Documentation中关于c28 Hwi的部分仅给出了中断号,并未明确指出是否一一对应;另外,在测试Hwi时,使用中断号130(即Int1.11)新建Hwi,通过Hwi_post(130)也可实现中断调用,中断号130(即Int1.11)在向量表中标为Reserved,请问如何理解Reserved中断?
3.关于28377D程序烧写,已知方法有JTAG(正在使用),SCI(正在学习)/CAN,但是这几种方法都是有线烧写。请问28377D是否支持无线烧写,有相关资料可以学习吗?
4.关于SYSBIOS,除了User‘s Guide文件和API Documentation,还有其他资料可以学习吗?
非常感谢您的回复!
你好,很抱歉的是这边对SYS/BIOS了解很少,关于SYS/BIOS的问题只能麻烦你移步至英文论坛去咨询一下:
这边目前还没有碰到过无线烧写的,最多就是基于各种通信协议的远程烧写,常见的比如基于SCI,CAN的