This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28035: C2Prog 燒錄問題

Part Number: TMS320F28035

Hi

請問我們在使用C2Prog 燒錄時軟體顯示no response

但一樣透過這個SCI介面單純通訊傳遞封包卻沒問題

確認過燒錄時應該是已經進入boot mode

實際量測SCI之波形如下

進到28035 RX(YELLO)

28035無反應(BLUE)

是否還有需要確認之地方?

When we use C2PROG 1.8.11-7 to record the software, the software show No Response

But through this SCI interface, normal communicating packets had no problem

We confirmed that the 28035 has be in Boot Mode

The waveform of the actual measurement of SCI in 28035 pin is as follows

28035 RX input pin (YELLO)

28035 had no response in Tx output pin(Blue)

Is there any point to confirm to solve this problem?

系統架構如下

The architecture is as follows

Thanks