Part Number: TMS320F28035
Hi
請問我們在使用C2Prog 燒錄時軟體顯示no response
但一樣透過這個SCI介面單純通訊傳遞封包卻沒問題
確認過燒錄時應該是已經進入boot mode
實際量測SCI之波形如下
進到28035 RX(YELLO)
28035無反應(BLUE)
是否還有需要確認之地方?
When we use C2PROG 1.8.11-7 to record the software, the software show No Response
But through this SCI interface, normal communicating packets had no problem
We confirmed that the 28035 has be in Boot Mode
The waveform of the actual measurement of SCI in 28035 pin is as follows
28035 RX input pin (YELLO)
28035 had no response in Tx output pin(Blue)
Is there any point to confirm to solve this problem?

系統架構如下
The architecture is as follows

Thanks