请教专家:
编译出现下列提示:
"../CMD/F28335.cmd", line 59: warning: no matching section
warning: creating output section "PartIdRegsFile" without a SECTIONS specification
warning: entry-point symbol other than "_c_int00" specified: "code_start"
{
F28335.cmd", line 59 是: IQmath_fpu32.lib<IQNexpTable.obj> (IQmathTablesRam)
}
仿真运行就会进入:
interrupt void ILLEGAL_ISR(void) // Illegal operation TRAP
{
// Insert ISR Code here
// Next two lines for debug only to halt the processor here
// Remove after inserting ISR Code
asm(" ESTOP0");
for(;;);
}
我用的是 DSP2833x_Headers_nonBIOS.cmd 和 F28335.cmd
请教怎么解决? ILLEGAL_ISR 是什么中断?
我需用IQmath,程序其他部份都正常.但加入IQmath就出错.应该怎么做?