根据emif1_16bit_asram.c修改,配置EMIF模块,在写的过程中EMIWE被拉低两次。这是怎么回事。

代码如下:
//###########################################################################
//
// FILE: emif1_16bit_asram.c
//
// TITLE: EMIF1 module accessing 16bit ASRAM.
//
//! \addtogroup cpu01_example_list
//! <h1> EMIF ASYNC module (emif1_16bit_asram)</h1>
//!
//! This example configures EMIF1 in 16bit ASYNC mode
//! This example uses CS2 as chip enable.
//!
//! \b Watch \b Variables: \n
//! - \b TEST_STATUS - Equivalent to \b TEST_PASS if test finished correctly,
//! else the value is set to \b TEST_FAIL
//! - \b ErrCount - Error counter
//!
//
//###########################################################################
//
// $Release Date: $
// $Copyright:
// Copyright (C) 2013-2022 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "F28x_Project.h"
#define ASRAM_CS2_START_ADDR 0x100000
#define ASRAM_CS2_SIZE 0x8000
//
// Globals
//
Uint16 ErrCount = 0;
Uint32 TEST_STATUS;
int i;
//
// Function Prototypes
//
extern void setup_emif1_pinmux_async_16bit(Uint16);
// mem_read_write - This function performs simple read/write word accesses to memory.
char mem_read_write(Uint32 start_addr, Uint32 mem_size)
{
//unsigned long mem_rds;
unsigned long mem_wds;
long *XMEM_ps;
//unsigned int i;
//Write data
XMEM_ps = (long *)start_addr;
//Fill memory
mem_wds = 0x1;
//for (i=0; i < mem_size; i++)
//{
//*XMEM_ps++ = mem_wds;
*XMEM_ps = mem_wds;
// mem_wds += 0x11111111;
//}
/*
//Verify memory
mem_wds = 0x01234567;
XMEM_ps = (long *)start_addr;
for (i=0; i < mem_size; i++)
{
mem_rds = *XMEM_ps;
if( mem_rds != mem_wds)
{
return(1);
}
XMEM_ps++;
mem_wds += 0x11111111;
}
*/
return(0);
}
void main(void)
{
char ErrCount_local;
//TEST_STATUS = TEST_FAIL;
//
// Initialize system control
//
InitSysCtrl();
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2837xD_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags:
//
EALLOW;
IER = 0x0000;
IFR = 0x0000;
EDIS;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// GService Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
InitPieVectTable();
//
//Configure to run EMIF1 on full Rate (EMIF1CLK = CPU1SYSCLK)
//
EALLOW;
ClkCfgRegs.PERCLKDIVSEL.bit.EMIF1CLKDIV = 0x0;
EDIS;
EALLOW;
//
// Grab EMIF1 For CPU1
//
Emif1ConfigRegs.EMIF1MSEL.all = 0x93A5CE71;
if(Emif1ConfigRegs.EMIF1MSEL.all != 0x1)
{
ErrCount++;
}
//
//Disable Access Protection (CPU_FETCH/CPU_WR/DMA_WR)
//
Emif1ConfigRegs.EMIF1ACCPROT0.all = 0x0;
if(Emif1ConfigRegs.EMIF1ACCPROT0.all != 0x0)
{
ErrCount++;
}
//
// Commit the configuration related to protection. Till this bit remains set
// content of EMIF1ACCPROT0 register can't be changed.
//
Emif1ConfigRegs.EMIF1COMMIT.all = 0x1;
if(Emif1ConfigRegs.EMIF1COMMIT.all != 0x1)
{
ErrCount++;
}
//
// Lock the configuration so that EMIF1COMMIT register can't be
// changed any more.
//
Emif1ConfigRegs.EMIF1LOCK.all = 0x1;
if(Emif1ConfigRegs.EMIF1LOCK.all != 1)
{
ErrCount++;
}
EDIS;
EALLOW;
GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1;//配置方向:0输入;1输出
GpioCtrlRegs.GPBDIR.bit.GPIO33 = 1;
GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;//上拉:0使能上拉;1禁止上拉
GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;
GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1;//数据清除:写0无效;写1置为低电平
GpioDataRegs.GPBCLEAR.bit.GPIO33 = 1;//数据清除:写0无效;写1置为低电平
EDIS;
//
//Configure GPIO pins for EMIF1
//
setup_emif1_pinmux_async_16bit(0);
Emif1Regs.ASYNC_CS2_CR.bit.ASIZE = 1;//1:0
Emif1Regs.ASYNC_CS2_CR.bit.TA= 10; //3:2
//Emif1Regs.ASYNC_CS2_CR.bit.R_HOLD= 0;//6:4
//Emif1Regs.ASYNC_CS2_CR.bit.R_STROBE = 0;//12:7
//Emif1Regs.ASYNC_CS2_CR.bit.R_SETUP = 0;//16:13
Emif1Regs.ASYNC_CS2_CR.bit.W_HOLD =0;//19:17
Emif1Regs.ASYNC_CS2_CR.bit.W_STROBE =2;//25:20
Emif1Regs.ASYNC_CS2_CR.bit.W_SETUP =0;//29:26
Emif1Regs.ASYNC_CS2_CR.bit.EW = 0;//30
Emif1Regs.ASYNC_CS2_CR.bit.SS = 0;//31
while (1)
{
ErrCount_local = mem_read_write(ASRAM_CS2_START_ADDR, ASRAM_CS2_SIZE);
ErrCount = ErrCount + ErrCount_local;
DELAY_US(100);
}
}