最近在用2812的AD进行模拟信号的采集,2812数据表上写着AD是十二位的,但是我采集同一电平怎么后3位数据一直在跳动?
有什么好的办法能提高精度吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
12位是标称精度,对于标准的直流源来说的,真正表征ADC转换精度的是一个叫做ENOB(有效位数Effective Number of Bits)的参数,具体定义可以参考F281x数据6.30.8章节,而F281x的ENOB是10.1. 另外三个参数也能说明采样结果的精度,即DNL/INL, offset error和gain error. 通常来讲,主要影响因素在后两个,具体参数也可以在6.30.2章节查到。
对你的应用而言,有几个建议:
1. 选用外部相对精准的ADC电压参考;
2. 确定你的模拟信号是直接电阻分压还是经过运放?需要保证输入到芯片ADC引脚的信号稳定;
3. 根据使用的频率确定外部电阻的大小符合要求;
4. 输入零电压确定offset error,再输入满量程电压确定gain error,根据应用文档F2810, F2811, and F2812 ADC Calibration Application Report (literature number SPRA989)进行软件补偿。
以上内容也都可以在6.30.2章节的注脚部分找到。
希望对你的应用有所帮助。