This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: 芯片的应用问题

Part Number: TMS320F280025


我现在在使用F280025的时候有点疑问,麻烦帮忙解答一下
我使用cmpss模块对AD口电压进行检测比较,检测有效后触发TZ封波。发现保护时间与设计偏差比较大
这是我cmpss的配置,理论保护时间是500ns,实测是1.56us

  • 你好,你的程序是运行在ram还是flash中的?

    另外,你是根据什么说明来设计的“理论保护时间是500ns”呢?


  • 程序运行在ram

    这是datasheet的描述


    我设置的CLKPRESCALE是2,SAMWIN是25,SYSCLK是100M

  • 收到,我需要与CMPSS方面的专家沟通一下后确认问题了再回复你,还请耐心等待。

  • 你好,有没有确保将 THRESH 加载到大于 SAMPWIN/2 的值?另外还需要在配置好之后进行 FILINT 才能正常工作。

  • Dear Green,你说的都做到了,没用诶.

    另外这是我们cmpss--xbar--pwm的寄存器配置.

    1. CMPSS configuration

    #define CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL  1

    #define CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW    25

    //CMPSS1-input1

        // Select the value for CMPHPM[object Object]SEL.

        ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1,CFG_BSP_IU_CMPSS_INPUT_NUM);

        // Select the value for CMPLPM[object Object]SEL.

        ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_1,CFG_BSP_IU_CMPSS_INPUT_NUM);

        CMPSS_configHighComparator(CFG_BSP_IU_CMPSS_BASE,(CMPSS_INSRC_DAC));

        // Sets the configuration for the Low comparator.

        CMPSS_configLowComparator(CFG_BSP_IU_CMPSS_BASE,(CMPSS_INSRC_DAC)| CMPSS_INV_INVERTED);

        // Sets the configuration for the internal comparator DACs.

        CMPSS_configDAC(CFG_BSP_IU_CMPSS_BASE,(CMPSS_DACVAL_SYSCLK | CMPSS_DACREF_VDDA | CMPSS_DACSRC_SHDW));

        // Sets the value of the internal DAC of the high comparator.

        CMPSS_setDACValueHigh(CFG_BSP_IU_CMPSS_BASE,2048 + CFG_BSP_IU_CMPSS_HIGH_VALUE);

        // Sets the value of the internal DAC of the low comparator.

        CMPSS_setDACValueLow(CFG_BSP_IU_CMPSS_BASE, 2048 - CFG_BSP_IU_CMPSS_LOW_VALUE);

        //  Configures the digital filter of the high comparator.

        CMPSS_configFilterHigh(CFG_BSP_IU_CMPSS_BASE, CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL, CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW, (CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW / 2) + 1u);

        // Configures the digital filter of the low comparator.

        CMPSS_configFilterLow(CFG_BSP_IU_CMPSS_BASE, CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL, CFG_BSP_IU_CMPSS_LOW_SAMPLEWINDOW, (CFG_BSP_IU_CMPSS_LOW_SAMPLEWINDOW / 2) + 1u);

      CMPSS_initFilterHigh(CFG_BSP_IU_CMPSS_BASE);

        CMPSS_initFilterLow(CFG_BSP_IU_CMPSS_BASE);

        CMPSS_configOutputsHigh(CFG_BSP_IU_CMPSS_BASE,(CMPSS_TRIPOUT_FILTER | CMPSS_TRIP_FILTER));

        // Sets the output signal configuration for the low comparator.

        CMPSS_configOutputsLow(CFG_BSP_IU_CMPSS_BASE, (CMPSS_TRIPOUT_FILTER | CMPSS_TRIP_FILTER));

        // Sets the comparator hysteresis settings.

        CMPSS_setHysteresis(CFG_BSP_IU_CMPSS_BASE,1U);

        CMPSS_clearFilterLatchHigh(CFG_BSP_IU_CMPSS_BASE);

        CMPSS_clearFilterLatchLow(CFG_BSP_IU_CMPSS_BASE);

        CMPSS_disableLatchResetOnPWMSYNCHigh(CFG_BSP_IU_CMPSS_BASE);

        // Disables reset of LOW comparator digital filter output latch on PWMSYNC

        CMPSS_disableLatchResetOnPWMSYNCLow(CFG_BSP_IU_CMPSS_BASE);

        // Sets the ePWM module blanking signal that holds trip in reset.

        CMPSS_configBlanking(CFG_BSP_IU_CMPSS_BASE,1U);

        // Disables an ePWM blanking signal from holding trip in reset.

        CMPSS_disableBlanking(CFG_BSP_IU_CMPSS_BASE);

        // Configures whether or not the digital filter latches are reset by PWMSYNC

    CMPSS_configLatchOnPWMSYNC(CFG_BSP_IU_CMPSS_BASE,false,false);

     

    1. XBAR configuration

     XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH_OR_L);

        XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00);

        XBAR_setEPWMMuxConfig(XBAR_TRIP5, XBAR_EPWM_MUX04_CMPSS3_CTRIPH_OR_L);

        XBAR_enableEPWMMux(XBAR_TRIP5, XBAR_MUX04);

        XBAR_setEPWMMuxConfig(XBAR_TRIP7, XBAR_EPWM_MUX02_CMPSS2_CTRIPH_OR_L);

        XBAR_enableEPWMMux(XBAR_TRIP7, XBAR_MUX02);

        XBAR_setEPWMMuxConfig(XBAR_TRIP8, XBAR_EPWM_MUX06_CMPSS4_CTRIPH_OR_L);

    XBAR_enableEPWMMux(XBAR_TRIP8, XBAR_MUX06);

     

    1. EPWM configuration

    EPWM_setTripZoneAction(EPWM1_BASE, EPWM_TZ_ACTION_EVENT_TZA,

                               EPWM_TZ_ACTION_HIGH_Z);

        // Trigger event when DCAH is high

        //

        EPWM_setTripZoneDigitalCompareEventCondition(EPWM1_BASE,

                                                     EPWM_TZ_DC_OUTPUT_A1,

                                                     EPWM_TZ_EVENT_DCXH_HIGH);

        //

        // Configure DCAH to use TRIP4  OR TRIP5 as an input

        //

        EPWM_enableDigitalCompareTripCombinationInput(EPWM1_BASE,

                                                      (EPWM_DC_COMBINATIONAL_TRIPIN4 | EPWM_DC_COMBINATIONAL_TRIPIN5

                                                      |EPWM_DC_COMBINATIONAL_TRIPIN7 | EPWM_DC_COMBINATIONAL_TRIPIN8),

                                                      EPWM_DC_TYPE_DCAH);

        // Enable DCA as OST

        //

        EPWM_enableTripZoneSignals(EPWM1_BASE, EPWM_TZ_SIGNAL_DCAEVT1);

     

        //

        // Configure the DCA path to be unfiltered and asynchronous

        //

        EPWM_setDigitalCompareEventSource(EPWM1_BASE,

                                          EPWM_DC_MODULE_A,

                                          EPWM_DC_EVENT_1,

                                          EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL);

     

        EPWM_setDigitalCompareEventSyncMode(EPWM1_BASE,

                                            EPWM_DC_MODULE_A,

                                            EPWM_DC_EVENT_1,

                                            EPWM_DC_EVENT_INPUT_NOT_SYNCED);

    CMPSS configuration.docx

  • 好的,我已经反馈给工程师了,还请耐心等待回复。

  • 你好,看到你已经在跟那个帖子了,我把链接贴这里:

    e2e.ti.com/.../tms320f280025-timing-of-cmpss-trigger-tz