Part Number: TMS320F280025
我现在在使用F280025的时候有点疑问,麻烦帮忙解答一下
我使用cmpss模块对AD口电压进行检测比较,检测有效后触发TZ封波。发现保护时间与设计偏差比较大
这是我cmpss的配置,理论保护时间是500ns,实测是1.56us
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025
我现在在使用F280025的时候有点疑问,麻烦帮忙解答一下
我使用cmpss模块对AD口电压进行检测比较,检测有效后触发TZ封波。发现保护时间与设计偏差比较大
这是我cmpss的配置,理论保护时间是500ns,实测是1.56us
你好,你的程序是运行在ram还是flash中的?
另外,你是根据什么说明来设计的“理论保护时间是500ns”呢?
Dear Green,你说的都做到了,没用诶.
另外这是我们cmpss--xbar--pwm的寄存器配置.
#define CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL 1
#define CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW 25
//CMPSS1-input1
// Select the value for CMPHPM[object Object]SEL.
ASysCtl_selectCMPHPMux(ASYSCTL_CMPHPMUX_SELECT_1,CFG_BSP_IU_CMPSS_INPUT_NUM);
// Select the value for CMPLPM[object Object]SEL.
ASysCtl_selectCMPLPMux(ASYSCTL_CMPLPMUX_SELECT_1,CFG_BSP_IU_CMPSS_INPUT_NUM);
CMPSS_configHighComparator(CFG_BSP_IU_CMPSS_BASE,(CMPSS_INSRC_DAC));
// Sets the configuration for the Low comparator.
CMPSS_configLowComparator(CFG_BSP_IU_CMPSS_BASE,(CMPSS_INSRC_DAC)| CMPSS_INV_INVERTED);
// Sets the configuration for the internal comparator DACs.
CMPSS_configDAC(CFG_BSP_IU_CMPSS_BASE,(CMPSS_DACVAL_SYSCLK | CMPSS_DACREF_VDDA | CMPSS_DACSRC_SHDW));
// Sets the value of the internal DAC of the high comparator.
CMPSS_setDACValueHigh(CFG_BSP_IU_CMPSS_BASE,2048 + CFG_BSP_IU_CMPSS_HIGH_VALUE);
// Sets the value of the internal DAC of the low comparator.
CMPSS_setDACValueLow(CFG_BSP_IU_CMPSS_BASE, 2048 - CFG_BSP_IU_CMPSS_LOW_VALUE);
// Configures the digital filter of the high comparator.
CMPSS_configFilterHigh(CFG_BSP_IU_CMPSS_BASE, CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL, CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW, (CFG_BSP_IU_CMPSS_HIGH_SAMPLEWINDOW / 2) + 1u);
// Configures the digital filter of the low comparator.
CMPSS_configFilterLow(CFG_BSP_IU_CMPSS_BASE, CFG_BSP_CURR_CMPSS_FILTER_CLK_PRESCAL, CFG_BSP_IU_CMPSS_LOW_SAMPLEWINDOW, (CFG_BSP_IU_CMPSS_LOW_SAMPLEWINDOW / 2) + 1u);
CMPSS_initFilterHigh(CFG_BSP_IU_CMPSS_BASE);
CMPSS_initFilterLow(CFG_BSP_IU_CMPSS_BASE);
CMPSS_configOutputsHigh(CFG_BSP_IU_CMPSS_BASE,(CMPSS_TRIPOUT_FILTER | CMPSS_TRIP_FILTER));
// Sets the output signal configuration for the low comparator.
CMPSS_configOutputsLow(CFG_BSP_IU_CMPSS_BASE, (CMPSS_TRIPOUT_FILTER | CMPSS_TRIP_FILTER));
// Sets the comparator hysteresis settings.
CMPSS_setHysteresis(CFG_BSP_IU_CMPSS_BASE,1U);
CMPSS_clearFilterLatchHigh(CFG_BSP_IU_CMPSS_BASE);
CMPSS_clearFilterLatchLow(CFG_BSP_IU_CMPSS_BASE);
CMPSS_disableLatchResetOnPWMSYNCHigh(CFG_BSP_IU_CMPSS_BASE);
// Disables reset of LOW comparator digital filter output latch on PWMSYNC
CMPSS_disableLatchResetOnPWMSYNCLow(CFG_BSP_IU_CMPSS_BASE);
// Sets the ePWM module blanking signal that holds trip in reset.
CMPSS_configBlanking(CFG_BSP_IU_CMPSS_BASE,1U);
// Disables an ePWM blanking signal from holding trip in reset.
CMPSS_disableBlanking(CFG_BSP_IU_CMPSS_BASE);
// Configures whether or not the digital filter latches are reset by PWMSYNC
CMPSS_configLatchOnPWMSYNC(CFG_BSP_IU_CMPSS_BASE,false,false);
XBAR_setEPWMMuxConfig(XBAR_TRIP4, XBAR_EPWM_MUX00_CMPSS1_CTRIPH_OR_L);
XBAR_enableEPWMMux(XBAR_TRIP4, XBAR_MUX00);
XBAR_setEPWMMuxConfig(XBAR_TRIP5, XBAR_EPWM_MUX04_CMPSS3_CTRIPH_OR_L);
XBAR_enableEPWMMux(XBAR_TRIP5, XBAR_MUX04);
XBAR_setEPWMMuxConfig(XBAR_TRIP7, XBAR_EPWM_MUX02_CMPSS2_CTRIPH_OR_L);
XBAR_enableEPWMMux(XBAR_TRIP7, XBAR_MUX02);
XBAR_setEPWMMuxConfig(XBAR_TRIP8, XBAR_EPWM_MUX06_CMPSS4_CTRIPH_OR_L);
XBAR_enableEPWMMux(XBAR_TRIP8, XBAR_MUX06);
EPWM_setTripZoneAction(EPWM1_BASE, EPWM_TZ_ACTION_EVENT_TZA,
EPWM_TZ_ACTION_HIGH_Z);
// Trigger event when DCAH is high
//
EPWM_setTripZoneDigitalCompareEventCondition(EPWM1_BASE,
EPWM_TZ_DC_OUTPUT_A1,
EPWM_TZ_EVENT_DCXH_HIGH);
//
// Configure DCAH to use TRIP4 OR TRIP5 as an input
//
EPWM_enableDigitalCompareTripCombinationInput(EPWM1_BASE,
(EPWM_DC_COMBINATIONAL_TRIPIN4 | EPWM_DC_COMBINATIONAL_TRIPIN5
|EPWM_DC_COMBINATIONAL_TRIPIN7 | EPWM_DC_COMBINATIONAL_TRIPIN8),
EPWM_DC_TYPE_DCAH);
// Enable DCA as OST
//
EPWM_enableTripZoneSignals(EPWM1_BASE, EPWM_TZ_SIGNAL_DCAEVT1);
//
// Configure the DCA path to be unfiltered and asynchronous
//
EPWM_setDigitalCompareEventSource(EPWM1_BASE,
EPWM_DC_MODULE_A,
EPWM_DC_EVENT_1,
EPWM_DC_EVENT_SOURCE_ORIG_SIGNAL);
EPWM_setDigitalCompareEventSyncMode(EPWM1_BASE,
EPWM_DC_MODULE_A,
EPWM_DC_EVENT_1,
EPWM_DC_EVENT_INPUT_NOT_SYNCED);