This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: 芯片的指令支持16位和32位,在软件工程的哪里设定实际采用的指令长度?

Part Number: TMS320F28335


在芯片的指令集说明手册里,写到28335支持16bit或32bit的指令,在哪里可以进行设定实际工程的指令长度?指令设置为16位时程序读数据总线还是32位的,那一次读两条指令同时进行处理?还是读一条指令处理?

  • 你好,C28是一个32位的架构,所以他是能识别16位指令。关于读取的话这个文档还有一个地方有如下说明:

    The instruction-fetch mechanism fetches 32-bits at a time from program memory; it fetches one 32-bit instruction or two 16-bit instructions.