Part Number: TMS320F28069
Other Parts Discussed in Thread: UNIFLASH
芯片丝印TMS320F28069PZT,使用也没什么问题。但是发现它的密码区,即0x3F7FF8开始的16个Uint16全部是0x0000,正常来说,这应该是一颗彻底锁死的芯片。但实际我通过SCIA更新固件完全正常。
即使把FLASHA全部擦除,0x3F7FF8开始的16个Uint16还是全部为0x0000,我尝试写入未加密固件,或者加密(密码不是全0)的固件,从0x3F7FF8读出来的16个Uint16始终全部是0x0000.
读取0x3D7E80的PARTID为0x009E,说明是TMS320F28069PZP/PZ,似乎没有什么问题。但是读取0x880开始的PF0内容全部都是0,0x0882地址的CLASSID和0x0883地址的REVID全部都是0x0000,感觉不太正常。
是买到假芯片了?还是设置错误导致的?