Part Number: TMS320F28335
我在使用TMS320F28335芯片做片内FLASH操作时,用到了官方的库文件Flash28335_API_V210.lib,在编译链接的时候,会报如下错误:“error #16008-D: file "F:/Protjects/PCS/PCS_CFG/soft/trunk/TI28335/libs/Flash28335_API_V210.lib" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line error #16008-D: file "F:/Protjects/PCS/PCS_CFG/soft/trunk/TI28335/libs/Flash28335_API_V210.lib" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2700" specified in a previous file or on the command line”,我们的工程里float_support由于别的原因选的是softlib方式,不是fpu32,而这个库Flash28335_API_V210.lib可能是基于fpu32编译的,所以产生了冲突,我想咨询一下是否有基于softlib方式编译的Flash28335_API_V210.lib库文件,谢谢!