This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Description Resource Path Location Type
build attribute vendor section TI missing in Sensored-BLDC C/C++ Problem
Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 6.0.1 [C2000]. Another version of the compiler will be used during build: 6.1.0. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. Sensored-BLDC properties TI Problem Marker
不这道这两个警告是什么意思,怎么解决
如果 忽略 着两警告, 程序可以下载到控制器里面去, 但是一点击运行就出现这样的提升
:C28xx: Error: (Error -1135 @ 0x8000) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.872.0)