Description Resource Path Location Type
build attribute vendor section TI missing in Sensored-BLDC C/C++ Problem
Description Resource Path Location Type
This project was created using a version of compiler that is not currently installed: 6.0.1 [C2000]. Another version of the compiler will be used during build: 6.1.0. Please install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. Sensored-BLDC properties TI Problem Marker
不这道这两个警告是什么意思,怎么解决