同样的安装包,在其它的电脑上顺利安装过,正常使用中,新买的X230i也可以顺利安装,但是安装完了以后点击“CCStudio v3.3”图标闪退,事件查看器中没有任何痕迹,“Setup CCStudio v3.3”可以顺利运行并设置。安装完运行CCS前安装了6.0.2的cgt。
X230i的配置为赛扬877CPU,2G内存。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不确定是否跟操作系统有关,或者你的安装包是否存在问题。
建议到下面网址下载,并使用最新版的CCS v5,TI官方以后将不再支持3.3:
我在第一次使用win7安装的CCS3.3的时候也遇到过,就是闪退的问题,当时也觉得很棘手很头痛。
最后我是用这个方法成功解决的闪退的问题的,目前为止运行编译都正常,在这提供给你参考一下,你可以试试:
我win7成功安装并运行ccs3.3的经验:
(1)安装过程中出现缺失文件ignore;
(2)安装完成之后右键点击CCS3.3的图标》选择Properties;
(3)compatibility中》勾选run this program in compatibility mode for:》windows XP(Service Pack 2)
不过在TI的官方网站上 已经停止提供CCS3.3的下载链接了,以后对3.3的支持也会减少。
所以,建议试试新版本5.4吧,要是有条件的话。