This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301-HC-C2-KIT: 关于I-TOTAL与实际母线电流对应关系的疑问

Part Number: DRV8301-HC-C2-KIT


以上路径中的原理图中,设计母线电流采集电路如下:

放大电路倍率为30,偏置电压1.65V,电动情况下,母线电流只有正向电流,也就是说母线电流从0A到MAX对应的电压变化为1.65V(母线电流0A运放输出1.65V,母线电流最大时运放输出3.3V)

请问这个电路,运放输出电压值和实际母线电流是什么关系呢?

我可以这样计算吗:

1.65V Heavy division sign 30 = 0.055V

0.055VHeavy division sign0.002ohm = 27.5A

27.5A x 3 = 82.5A,也就是当母线电流是82.5A的时候,放大器输出3.3V(增量1.65V)

当VG1 = 55mV时,运放输出为1.65V+0.55V

当VG1和VG2均为55mV时,运放输出为1.65V + 0.55V + 0.55V 

当VG1、VG2、VG3均为55mV时,运放输出为1.65V+0.55V+0.55V+0.55V

采样电阻时2mohm,如果每相采样电阻都产生55mV的压降,那么每相的电流就是27.5A,母线电流时三相电流和,那是不是就是27.5A x 3呢