This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: 关于无法进入RX fifo 中断的问题

Part Number: TMS320F280039C

您好:

我参考的是官方的sci_ex2_loopback_interrupts.c例程进行串口收发的调试,经过测试发现无法进入接收中断服务函数,代码如下:

uint16_t sDataA[2];
uint16_t rDataA[2];

//
// Function Prototypes
//
__interrupt void sciaTxISR(void);
__interrupt void sciaRxISR(void);

//
// Main
//
void main(void)
{
    uint16_t i;
    //
    // Configure PLL, disable WD, enable peripheral clocks.
    //
    Device_init();

    //
    // Disable pin locks and enable internal pullups.
    //
    Device_initGPIO();

    //
    // GPIO28 is the SCI Rx pin.
    //
    GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
    GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);

    //
    // GPIO29 is the SCI Tx pin.
    //
    GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
    GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT);
    GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
    GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);

    //
    // Disable global interrupts.
    //
//    DINT;

    //
    // Initialize interrupt controller and vector table.
    //
    Interrupt_initModule();
    Interrupt_initVectorTable();


    //
    // Map the ISR to the wake interrupt.
    //
    Interrupt_register(INT_SCIA_TX, sciaTxISR);
    Interrupt_register(INT_SCIA_RX, sciaRxISR);

    //
    // Initialize SCIA and its FIFO.
    //
    SCI_performSoftwareReset(SCIA_BASE);

    //
    // Configure SCIA for echoback.
    //
    SCI_setConfig(SCIA_BASE, DEVICE_LSPCLK_FREQ, 9600, (SCI_CONFIG_WLEN_8 |
                                             SCI_CONFIG_STOP_ONE |
                                             SCI_CONFIG_PAR_NONE));
    SCI_enableModule(SCIA_BASE);
    SCI_disableLoopback(SCIA_BASE);
    SCI_resetChannels(SCIA_BASE);
    SCI_enableFIFO(SCIA_BASE);


    SCI_enableInterrupt(SCIA_BASE, (SCI_INT_RXFF | SCI_INT_TXFF));
    SCI_disableInterrupt(SCIA_BASE, SCI_INT_RXERR);


    SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX2, SCI_FIFO_RX2);
    SCI_performSoftwareReset(SCIA_BASE);
    SCI_resetTxFIFO(SCIA_BASE);
    SCI_resetRxFIFO(SCIA_BASE);


    for(i = 0; i < 2; i++)
    {
        sDataA[i] = i + 1;
    }

#ifdef AUTOBAUD
    //
    // Perform an autobaud lock.
    // SCI expects an 'a' or 'A' to lock the baud rate.
    //
    SCI_lockAutobaud(SCIA_BASE);
#endif



    //
    // Clear the SCI interrupts before enabling them.
    //
    SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);

    //
    // Enable the interrupts in the PIE: Group 9 interrupts 1 & 2.
    //
    Interrupt_enable(INT_SCIA_RX);
    Interrupt_enable(INT_SCIA_TX);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);

    //
    // Enable global interrupts.
    //
    EINT;
    ERTM;

    for(;;)
    {

    }
}

//
// sciaTxISR - Disable the TXRDY interrupt and print message asking
//             for a character.
//
__interrupt void sciaTxISR(void)
{
    //
    // Disable the TXRDY interrupt.
    //
    SCI_disableInterrupt(SCIA_BASE, SCI_INT_TXFF);

    SCI_writeCharArray(SCIA_BASE, sDataA, 2);

    //
    // Ackowledge the PIE interrupt.
    //
    SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

//
// sciaRxISR - Read the character from the RXBUF and echo it back.
//
__interrupt void sciaRxISR(void)
{
    //
    // Read a character from the RXBUF.
    //
    SCI_readCharArray(SPIA_BASE,rDataA,2);


    //
    // Acknowledge the PIE interrupt.
    //
    SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF);
    Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}

我打断点发现,在完成SCI_enableFIFO(SCIA_BASE)后,SCIFFPE变成了1,并且后面的复位操作并没有消除该错误标志。

麻烦您帮忙看看我的程序是否存在问题,谢谢!