Part Number: TMS320F280039C
您好:
我参考的是官方的sci_ex2_loopback_interrupts.c例程进行串口收发的调试,经过测试发现无法进入接收中断服务函数,代码如下:
uint16_t sDataA[2];
uint16_t rDataA[2];
//
// Function Prototypes
//
__interrupt void sciaTxISR(void);
__interrupt void sciaRxISR(void);
//
// Main
//
void main(void)
{
uint16_t i;
//
// Configure PLL, disable WD, enable peripheral clocks.
//
Device_init();
//
// Disable pin locks and enable internal pullups.
//
Device_initGPIO();
//
// GPIO28 is the SCI Rx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCIRXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_DIR_MODE_IN);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCIRXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCIRXDA, GPIO_QUAL_ASYNC);
//
// GPIO29 is the SCI Tx pin.
//
GPIO_setPinConfig(DEVICE_GPIO_CFG_SCITXDA);
GPIO_setDirectionMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(DEVICE_GPIO_PIN_SCITXDA, GPIO_PIN_TYPE_STD);
GPIO_setQualificationMode(DEVICE_GPIO_PIN_SCITXDA, GPIO_QUAL_ASYNC);
//
// Disable global interrupts.
//
// DINT;
//
// Initialize interrupt controller and vector table.
//
Interrupt_initModule();
Interrupt_initVectorTable();
//
// Map the ISR to the wake interrupt.
//
Interrupt_register(INT_SCIA_TX, sciaTxISR);
Interrupt_register(INT_SCIA_RX, sciaRxISR);
//
// Initialize SCIA and its FIFO.
//
SCI_performSoftwareReset(SCIA_BASE);
//
// Configure SCIA for echoback.
//
SCI_setConfig(SCIA_BASE, DEVICE_LSPCLK_FREQ, 9600, (SCI_CONFIG_WLEN_8 |
SCI_CONFIG_STOP_ONE |
SCI_CONFIG_PAR_NONE));
SCI_enableModule(SCIA_BASE);
SCI_disableLoopback(SCIA_BASE);
SCI_resetChannels(SCIA_BASE);
SCI_enableFIFO(SCIA_BASE);
SCI_enableInterrupt(SCIA_BASE, (SCI_INT_RXFF | SCI_INT_TXFF));
SCI_disableInterrupt(SCIA_BASE, SCI_INT_RXERR);
SCI_setFIFOInterruptLevel(SCIA_BASE, SCI_FIFO_TX2, SCI_FIFO_RX2);
SCI_performSoftwareReset(SCIA_BASE);
SCI_resetTxFIFO(SCIA_BASE);
SCI_resetRxFIFO(SCIA_BASE);
for(i = 0; i < 2; i++)
{
sDataA[i] = i + 1;
}
#ifdef AUTOBAUD
//
// Perform an autobaud lock.
// SCI expects an 'a' or 'A' to lock the baud rate.
//
SCI_lockAutobaud(SCIA_BASE);
#endif
//
// Clear the SCI interrupts before enabling them.
//
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF | SCI_INT_RXFF);
//
// Enable the interrupts in the PIE: Group 9 interrupts 1 & 2.
//
Interrupt_enable(INT_SCIA_RX);
Interrupt_enable(INT_SCIA_TX);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
//
// Enable global interrupts.
//
EINT;
ERTM;
for(;;)
{
}
}
//
// sciaTxISR - Disable the TXRDY interrupt and print message asking
// for a character.
//
__interrupt void sciaTxISR(void)
{
//
// Disable the TXRDY interrupt.
//
SCI_disableInterrupt(SCIA_BASE, SCI_INT_TXFF);
SCI_writeCharArray(SCIA_BASE, sDataA, 2);
//
// Ackowledge the PIE interrupt.
//
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_TXFF);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
//
// sciaRxISR - Read the character from the RXBUF and echo it back.
//
__interrupt void sciaRxISR(void)
{
//
// Read a character from the RXBUF.
//
SCI_readCharArray(SPIA_BASE,rDataA,2);
//
// Acknowledge the PIE interrupt.
//
SCI_clearInterruptStatus(SCIA_BASE, SCI_INT_RXFF);
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
我打断点发现,在完成SCI_enableFIFO(SCIA_BASE)后,SCIFFPE变成了1,并且后面的复位操作并没有消除该错误标志。

麻烦您帮忙看看我的程序是否存在问题,谢谢!