This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: HEX文件第一行不对,是哪里出了问题

Part Number: TMS320F28377S


  • 您好,您的HEX文件是怎么生成的?

    方便具体指明一下异常的情况吗?

  • 通过生成的out文件,用hex2000

    生成的,hex文件开始应该是:02000004003FBB,而这个hex有问题,第一行不是这种,直接是数据的hex,cmd没有问题

  • 就是hex文件里的代码,cla里面的代码hex数据出现在我的flash之前,且第一行没有出现拓展地址

  • 就是hex文件里的代码,cla里面的代码hex数据出现在我的flash之前

    能再进一步阐明一下吗?方便我与相关工程师沟通

    且第一行没有出现拓展地址

    就是您说的02000004003FBB吧?

    hex文件开始应该是:02000004003FBB
  • // The user must define CLA_C in the project linker settings if using the
    // CLA C compiler
    // Project Properties -> C2000 Linker -> Advanced Options -> Command File
    // Preprocessing -> --define
    _Cla1Prog_Start = _Cla1funcsRunStart;
    #define CLA_C 1
    #ifdef CLA_C
    // Define a size for the CLA scratchpad area that will be used
    // by the CLA compiler for local symbols and temps
    // Also force references to the special symbols that mark the
    // scratchpad are.
    CLA_SCRATCHPAD_SIZE = 0x100;
    --undef_sym=__cla_scratchpad_end
    --undef_sym=__cla_scratchpad_start
    #endif //CLA_C

    MEMORY
    {
    PAGE 0 :
    /* BEGIN is used for the "boot to SARAM" bootloader mode */

    BEGIN : origin = 0x084000, length = 0x000010
    RAMM0 : origin = 0x000123, length = 0x0002DD
    RAMD0 : origin = 0x00B000, length = 0x000800
    RAMLS0 : origin = 0x008000, length = 0x000800
    RAMLS1 : origin = 0x008800, length = 0x000800
    /* RAMLS4 : origin = 0x00A000, length = 0x000800 */
    /* RAMLS5 : origin = 0x00A800, length = 0x000800 */
    // RAMLS3 : origin = 0x009800, length = 0x000800
    // RAMLS4_5 : origin = 0x00A000, length = 0x001000
    RAMLS4_5_3 : origin = 0x009800, length = 0x001800
    RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on , F28377S, F28375S devices. Remove line on other devices. */
    RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on , F28377S, F28375S devices. Remove line on other devices. */

    // RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    RESET : origin = 0x3FFFC0, length = 0x000002

    /* Flash sectors */
    FLASHA : origin = 0x080002, length = 0x001FFE /* on-chip Flash */
    FLASHB : origin = 0x082000, length = 0x002000 /* on-chip Flash */
    FLASHC : origin = 0x084010, length = 0x001FF0 /* on-chip Flash */
    FLASHD : origin = 0x086000, length = 0x002000 /* on-chip Flash */
    FLASHE : origin = 0x088000, length = 0x008000 /* on-chip Flash */
    FLASHF : origin = 0x090000, length = 0x008000 /* on-chip Flash */
    FLASHG : origin = 0x098000, length = 0x008000 /* on-chip Flash */
    FLASHH : origin = 0x0A0000, length = 0x008000 /* on-chip Flash */
    FLASHI : origin = 0x0A8000, length = 0x008000 /* on-chip Flash */
    FLASHJ : origin = 0x0B0000, length = 0x008000 /* on-chip Flash */
    FLASHK : origin = 0x0B8000, length = 0x002000 /* on-chip Flash */
    FLASHL : origin = 0x0BA000, length = 0x002000 /* on-chip Flash */
    FLASHM : origin = 0x0BC000, length = 0x002000 /* on-chip Flash */
    FLASHN : origin = 0x0BE000, length = 0x001FF0 /* on-chip Flash */

    // FLASHN_RSVD : origin = 0x0BFFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */


    PAGE 1 :

    BOOT_RSVD : origin = 0x000002, length = 0x000121 /* Part of M0, BOOT rom will use this for stack */
    RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */
    // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    RAMLS2 : origin = 0x009000, length = 0x000800
    // RAMLS3 : origin = 0x009800, length = 0x000800

    RAMGS0 : origin = 0x00C000, length = 0x001000
    RAMGS1 : origin = 0x00D000, length = 0x001000
    RAMGS2 : origin = 0x00E000, length = 0x001000
    RAMGS3 : origin = 0x00F000, length = 0x001000
    RAMGS4 : origin = 0x010000, length = 0x001000
    RAMGS5 : origin = 0x011000, length = 0x001000
    RAMGS6 : origin = 0x012000, length = 0x001000
    RAMGS7 : origin = 0x013000, length = 0x001000
    RAMGS8 : origin = 0x014000, length = 0x001000
    RAMGS9 : origin = 0x015000, length = 0x001000
    RAMGS10 : origin = 0x016000, length = 0x001000

    // RAMGS11 : origin = 0x017000, length = 0x000FF8 /* Uncomment for F28374D, F28376D devices */

    // RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */

    RAMGS11 : origin = 0x017000, length = 0x001000 /* Only Available on , F28377S, F28375S devices. Remove line on other devices. */
    RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on , F28377S, F28375S devices. Remove line on other devices. */
    RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on , F28377S, F28375S devices. Remove line on other devices. */

    EMIF1_CS0n : origin = 0x80000000, length = 0x10000000
    EMIF1_CS2n : origin = 0x00100000, length = 0x00200000
    EMIF1_CS3n : origin = 0x00300000, length = 0x00080000
    EMIF1_CS4n : origin = 0x00380000, length = 0x00060000
    EMIF2_CS0n : origin = 0x90000000, length = 0x10000000
    EMIF2_CS2n : origin = 0x00002000, length = 0x00001000

    CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
    CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
    }


    SECTIONS
    {
    /* Allocate program areas: */
    .cinit : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
    .text : >> FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
    codestart : > BEGIN PAGE = 0, ALIGN(8)
    .stack : > RAMM1 PAGE = 1
    .switch : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)

    /* Allocate uninitalized data sections: */

    #if defined(__TI_EABI__)
    .init_array : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH, PAGE = 0, ALIGN(4)
    .bss : > RAMLS2, PAGE = 1
    .bss:output : > RAMLS2, PAGE = 1
    .data : > RAMLS2, PAGE = 1
    .sysmem : > RAMLS2, PAGE = 1
    .const : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH, PAGE = 0, ALIGN(4)
    #else
    .pinit : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH, PAGE = 0, ALIGN(4)
    .ebss : >> RAMLS2|RAMGS5|RAMGS6, PAGE = 1
    .esysmem : > RAMLS2, PAGE = 1
    .econst : > FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4)
    #endif

    .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */

    Filter_RegsFile : > RAMGS0, PAGE = 1

    .em2_cs0 : > EMIF2_CS0n, PAGE = 1
    .em2_cs2 : > EMIF2_CS2n, PAGE = 1

    /* CLA specific sections */
    #if defined(__TI_EABI__)
    Cla1Prog : LOAD = FLASHD,
    RUN = RAMLS4_5_3,
    LOAD_START(Cla1funcsLoadStart),
    LOAD_END(Cla1funcsLoadEnd),
    RUN_START(Cla1funcsRunStart),
    LOAD_SIZE(Cla1funcsLoadSize),
    PAGE = 0, ALIGN(4)
    #else
    Cla1Prog : LOAD = FLASHD,
    RUN = RAMLS4_5_3,
    LOAD_START(_Cla1funcsLoadStart),
    LOAD_END(_Cla1funcsLoadEnd),
    RUN_START(_Cla1funcsRunStart),
    LOAD_SIZE(_Cla1funcsLoadSize),
    PAGE = 0, ALIGN(4)
    #endif

    CLADataLS0 : > RAMLS0, PAGE=0
    CLADataLS1 : > RAMLS1, PAGE=0

    Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
    CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1

    #ifdef __TI_COMPILER_VERSION__
    #if __TI_COMPILER_VERSION__ >= 15009000
    #if defined(__TI_EABI__)
    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMD0 | RAMLS0 | RAMLS1,
    LOAD_START(RamfuncsLoadStart),
    LOAD_SIZE(RamfuncsLoadSize),
    LOAD_END(RamfuncsLoadEnd),
    RUN_START(RamfuncsRunStart),
    RUN_SIZE(RamfuncsRunSize),
    RUN_END(RamfuncsRunEnd),
    PAGE = 0, ALIGN(4)
    #else
    .TI.ramfunc : {} LOAD = FLASHD,
    RUN = RAMD0 | RAMLS0 | RAMLS1,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0, ALIGN(4)
    #endif
    #else
    ramfuncs : LOAD = FLASHD,
    RUN = RAMD0 | RAMLS0 | RAMLS1,
    LOAD_START(_RamfuncsLoadStart),
    LOAD_SIZE(_RamfuncsLoadSize),
    LOAD_END(_RamfuncsLoadEnd),
    RUN_START(_RamfuncsRunStart),
    RUN_SIZE(_RamfuncsRunSize),
    RUN_END(_RamfuncsRunEnd),
    PAGE = 0, ALIGN(4)
    #endif
    #endif

    /* The following section definition are for SDFM examples */
    Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111
    Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222
    Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333
    Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444

    #ifdef CLA_C
    /* CLA C compiler sections */
    //
    // Must be allocated to memory the CLA has write access to
    //
    CLAscratch :
    { *.obj(CLAscratch)
    . += CLA_SCRATCHPAD_SIZE;
    *.obj(CLAscratch_end) } > RAMLS1, PAGE = 0, ALIGN(4)

    .scratchpad : > RAMLS1, PAGE = 0
    .bss_cla : > RAMLS1, PAGE = 0
    .const_cla : LOAD = FLASHC | FLASHD | FLASHE | FLASHF | FLASHG | FLASHH,
    RUN = RAMLS1,
    RUN_START(_Cla1ConstRunStart),
    LOAD_START(_Cla1ConstLoadStart),
    LOAD_SIZE(_Cla1ConstLoadSize),
    PAGE = 0, ALIGN(4)
    #endif //CLA_C
    }

    /*
    //===========================================================================
    // End of file.
    //===========================================================================
    */

    这是我的cmd配置,怎么把ramls0和ramls1的代码放到flash扇区

  • 这个问题和您之前的问题有关联吗?

    CLA的代码放置在FLASH中,运行时先copy到RAM中,再从RAM中运行。您帖出来的CMD文件就是这样的,CLA的代码存放在FLASHD,运行时copy到RAMLS0和RAMLS1中。

  • 但是我的hex文件里,ramls0和ramls1相关代码还体现在ram区

  • 您所说的体现是什么意思?

    因为这些代码最终是要搬到RAM中运行,所以在TI的例程中,loadstart选择的是FLASH,而runstart选择的则是RAM

  •  您好,就是现在flash写入,C D扇区都能写入,但是flashE写不进去,知道可能是哪里的原因吗

  • 您所说的不能写入是不能链接到输出文件中,还是可以链接到输出文件、但是无法烧入MCU的相关FLASH中?

  • 可以链接到输出文件,无法烧入MCU的flash,flashC和FLASHd能正常烧入,但是flashe无法烧入,打断点编程语句也执行了,但是还是FFFF

  • 打断点可以执行的话看一下反汇编,反汇编会显示代码存放的地址

  • debug界面下view-->disassembly,反汇编代码前面就会显示相应的地址